LESENSE_TypeDef Struct ReferenceDevices > EFM32GG_LESENSE
Definition at line 48
of file efm32gg_lesense.h
.
Data Fields | |
__IOM uint32_t | ALTEXCONF |
__IOM uint32_t | BIASCTRL |
LESENSE_BUF_TypeDef | BUF [16] |
__IM uint32_t | BUFDATA |
LESENSE_CH_TypeDef | CH [16] |
__IOM uint32_t | CHEN |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IM uint32_t | CURCH |
__IOM uint32_t | DECCTRL |
__IOM uint32_t | DECSTATE |
__IOM uint32_t | IDLECONF |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | PERCTRL |
__IOM uint32_t | POWERDOWN |
__IM uint32_t | PTR |
uint32_t | RESERVED0 [105] |
__IOM uint32_t | ROUTE |
__IM uint32_t | SCANRES |
__IOM uint32_t | SENSORSTATE |
LESENSE_ST_TypeDef | ST [16] |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
__IOM uint32_t | TIMCTRL |
Field Documentation
__IOM uint32_t LESENSE_TypeDef::ALTEXCONF |
Alternative excite pin configuration
Definition at line 64
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::BIASCTRL |
Bias Control Register
Definition at line 53
of file efm32gg_lesense.h
.
LESENSE_BUF_TypeDef LESENSE_TypeDef::BUF[16] |
Scanresult
Definition at line 76
of file efm32gg_lesense.h
.
__IM uint32_t LESENSE_TypeDef::BUFDATA |
Result buffer data register
Definition at line 59
of file efm32gg_lesense.h
.
LESENSE_CH_TypeDef LESENSE_TypeDef::CH[16] |
Scanconfig
Definition at line 78
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::CHEN |
Channel enable Register
Definition at line 55
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::CMD |
Command Register
Definition at line 54
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32gg_lesense.h
.
__IM uint32_t LESENSE_TypeDef::CURCH |
Current channel index
Definition at line 60
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::DECCTRL |
Decoder control Register
Definition at line 52
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::DECSTATE |
Current decoder state
Definition at line 61
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::IDLECONF |
GPIO Idle phase configuration
Definition at line 63
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::IEN |
Interrupt Enable Register
Definition at line 68
of file efm32gg_lesense.h
.
__IM uint32_t LESENSE_TypeDef::IF |
Interrupt Flag Register
Definition at line 65
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 66
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 67
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::PERCTRL |
Peripheral Control Register
Definition at line 51
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::POWERDOWN |
LESENSE RAM power-down register
Definition at line 71
of file efm32gg_lesense.h
.
__IM uint32_t LESENSE_TypeDef::PTR |
Result buffer pointers
Definition at line 58
of file efm32gg_lesense.h
.
uint32_t LESENSE_TypeDef::RESERVED0[105] |
Reserved registers
Definition at line 73
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::ROUTE |
I/O Routing Register
Definition at line 70
of file efm32gg_lesense.h
.
__IM uint32_t LESENSE_TypeDef::SCANRES |
Scan result register
Definition at line 56
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::SENSORSTATE |
Decoder input register
Definition at line 62
of file efm32gg_lesense.h
.
LESENSE_ST_TypeDef LESENSE_TypeDef::ST[16] |
Decoding states
Definition at line 74
of file efm32gg_lesense.h
.
__IM uint32_t LESENSE_TypeDef::STATUS |
Status Register
Definition at line 57
of file efm32gg_lesense.h
.
__IM uint32_t LESENSE_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 69
of file efm32gg_lesense.h
.
__IOM uint32_t LESENSE_TypeDef::TIMCTRL |
Timing Control Register
Definition at line 50
of file efm32gg_lesense.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG/Include/
efm32gg_lesense.h