EBI_TypeDef Struct ReferenceDevices > EFM32GG_EBI
Definition at line 48
of file efm32gg_ebi.h
.
Data Fields | |
__IOM uint32_t | ADDRTIMING |
__IOM uint32_t | ADDRTIMING1 |
__IOM uint32_t | ADDRTIMING2 |
__IOM uint32_t | ADDRTIMING3 |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IM uint32_t | ECCPARITY |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | NANDCTRL |
__IOM uint32_t | PAGECTRL |
__IOM uint32_t | POLARITY |
__IOM uint32_t | POLARITY1 |
__IOM uint32_t | POLARITY2 |
__IOM uint32_t | POLARITY3 |
__IOM uint32_t | RDTIMING |
__IOM uint32_t | RDTIMING1 |
__IOM uint32_t | RDTIMING2 |
__IOM uint32_t | RDTIMING3 |
__IOM uint32_t | ROUTE |
__IM uint32_t | STATUS |
__IOM uint32_t | TFTALPHA |
__IOM uint32_t | TFTCTRL |
__IOM uint32_t | TFTDD |
__IOM uint32_t | TFTFRAMEBASE |
__IOM uint32_t | TFTHPORCH |
__IOM uint32_t | TFTMASK |
__IM uint32_t | TFTPIXEL |
__IOM uint32_t | TFTPIXEL0 |
__IOM uint32_t | TFTPIXEL1 |
__IOM uint32_t | TFTPOLARITY |
__IOM uint32_t | TFTSIZE |
__IM uint32_t | TFTSTATUS |
__IOM uint32_t | TFTSTRIDE |
__IOM uint32_t | TFTTIMING |
__IOM uint32_t | TFTVPORCH |
__IOM uint32_t | WRTIMING |
__IOM uint32_t | WRTIMING1 |
__IOM uint32_t | WRTIMING2 |
__IOM uint32_t | WRTIMING3 |
Field Documentation
__IOM uint32_t EBI_TypeDef::ADDRTIMING |
Address Timing Register
Definition at line 50
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::ADDRTIMING1 |
Address Timing Register 1
Definition at line 55
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::ADDRTIMING2 |
Address Timing Register 2
Definition at line 59
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::ADDRTIMING3 |
Address Timing Register 3
Definition at line 63
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::CMD |
Command Register
Definition at line 69
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::CTRL |
Control Register
Definition at line 49
of file efm32gg_ebi.h
.
__IM uint32_t EBI_TypeDef::ECCPARITY |
ECC Parity register
Definition at line 71
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::IEN |
Interrupt Enable Register
Definition at line 90
of file efm32gg_ebi.h
.
__IM uint32_t EBI_TypeDef::IF |
Interrupt Flag Register
Definition at line 87
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 89
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 88
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::NANDCTRL |
NAND Control Register
Definition at line 68
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::PAGECTRL |
Page Control Register
Definition at line 67
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::POLARITY |
Polarity Register
Definition at line 53
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::POLARITY1 |
Polarity Register 1
Definition at line 58
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::POLARITY2 |
Polarity Register 2
Definition at line 62
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::POLARITY3 |
Polarity Register 3
Definition at line 66
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::RDTIMING |
Read Timing Register
Definition at line 51
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::RDTIMING1 |
Read Timing Register 1
Definition at line 56
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::RDTIMING2 |
Read Timing Register 2
Definition at line 60
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::RDTIMING3 |
Read Timing Register 3
Definition at line 64
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::ROUTE |
I/O Routing Register
Definition at line 54
of file efm32gg_ebi.h
.
__IM uint32_t EBI_TypeDef::STATUS |
Status Register
Definition at line 70
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTALPHA |
TFT Alpha Blending Register
Definition at line 82
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTCTRL |
TFT Control Register
Definition at line 72
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTDD |
TFT Direct Drive Data Register
Definition at line 81
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTFRAMEBASE |
TFT Frame Base Register
Definition at line 74
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTHPORCH |
TFT Horizontal Porch Register
Definition at line 77
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTMASK |
TFT Masking Register
Definition at line 86
of file efm32gg_ebi.h
.
__IM uint32_t EBI_TypeDef::TFTPIXEL |
TFT Alpha Blending Result Pixel Register
Definition at line 85
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTPIXEL0 |
TFT Pixel 0 Register
Definition at line 83
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTPIXEL1 |
TFT Pixel 1 Register
Definition at line 84
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTPOLARITY |
TFT Polarity Register
Definition at line 80
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTSIZE |
TFT Size Register
Definition at line 76
of file efm32gg_ebi.h
.
__IM uint32_t EBI_TypeDef::TFTSTATUS |
TFT Status Register
Definition at line 73
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTSTRIDE |
TFT Stride Register
Definition at line 75
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTTIMING |
TFT Timing Register
Definition at line 79
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::TFTVPORCH |
TFT Vertical Porch Register
Definition at line 78
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::WRTIMING |
Write Timing Register
Definition at line 52
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::WRTIMING1 |
Write Timing Register 1
Definition at line 57
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::WRTIMING2 |
Write Timing Register 2
Definition at line 61
of file efm32gg_ebi.h
.
__IOM uint32_t EBI_TypeDef::WRTIMING3 |
Write Timing Register 3
Definition at line 65
of file efm32gg_ebi.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG/Include/
efm32gg_ebi.h