USB_HC_TypeDef Struct ReferenceDevices
USB_HC EFM32GG USB HC.
Definition at line 46
of file efm32gg_usb_hc.h
.
#include <
efm32gg_usb_hc.h
>
Data Fields | |
__IOM uint32_t | CHAR |
__IOM uint32_t | DMAADDR |
__IOM uint32_t | INT |
__IOM uint32_t | INTMSK |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [2] |
__IOM uint32_t | TSIZ |
Field Documentation
__IOM uint32_t USB_HC_TypeDef::CHAR |
Host Channel x Characteristics Register
Definition at line 47
of file efm32gg_usb_hc.h
.
__IOM uint32_t USB_HC_TypeDef::DMAADDR |
Host Channel x DMA Address Register
Definition at line 52
of file efm32gg_usb_hc.h
.
__IOM uint32_t USB_HC_TypeDef::INT |
Host Channel x Interrupt Register
Definition at line 49
of file efm32gg_usb_hc.h
.
__IOM uint32_t USB_HC_TypeDef::INTMSK |
Host Channel x Interrupt Mask Register
Definition at line 50
of file efm32gg_usb_hc.h
.
uint32_t USB_HC_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 48
of file efm32gg_usb_hc.h
.
uint32_t USB_HC_TypeDef::RESERVED1[2] |
Reserved future
Definition at line 53
of file efm32gg_usb_hc.h
.
__IOM uint32_t USB_HC_TypeDef::TSIZ |
Host Channel x Transfer Size Register
Definition at line 51
of file efm32gg_usb_hc.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG/Include/
efm32gg_usb_hc.h