CANEMLIB
Detailed Description
Controller Area Network API.
The Controller Area Network Interface Bus (CAN) implements a multi-master serial bus for connecting microcontrollers and devices, also known as nodes, to communicate with each other in applications without a host computer. CAN is a message-based protocol, designed originally for automotive applications, but meanwhile used also in many other surroundings. The complexity of the node can range from a simple I/O device up to an embedded computer with a CAN interface and sophisticated software. The node may also be a gateway allowing a standard computer to communicate over a USB or Ethernet port to the devices on a CAN network. Devices are connected to the bus through a host processor, a CAN controller, and a CAN transceiver.
Data Structures |
|
| struct | CAN_Init_TypeDef |
| struct | CAN_MessageObject_TypeDef |
Macros |
|
| #define | CAN_INIT_DEFAULT |
Enumerations |
|
| enum |
CAN_ErrorCode_TypeDef
{
canErrorNoError = CAN_STATUS_LEC_NONE, canErrorStuff = CAN_STATUS_LEC_STUFF, canErrorForm = CAN_STATUS_LEC_FORM, canErrorAck = CAN_STATUS_LEC_ACK, canErrorBit1 = CAN_STATUS_LEC_BIT1, canErrorBit0 = CAN_STATUS_LEC_BIT0, canErrorCrc = CAN_STATUS_LEC_CRC, canErrorUnused = CAN_STATUS_LEC_UNUSED } |
| enum |
CAN_Mode_TypeDef
{
canModeNormal , canModeBasic , canModeLoopBack , canModeSilentLoopBack , canModeSilent } |
Functions |
|
| void | CAN_AbortSendMessage ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool wait) |
|
Abort the sending of a message.
|
|
| void | CAN_ConfigureMessageObject ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool valid, bool tx, bool remoteTransfer, bool endOfBuffer, bool wait) |
|
Configure valid, tx/rx, remoteTransfer for a specific Message Object.
|
|
| __STATIC_INLINE void | CAN_Enable ( CAN_TypeDef *can, bool enable) |
|
Enable the Host Controller to send messages.
|
|
| uint32_t | CAN_GetClockFrequency ( CAN_TypeDef *can) |
|
Get the CAN module frequency.
|
|
| __STATIC_INLINE uint32_t | CAN_GetErrorCount ( CAN_TypeDef *can) |
|
Get the error count.
|
|
| __STATIC_INLINE CAN_ErrorCode_TypeDef | CAN_GetLastErrorCode ( CAN_TypeDef *can) |
|
Get the last error code and clear its register.
|
|
| __STATIC_INLINE uint32_t | CAN_HasNewdata ( CAN_TypeDef *can) |
|
Indicates which messages objects have received new data.
|
|
| void | CAN_Init ( CAN_TypeDef *can, const CAN_Init_TypeDef *init) |
|
Initialize CAN.
|
|
| __STATIC_INLINE bool | CAN_IsEnabled ( CAN_TypeDef *can) |
|
Gives the communication capabilities state.
|
|
| __STATIC_INLINE void | CAN_MessageIntClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear one or more pending CAN message interrupts.
|
|
| __STATIC_INLINE void | CAN_MessageIntDisable ( CAN_TypeDef *can, uint32_t flags) |
|
Disable CAN message interrupts.
|
|
| __STATIC_INLINE void | CAN_MessageIntEnable ( CAN_TypeDef *can, uint32_t flags) |
|
Enable CAN message interrupts.
|
|
| __STATIC_INLINE uint32_t | CAN_MessageIntGet ( CAN_TypeDef *can) |
|
Get pending CAN message interrupt flags.
|
|
| __STATIC_INLINE uint32_t | CAN_MessageIntGetEnabled ( CAN_TypeDef *can) |
|
Get CAN message interrupt flags that are pending and enabled.
|
|
| __STATIC_INLINE void | CAN_MessageIntSet ( CAN_TypeDef *can, uint32_t flags) |
|
Set one or more CAN message interrupts.
|
|
| bool | CAN_MessageLost ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum) |
|
Read a Message Object to find if a message was lost ; reset the 'Message Lost' flag.
|
|
| void | CAN_ReadMessage ( CAN_TypeDef *can, uint8_t interface, CAN_MessageObject_TypeDef *message) |
|
Read the data from a Message Object in the RAM and store it in message.
|
|
| __STATIC_INLINE void | CAN_ReadyWait ( CAN_TypeDef *can, uint8_t interface) |
|
Waiting function.
|
|
| void | CAN_Reset ( CAN_TypeDef *can) |
|
Set all the CAN registers to RESETVALUE. Leave the CAN Device disabled.
|
|
| void | CAN_ResetMessages ( CAN_TypeDef *can, uint8_t interface) |
|
Reset all the Message Objects and set their data to 0.
|
|
| void | CAN_SendMessage ( CAN_TypeDef *can, uint8_t interface, const CAN_MessageObject_TypeDef *message, bool wait) |
|
Send the data from the Message Object message.
|
|
| void | CAN_SendRequest ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool wait) |
|
Send request for writing or reading the RAM of Message Object msgNum.
|
|
| void | CAN_SetBitTiming ( CAN_TypeDef *can, uint32_t bitrate, uint16_t propagationTimeSegment, uint16_t phaseBufferSegment1, uint16_t phaseBufferSegment2, uint16_t synchronisationJumpWidth) |
|
Set the bitrate and its parameters.
|
|
| void | CAN_SetIdAndFilter ( CAN_TypeDef *can, uint8_t interface, bool useMask, const CAN_MessageObject_TypeDef *message, bool wait) |
|
Set the Id and the filter for a specific Message Object.
|
|
| void | CAN_SetMode ( CAN_TypeDef *can, CAN_Mode_TypeDef mode) |
|
Set the CAN operation mode.
|
|
| void | CAN_SetRoute ( CAN_TypeDef *can, bool active, uint16_t pinRxLoc, uint16_t pinTxLoc) |
|
Set the ROUTE registers.
|
|
| __STATIC_INLINE void | CAN_StatusClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear CAN status.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusGet ( CAN_TypeDef *can) |
|
Get CAN status.
|
|
| __STATIC_INLINE void | CAN_StatusIntClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear one or more pending CAN status interrupts.
|
|
| __STATIC_INLINE void | CAN_StatusIntDisable ( CAN_TypeDef *can, uint32_t flags) |
|
Disable CAN status interrupts.
|
|
| __STATIC_INLINE void | CAN_StatusIntEnable ( CAN_TypeDef *can, uint32_t flags) |
|
Enable CAN status interrupts.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusIntGet ( CAN_TypeDef *can) |
|
Get pending CAN status interrupt flags.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusIntGetEnabled ( CAN_TypeDef *can) |
|
Get pending and enabled CAN status interrupt flags.
|
|
| __STATIC_INLINE void | CAN_StatusIntSet ( CAN_TypeDef *can, uint32_t flags) |
|
Set one or more CAN status interrupts.
|
|
| void | CAN_WriteData ( CAN_TypeDef *can, uint8_t interface, const CAN_MessageObject_TypeDef *message) |
|
Write the data from message to the MIRx registers.
|
|
Macro Definition Documentation
| #define CAN_INIT_DEFAULT |
Default initialization of CAN_Init_TypeDef . The total duration of a bit with these default parameters is 10 tq (time quantum : tq = brp/fsys, brp being the baudrate prescaler and being set according to the wanted bitrate, fsys beeing the CAN Device frequency).
Definition at line
185
of file
em_can.h
.
Enumeration Type Documentation
CAN Status codes
Definition at line
65
of file
em_can.h
.
| enum CAN_Mode_TypeDef |
CAN peripheral mode
Definition at line
95
of file
em_can.h
.
Function Documentation
| void CAN_AbortSendMessage | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| uint8_t |
msgNum,
|
||
| bool |
wait
|
||
| ) |
Abort the sending of a message.
Set the TXRQST of the CTRL register to 0. Doesn't touch the data ot the others parameters. The user can reuse CAN_SendMessage() to send the object after using CAN_AbortSendMessage() .
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] msgNumMessage number of this Message Object, [1 - 32]. [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
733
of file
em_can.c
.
References _CAN_MIR_CTRL_TXRQST_MASK , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_WRRD , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , and CAN_TypeDef::MIR .
| void CAN_ConfigureMessageObject | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| uint8_t |
msgNum,
|
||
| bool |
valid,
|
||
| bool |
tx,
|
||
| bool |
remoteTransfer,
|
||
| bool |
endOfBuffer,
|
||
| bool |
wait
|
||
| ) |
Configure valid, tx/rx, remoteTransfer for a specific Message Object.
The Init bit have to be 0 to use this function.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] msgNumMessage number of this Message Object, [1 - 32]. [in] validtrue if Message Object is valid, false otherwise. [in] txtrue if Message Object is used for transmission, false if used for reception. [in] remoteTransfertrue if Message Object is used for remote transmission, false otherwise. [in] endOfBuffertrue if it is for a single Message Object or the end of a fifo buffer, false if the Message Object is part of a fifo buffer and not the last. [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
505
of file
em_can.c
.
References _CAN_MIR_ARB_DIR_MASK , _CAN_MIR_ARB_DIR_SHIFT , _CAN_MIR_ARB_MSGVAL_MASK , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_CTRL_EOB_SHIFT , _CAN_MIR_CTRL_RMTEN_SHIFT , _CAN_MIR_CTRL_RXIE_MASK , _CAN_MIR_CTRL_TXIE_MASK , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , and CAN_TypeDef::MIR .
| __STATIC_INLINE void CAN_Enable | ( | CAN_TypeDef * |
can,
|
| bool |
enable
|
||
| ) |
Enable the Host Controller to send messages.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] enabletrue to enable CAN device, false to disable it. If the CAN device is enabled, it goes in normal mode (the default working mode).
Definition at line
273
of file
em_can.h
.
References _CAN_CTRL_INIT_SHIFT , BUS_RegBitWrite() , and CAN_TypeDef::CTRL .
Referenced by CAN_Init() , and CAN_Reset() .
| uint32_t CAN_GetClockFrequency | ( | CAN_TypeDef * |
can
|
) |
Get the CAN module frequency.
There is an internal prescaler of 2 inside the CAN module.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- Clock value
Definition at line
133
of file
em_can.c
.
References CAN0 , CMU_ClockFreqGet() , and cmuClock_CAN0 .
Referenced by CAN_SetBitTiming() .
| __STATIC_INLINE uint32_t CAN_GetErrorCount | ( | CAN_TypeDef * |
can
|
) |
Get the error count.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- Error count.
Definition at line
484
of file
em_can.h
.
References CAN_TypeDef::ERRCNT .
| __STATIC_INLINE CAN_ErrorCode_TypeDef CAN_GetLastErrorCode | ( | CAN_TypeDef * |
can
|
) |
Get the last error code and clear its register.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- return Last error code.
Definition at line
321
of file
em_can.h
.
References _CAN_STATUS_LEC_MASK , and CAN_TypeDef::STATUS .
| __STATIC_INLINE uint32_t CAN_HasNewdata | ( | CAN_TypeDef * |
can
|
) |
Indicates which messages objects have received new data.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- State of MESSAGEDATA register indicating which messages objects have received new data.
Definition at line
340
of file
em_can.h
.
References CAN_TypeDef::MESSAGEDATA .
| void CAN_Init | ( | CAN_TypeDef * |
can,
|
| const CAN_Init_TypeDef * |
init
|
||
| ) |
Initialize CAN.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] initPointer to CAN initialization structure.
Definition at line
100
of file
em_can.c
.
References _CAN_CTRL_TEST_MASK , _CAN_TEST_RESETVALUE , CAN_Init_TypeDef::bitrate , CAN_CTRL_INIT , CAN_Enable() , CAN_ResetMessages() , CAN_SetBitTiming() , CAN_TypeDef::CTRL , CAN_Init_TypeDef::enable , CAN_Init_TypeDef::phaseBufferSegment1 , CAN_Init_TypeDef::phaseBufferSegment2 , CAN_Init_TypeDef::propagationTimeSegment , CAN_Init_TypeDef::resetMessages , CAN_Init_TypeDef::synchronisationJumpWidth , and CAN_TypeDef::TEST .
| __STATIC_INLINE bool CAN_IsEnabled | ( | CAN_TypeDef * |
can
|
) |
Gives the communication capabilities state.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- true if the Host Controller can send messages, false otherwise.
Definition at line
288
of file
em_can.h
.
References _CAN_CTRL_INIT_MASK , and CAN_TypeDef::CTRL .
Referenced by CAN_SetBitTiming() .
| __STATIC_INLINE void CAN_MessageIntClear | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending CAN message interrupts.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsPending CAN message interrupt source(s) to clear.
Definition at line
499
of file
em_can.h
.
References CAN_TypeDef::IF0IFC .
| __STATIC_INLINE void CAN_MessageIntDisable | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Disable CAN message interrupts.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsCAN message interrupt source(s) to disable.
Definition at line
514
of file
em_can.h
.
References CAN_TypeDef::IF0IEN .
| __STATIC_INLINE void CAN_MessageIntEnable | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Enable CAN message interrupts.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsCAN message interrupt source(s) to enable.
Definition at line
529
of file
em_can.h
.
References CAN_TypeDef::IF0IEN .
| __STATIC_INLINE uint32_t CAN_MessageIntGet | ( | CAN_TypeDef * |
can
|
) |
Get pending CAN message interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- CAN message interrupt source(s) pending.
Definition at line
547
of file
em_can.h
.
References CAN_TypeDef::IF0IF .
| __STATIC_INLINE uint32_t CAN_MessageIntGetEnabled | ( | CAN_TypeDef * |
can
|
) |
Get CAN message interrupt flags that are pending and enabled.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- CAN message interrupt source(s) pending and enabled.
Definition at line
565
of file
em_can.h
.
References CAN_TypeDef::IF0IEN , and CAN_TypeDef::IF0IF .
| __STATIC_INLINE void CAN_MessageIntSet | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Set one or more CAN message interrupts.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsCAN message interrupt source(s) to set to pending.
Definition at line
583
of file
em_can.h
.
References CAN_TypeDef::IF0IFS .
| bool CAN_MessageLost | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| uint8_t |
msgNum
|
||
| ) |
Read a Message Object to find if a message was lost ; reset the 'Message Lost' flag.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] msgNumMessage number of the Message Object, [1 - 32].
- Returns
- true if a message was lost, false otherwise.
Definition at line
167
of file
em_can.c
.
References _CAN_MIR_CTRL_MESSAGEOF_MASK , CAN_MIR_CMDMASK_CLRINTPND , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , and CAN_TypeDef::MIR .
| void CAN_ReadMessage | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| CAN_MessageObject_TypeDef * |
message
|
||
| ) |
Read the data from a Message Object in the RAM and store it in message.
Read all the information from the RAM on this Message Object : the data but also the configuration of the other registers.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] messageMessage Object
Definition at line
663
of file
em_can.c
.
References _CAN_MIR_CTRL_DLC_MASK , _CAN_MIR_CTRL_DLC_SHIFT , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CLRINTPND , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_TXRQSTNEWDAT , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::data , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MessageObject_TypeDef::dlc , CAN_TypeDef::MIR , CAN_MessageObject_TypeDef::msgNum , and SL_MIN .
| __STATIC_INLINE void CAN_ReadyWait | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface
|
||
| ) |
Waiting function.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use.
Definition at line
304
of file
em_can.h
.
References _CAN_MIR_CMDREQ_BUSY_MASK , CAN_MIR_TypeDef::CMDREQ , and CAN_TypeDef::MIR .
Referenced by CAN_AbortSendMessage() , CAN_ConfigureMessageObject() , CAN_MessageLost() , CAN_ReadMessage() , CAN_Reset() , CAN_ResetMessages() , CAN_SendMessage() , CAN_SendRequest() , CAN_SetIdAndFilter() , and CAN_WriteData() .
| void CAN_Reset | ( | CAN_TypeDef * |
can
|
) |
Set all the CAN registers to RESETVALUE. Leave the CAN Device disabled.
- Parameters
-
[in] canPointer to CAN peripheral register block.
Definition at line
797
of file
em_can.c
.
References _CAN_BITTIMING_RESETVALUE , _CAN_BRPE_RESETVALUE , _CAN_CONFIG_RESETVALUE , _CAN_CTRL_CCE_MASK , _CAN_CTRL_TEST_MASK , _CAN_IF0IEN_RESETVALUE , _CAN_IF0IFC_RESETVALUE , _CAN_IF0IFS_RESETVALUE , _CAN_IF1IEN_RESETVALUE , _CAN_IF1IF_RESETVALUE , _CAN_IF1IFC_RESETVALUE , _CAN_MIR_ARB_RESETVALUE , _CAN_MIR_CMDMASK_RESETVALUE , _CAN_MIR_CMDREQ_RESETVALUE , _CAN_MIR_CTRL_RESETVALUE , _CAN_MIR_DATAH_RESETVALUE , _CAN_MIR_DATAL_RESETVALUE , _CAN_MIR_MASK_RESETVALUE , _CAN_ROUTE_RESETVALUE , _CAN_STATUS_RESETVALUE , _CAN_TEST_RESETVALUE , CAN_MIR_TypeDef::ARB , CAN_TypeDef::BITTIMING , CAN_TypeDef::BRPE , CAN_Enable() , CAN_ReadyWait() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CMDREQ , CAN_TypeDef::CONFIG , CAN_TypeDef::CTRL , CAN_MIR_TypeDef::CTRL , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_TypeDef::IF0IEN , CAN_TypeDef::IF0IFC , CAN_TypeDef::IF0IFS , CAN_TypeDef::IF1IEN , CAN_TypeDef::IF1IFC , CAN_TypeDef::IF1IFS , CAN_MIR_TypeDef::MASK , CAN_TypeDef::MIR , CAN_TypeDef::ROUTE , CAN_TypeDef::STATUS , and CAN_TypeDef::TEST .
| void CAN_ResetMessages | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface
|
||
| ) |
Reset all the Message Objects and set their data to 0.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use.
Definition at line
765
of file
em_can.c
.
References _CAN_MIR_ARB_RESETVALUE , _CAN_MIR_CTRL_RESETVALUE , _CAN_MIR_MASK_RESETVALUE , CAN_MIR_TypeDef::ARB , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_WRRD , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MIR_TypeDef::MASK , and CAN_TypeDef::MIR .
Referenced by CAN_Init() .
| void CAN_SendMessage | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| const CAN_MessageObject_TypeDef * |
message,
|
||
| bool |
wait
|
||
| ) |
Send the data from the Message Object message.
If message is configured as tx and remoteTransfer = 0, calling this function will send the data of this Message Object if its parameters are correct. If message is tx and remoteTransfer = 1, this function will set the data of message to the RAM and exit, the data will be automatically sent after reception of a remote frame. If message is rx and remoteTransfer = 1, this function will send a remote frame to the corresponding id. If message is rx and remoteTransfer = 0, the user shouldn't call this function. It will also send a remote frame.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] messageMessage Object [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
576
of file
em_can.c
.
References _CAN_MIR_ARB_DIR_MASK , _CAN_MIR_ARB_DIR_RX , _CAN_MIR_ARB_ID_MASK , _CAN_MIR_ARB_ID_SHIFT , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_ARB_XTD_MASK , _CAN_MIR_CTRL_DLC_MASK , _CAN_MIR_CTRL_RMTEN_MASK , _CAN_STATUS_LEC_MASK , CAN_MIR_TypeDef::ARB , BUS_RegMaskedWrite() , CAN_MIR_ARB_XTD_EXT , CAN_MIR_ARB_XTD_STD , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_DATAA , CAN_MIR_CMDMASK_DATAB , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_MIR_CTRL_DATAVALID , CAN_MIR_CTRL_TXRQST , CAN_ReadyWait() , CAN_SendRequest() , CAN_WriteData() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::dlc , CAN_MessageObject_TypeDef::extended , CAN_MessageObject_TypeDef::id , CAN_TypeDef::MIR , CAN_MessageObject_TypeDef::msgNum , and CAN_TypeDef::STATUS .
| void CAN_SendRequest | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| uint8_t |
msgNum,
|
||
| bool |
wait
|
||
| ) |
Send request for writing or reading the RAM of Message Object msgNum.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] msgNumMessage number of the Message Object, [1 - 32]. [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
888
of file
em_can.c
.
References _CAN_MIR_CMDREQ_MSGNUM_SHIFT , CAN_ReadyWait() , CAN_MIR_TypeDef::CMDREQ , and CAN_TypeDef::MIR .
Referenced by CAN_AbortSendMessage() , CAN_ConfigureMessageObject() , CAN_MessageLost() , CAN_ReadMessage() , CAN_ResetMessages() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
| void CAN_SetBitTiming | ( | CAN_TypeDef * |
can,
|
| uint32_t |
bitrate,
|
||
| uint16_t |
propagationTimeSegment,
|
||
| uint16_t |
phaseBufferSegment1,
|
||
| uint16_t |
phaseBufferSegment2,
|
||
| uint16_t |
synchronisationJumpWidth
|
||
| ) |
Set the bitrate and its parameters.
There are multiple parameters which need to be properly configured. Please refer to the reference manual for a detailed description. Careful : the BRP (Baud Rate Prescaler) is calculated by: 'brp = freq / (period * bitrate);'. freq is the frequency of the CAN device, period the time of transmission of a bit. The result is an uint32_t hence it's truncated, causing an approximation error. This error is non negligeable when period is high, bitrate is high and freq is low.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] bitrateWanted bitrate on the CAN bus. [in] propagationTimeSegmentValue for the Propagation Time Segment. [in] phaseBufferSegment1Value for the Phase Buffer Segment 1. [in] phaseBufferSegment2Value for the Phase Buffer Segment 2. [in] synchronisationJumpWidthValue for the Synchronisation Jump Width.
Definition at line
264
of file
em_can.c
.
References _CAN_BITTIMING_BRP_SHIFT , _CAN_BITTIMING_SJW_SHIFT , _CAN_BITTIMING_TSEG1_SHIFT , _CAN_BITTIMING_TSEG2_SHIFT , _CAN_CTRL_CCE_MASK , _CAN_CTRL_INIT_MASK , CAN_TypeDef::BITTIMING , CAN_TypeDef::BRPE , CAN_CTRL_CCE , CAN_CTRL_INIT , CAN_GetClockFrequency() , CAN_IsEnabled() , and CAN_TypeDef::CTRL .
Referenced by CAN_Init() .
| void CAN_SetIdAndFilter | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| bool |
useMask,
|
||
| const CAN_MessageObject_TypeDef * |
message,
|
||
| bool |
wait
|
||
| ) |
Set the Id and the filter for a specific Message Object.
The Init bit have to be 0 to use this function.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] useMaskBoolean to choose whether or not to use the masks. [in] messageMessage Object [in] waitIf true, wait for the end of the transfer between the MIRx registers and the RAM to exit. If false, exit immediately, the transfer can still be in progress.
Definition at line
410
of file
em_can.c
.
References _CAN_MIR_ARB_ID_MASK , _CAN_MIR_ARB_ID_SHIFT , _CAN_MIR_ARB_MSGVAL_SHIFT , _CAN_MIR_CTRL_UMASK_SHIFT , _CAN_MIR_MASK_MASK_SHIFT , _CAN_MIR_MASK_MDIR_SHIFT , _CAN_MIR_MASK_MXTD_SHIFT , CAN_MIR_TypeDef::ARB , BUS_RegBitWrite() , CAN_MIR_ARB_XTD_EXT , CAN_MIR_ARB_XTD_STD , CAN_MIR_CMDMASK_ARBACC , CAN_MIR_CMDMASK_CONTROL , CAN_MIR_CMDMASK_MASKACC , CAN_MIR_CMDMASK_WRRD , CAN_MIR_CMDMASK_WRRD_READ , CAN_ReadyWait() , CAN_SendRequest() , CAN_MIR_TypeDef::CMDMASK , CAN_MIR_TypeDef::CTRL , CAN_MessageObject_TypeDef::directionMask , CAN_MessageObject_TypeDef::extended , CAN_MessageObject_TypeDef::extendedMask , CAN_MessageObject_TypeDef::id , CAN_MIR_TypeDef::MASK , CAN_MessageObject_TypeDef::mask , CAN_TypeDef::MIR , and CAN_MessageObject_TypeDef::msgNum .
| void CAN_SetMode | ( | CAN_TypeDef * |
can,
|
| CAN_Mode_TypeDef |
mode
|
||
| ) |
Set the CAN operation mode.
In Init mode, the CAN module is deactivated. Reset of the Messages in all the other modes to be sure that there are no leftover data and that they need to be configured before being of use.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] modeMode of operation : Init, Normal, Loopback, SilentLoopback, Silent, Basic.
Definition at line
336
of file
em_can.c
.
References _CAN_CTRL_EIE_MASK , _CAN_CTRL_IE_MASK , _CAN_CTRL_SIE_MASK , _CAN_CTRL_TEST_MASK , _CAN_TEST_RESETVALUE , CAN_CTRL_TEST , CAN_TEST_BASIC , CAN_TEST_LBACK , CAN_TEST_SILENT , canModeBasic , canModeLoopBack , canModeNormal , canModeSilent , canModeSilentLoopBack , CAN_TypeDef::CTRL , and CAN_TypeDef::TEST .
| void CAN_SetRoute | ( | CAN_TypeDef * |
can,
|
| bool |
active,
|
||
| uint16_t |
pinRxLoc,
|
||
| uint16_t |
pinTxLoc
|
||
| ) |
Set the ROUTE registers.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] activeBoolean to activate or not the ROUTE registers. [in] pinRxLocLocation of the rx pin. [in] pinTxLocLocation of the tx pin.
Definition at line
217
of file
em_can.c
.
References _CAN_ROUTE_RXLOC_SHIFT , _CAN_ROUTE_TXLOC_SHIFT , CAN_ROUTE_TXPEN , and CAN_TypeDef::ROUTE .
| __STATIC_INLINE void CAN_StatusClear | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Clear CAN status.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsCAN status bits to clear.
Definition at line
469
of file
em_can.h
.
References CAN_TypeDef::STATUS .
| __STATIC_INLINE uint32_t CAN_StatusGet | ( | CAN_TypeDef * |
can
|
) |
Get CAN status.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- Value of CAN register STATUS.
Definition at line
454
of file
em_can.h
.
References _CAN_STATUS_LEC_MASK , and CAN_TypeDef::STATUS .
| __STATIC_INLINE void CAN_StatusIntClear | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Clear one or more pending CAN status interrupts.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsPending CAN status interrupt source(s) to clear.
Definition at line
355
of file
em_can.h
.
References CAN_TypeDef::IF1IFC .
| __STATIC_INLINE void CAN_StatusIntDisable | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Disable CAN status interrupts.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsCAN status interrupt source(s) to disable.
Definition at line
370
of file
em_can.h
.
References CAN_TypeDef::IF1IEN .
| __STATIC_INLINE void CAN_StatusIntEnable | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Enable CAN status interrupts.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsCAN status interrupt source(s) to enable.
Definition at line
385
of file
em_can.h
.
References CAN_TypeDef::IF1IEN .
| __STATIC_INLINE uint32_t CAN_StatusIntGet | ( | CAN_TypeDef * |
can
|
) |
Get pending CAN status interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- CAN interrupt source(s) pending.
Definition at line
403
of file
em_can.h
.
References CAN_TypeDef::IF1IF .
| __STATIC_INLINE uint32_t CAN_StatusIntGetEnabled | ( | CAN_TypeDef * |
can
|
) |
Get pending and enabled CAN status interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Parameters
-
[in] canPointer to CAN peripheral register block.
- Returns
- CAN interrupt source(s) pending and enabled.
Definition at line
421
of file
em_can.h
.
References CAN_TypeDef::IF1IEN , and CAN_TypeDef::IF1IF .
| __STATIC_INLINE void CAN_StatusIntSet | ( | CAN_TypeDef * |
can,
|
| uint32_t |
flags
|
||
| ) |
Set one or more CAN status interrupts.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] flagsCAN status interrupt source(s) to set to pending.
Definition at line
439
of file
em_can.h
.
References CAN_TypeDef::IF1IFS .
| void CAN_WriteData | ( | CAN_TypeDef * |
can,
|
| uint8_t |
interface,
|
||
| const CAN_MessageObject_TypeDef * |
message
|
||
| ) |
Write the data from message to the MIRx registers.
- Parameters
-
[in] canPointer to CAN peripheral register block. [in] interfaceIndicate which Message Interface Register to use. [in] messageMessage Object
Definition at line
847
of file
em_can.c
.
References CAN_ReadyWait() , CAN_MessageObject_TypeDef::data , CAN_MIR_TypeDef::DATAH , CAN_MIR_TypeDef::DATAL , CAN_MessageObject_TypeDef::dlc , CAN_TypeDef::MIR , and SL_MIN .
Referenced by CAN_SendMessage() .