RMU_TypeDef Struct ReferenceDevices > RMU

RMU Register Declaration

Definition at line 49 of file efm32tg11b_rmu.h.

#include <efm32tg11b_rmu.h>

Data Fields

__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IOM uint32_t LOCK
 
__IOM uint32_t RST
 
__IM uint32_t RSTCAUSE
 

Field Documentation

__IOM uint32_t RMU_TypeDef::CMD

Command Register

Definition at line 52 of file efm32tg11b_rmu.h.

__IOM uint32_t RMU_TypeDef::CTRL

Control Register

Definition at line 50 of file efm32tg11b_rmu.h.

__IOM uint32_t RMU_TypeDef::LOCK

Configuration Lock Register

Definition at line 54 of file efm32tg11b_rmu.h.

__IOM uint32_t RMU_TypeDef::RST

Reset Control Register

Definition at line 53 of file efm32tg11b_rmu.h.

__IM uint32_t RMU_TypeDef::RSTCAUSE

Reset Cause Register

Definition at line 51 of file efm32tg11b_rmu.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/efm32tg11b_rmu.h