CSEN_TypeDef Struct ReferenceDevices > CSEN
CSEN Register Declaration
Definition at line 49
of file efm32tg11b_csen.h
.
#include <
efm32tg11b_csen.h
>
Data Fields | |
__IOM uint32_t | ANACTRL |
__IM uint32_t | APORTCONFLICT |
__IM uint32_t | APORTREQ |
__IOM uint32_t | CMD |
__IOM uint32_t | CMPTHR |
__IOM uint32_t | CTRL |
__IOM uint32_t | DATA |
__IOM uint32_t | DMBASELINE |
__IOM uint32_t | DMCFG |
__IOM uint32_t | EMA |
__IOM uint32_t | EMACTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | PRSSEL |
uint32_t | RESERVED0 [2] |
__IOM uint32_t | SCANINPUTSEL0 |
__IOM uint32_t | SCANINPUTSEL1 |
__IOM uint32_t | SCANMASK0 |
__IOM uint32_t | SCANMASK1 |
__IOM uint32_t | SINGLECTRL |
__IM uint32_t | STATUS |
__IOM uint32_t | TIMCTRL |
Field Documentation
__IOM uint32_t CSEN_TypeDef::ANACTRL |
Analog Control
Definition at line 68
of file efm32tg11b_csen.h
.
Referenced by CSEN_InitMode(), and CSEN_Reset().
__IM uint32_t CSEN_TypeDef::APORTCONFLICT |
APORT Request Conflict
Definition at line 61
of file efm32tg11b_csen.h
.
__IM uint32_t CSEN_TypeDef::APORTREQ |
APORT Request Status
Definition at line 60
of file efm32tg11b_csen.h
.
__IOM uint32_t CSEN_TypeDef::CMD |
__IOM uint32_t CSEN_TypeDef::CMPTHR |
Comparator Threshold
Definition at line 62
of file efm32tg11b_csen.h
.
Referenced by CSEN_InitMode(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::CTRL |
Control
Definition at line 50
of file efm32tg11b_csen.h
.
Referenced by CSEN_Disable(), CSEN_Enable(), CSEN_Init(), CSEN_InitMode(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::DATA |
Output Data
Definition at line 55
of file efm32tg11b_csen.h
.
Referenced by CSEN_DataGet(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::DMBASELINE |
Delta Modulation Baseline
Definition at line 66
of file efm32tg11b_csen.h
.
Referenced by CSEN_DMBaselineSet(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::DMCFG |
Delta Modulation Configuration
Definition at line 67
of file efm32tg11b_csen.h
.
Referenced by CSEN_InitMode(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::EMA |
Exponential Moving Average
Definition at line 63
of file efm32tg11b_csen.h
.
Referenced by CSEN_EMAGet(), CSEN_EMASet(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::EMACTRL |
Exponential Moving Average Control
Definition at line 64
of file efm32tg11b_csen.h
.
Referenced by CSEN_InitMode(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::IEN |
Interrupt Enable
Definition at line 74
of file efm32tg11b_csen.h
.
Referenced by CSEN_IntDisable(), CSEN_IntEnable(), CSEN_IntGetEnabled(), and CSEN_Reset().
__IM uint32_t CSEN_TypeDef::IF |
Interrupt Flag
Definition at line 71
of file efm32tg11b_csen.h
.
Referenced by CSEN_IntGet(), and CSEN_IntGetEnabled().
__IOM uint32_t CSEN_TypeDef::IFC |
Interrupt Flag Clear
Definition at line 73
of file efm32tg11b_csen.h
.
Referenced by CSEN_IntClear(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::IFS |
__IOM uint32_t CSEN_TypeDef::PRSSEL |
PRS Select
Definition at line 54
of file efm32tg11b_csen.h
.
Referenced by CSEN_Init(), and CSEN_Reset().
uint32_t CSEN_TypeDef::RESERVED0[2] |
Reserved for future use
Definition at line 70
of file efm32tg11b_csen.h
.
__IOM uint32_t CSEN_TypeDef::SCANINPUTSEL0 |
Scan Input Selection 0
Definition at line 57
of file efm32tg11b_csen.h
.
Referenced by CSEN_Init(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::SCANINPUTSEL1 |
Scan Input Selection 1
Definition at line 59
of file efm32tg11b_csen.h
.
Referenced by CSEN_Init(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::SCANMASK0 |
Scan Channel Mask 0
Definition at line 56
of file efm32tg11b_csen.h
.
Referenced by CSEN_InitMode(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::SCANMASK1 |
Scan Channel Mask 1
Definition at line 58
of file efm32tg11b_csen.h
.
Referenced by CSEN_InitMode(), and CSEN_Reset().
__IOM uint32_t CSEN_TypeDef::SINGLECTRL |
Single Conversion Control
Definition at line 65
of file efm32tg11b_csen.h
.
Referenced by CSEN_InitMode(), and CSEN_Reset().
__IM uint32_t CSEN_TypeDef::STATUS |
__IOM uint32_t CSEN_TypeDef::TIMCTRL |
Timing Control
Definition at line 51
of file efm32tg11b_csen.h
.
Referenced by CSEN_Init(), and CSEN_Reset().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/
efm32tg11b_csen.h