DEVINFO_TypeDef Struct ReferenceDevices > Device Information and Calibration

DEVINFO Register Declaration

Definition at line 49 of file efm32tg11b_devinfo.h .

#include < efm32tg11b_devinfo.h >

Data Fields

__IM uint32_t ADC0CAL0
__IM uint32_t ADC0CAL1
__IM uint32_t ADC0CAL2
__IM uint32_t ADC0CAL3
__IM uint32_t AUXHFRCOCAL0
__IM uint32_t AUXHFRCOCAL10
__IM uint32_t AUXHFRCOCAL11
__IM uint32_t AUXHFRCOCAL12
__IM uint32_t AUXHFRCOCAL13
__IM uint32_t AUXHFRCOCAL3
__IM uint32_t AUXHFRCOCAL6
__IM uint32_t AUXHFRCOCAL7
__IM uint32_t AUXHFRCOCAL8
__IM uint32_t CAL
__IM uint32_t CSENGAINCAL
__IM uint32_t CUSTOMINFO
__IM uint32_t DCDCLNVCTRL0
__IM uint32_t DCDCLPCMPHYSSEL0
__IM uint32_t DCDCLPCMPHYSSEL1
__IM uint32_t DCDCLPVCTRL0
__IM uint32_t DCDCLPVCTRL1
__IM uint32_t DCDCLPVCTRL2
__IM uint32_t DCDCLPVCTRL3
__IM uint32_t DEVINFOREV
__IM uint32_t EMUTEMP
__IM uint32_t HFRCOCAL0
__IM uint32_t HFRCOCAL10
__IM uint32_t HFRCOCAL11
__IM uint32_t HFRCOCAL12
__IM uint32_t HFRCOCAL13
__IM uint32_t HFRCOCAL3
__IM uint32_t HFRCOCAL6
__IM uint32_t HFRCOCAL7
__IM uint32_t HFRCOCAL8
__IM uint32_t MEMINFO
__IM uint32_t MSIZE
__IM uint32_t OPA0CAL0
__IM uint32_t OPA0CAL1
__IM uint32_t OPA0CAL2
__IM uint32_t OPA0CAL3
__IM uint32_t OPA0CAL4
__IM uint32_t OPA0CAL5
__IM uint32_t OPA0CAL6
__IM uint32_t OPA0CAL7
__IM uint32_t OPA1CAL0
__IM uint32_t OPA1CAL1
__IM uint32_t OPA1CAL2
__IM uint32_t OPA1CAL3
__IM uint32_t OPA1CAL4
__IM uint32_t OPA1CAL5
__IM uint32_t OPA1CAL6
__IM uint32_t OPA1CAL7
__IM uint32_t OPA2CAL0
__IM uint32_t OPA2CAL1
__IM uint32_t OPA2CAL2
__IM uint32_t OPA2CAL3
__IM uint32_t OPA2CAL4
__IM uint32_t OPA2CAL5
__IM uint32_t OPA2CAL6
__IM uint32_t OPA2CAL7
__IM uint32_t OPA3CAL0
__IM uint32_t OPA3CAL1
__IM uint32_t OPA3CAL2
__IM uint32_t OPA3CAL3
__IM uint32_t OPA3CAL4
__IM uint32_t OPA3CAL5
__IM uint32_t OPA3CAL6
__IM uint32_t OPA3CAL7
__IM uint32_t PART
uint32_t RESERVED0 [11]
uint32_t RESERVED1 [2]
uint32_t RESERVED10 [1]
uint32_t RESERVED11 [10]
uint32_t RESERVED12 [7]
uint32_t RESERVED2 [2]
uint32_t RESERVED3 [4]
uint32_t RESERVED4 [2]
uint32_t RESERVED5 [2]
uint32_t RESERVED6 [1]
uint32_t RESERVED7 [10]
uint32_t RESERVED8 [2]
uint32_t RESERVED9 [2]
__IM uint32_t UNIQUEH
__IM uint32_t UNIQUEL
__IM uint32_t VDAC0ALTCAL
__IM uint32_t VDAC0CH1CAL
__IM uint32_t VDAC0MAINCAL
__IM uint32_t VMONCAL0
__IM uint32_t VMONCAL1
__IM uint32_t VMONCAL2

Field Documentation

__IM uint32_t DEVINFO_TypeDef::ADC0CAL0

ADC0 calibration register 0

Definition at line 62 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::ADC0CAL1

ADC0 calibration register 1

Definition at line 63 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::ADC0CAL2

ADC0 calibration register 2

Definition at line 64 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::ADC0CAL3

ADC0 calibration register 3

Definition at line 65 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL0

AUXHFRCO Calibration Register (4 MHz)

Definition at line 80 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL10

AUXHFRCO Calibration Register (26 MHz)

Definition at line 88 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL11

AUXHFRCO Calibration Register (32 MHz)

Definition at line 89 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL12

AUXHFRCO Calibration Register (38 MHz)

Definition at line 90 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL13

AUXHFRCO Calibration Register (48 MHz)

Definition at line 91 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL3

AUXHFRCO Calibration Register (7 MHz)

Definition at line 82 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL6

AUXHFRCO Calibration Register (13 MHz)

Definition at line 84 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL7

AUXHFRCO Calibration Register (16 MHz)

Definition at line 85 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL8

AUXHFRCO Calibration Register (19 MHz)

Definition at line 86 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::CAL

CRC of DI-page and calibration temperature

Definition at line 50 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::CSENGAINCAL

Cap Sense Gain Adjustment

Definition at line 139 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::CUSTOMINFO

Custom information

Definition at line 52 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DCDCLNVCTRL0

DCDC Low-noise VREF Trim Register 0

Definition at line 97 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DCDCLPCMPHYSSEL0

DCDC LPCMPHYSSEL Trim Register 0

Definition at line 102 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DCDCLPCMPHYSSEL1

DCDC LPCMPHYSSEL Trim Register 1

Definition at line 103 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DCDCLPVCTRL0

DCDC Low-power VREF Trim Register 0

Definition at line 98 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DCDCLPVCTRL1

DCDC Low-power VREF Trim Register 1

Definition at line 99 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DCDCLPVCTRL2

DCDC Low-power VREF Trim Register 2

Definition at line 100 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DCDCLPVCTRL3

DCDC Low-power VREF Trim Register 3

Definition at line 101 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DEVINFOREV

Device information page revision

Definition at line 59 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::EMUTEMP

EMU Temperature Calibration Information

Definition at line 60 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL0

HFRCO Calibration Register (4 MHz)

Definition at line 67 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL10

HFRCO Calibration Register (26 MHz)

Definition at line 75 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL11

HFRCO Calibration Register (32 MHz)

Definition at line 76 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL12

HFRCO Calibration Register (38 MHz)

Definition at line 77 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL13

HFRCO Calibration Register (48 MHz)

Definition at line 78 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL3

HFRCO Calibration Register (7 MHz)

Definition at line 69 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL6

HFRCO Calibration Register (13 MHz)

Definition at line 71 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL7

HFRCO Calibration Register (16 MHz)

Definition at line 72 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL8

HFRCO Calibration Register (19 MHz)

Definition at line 73 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::MEMINFO

Flash page size and misc. chip information

Definition at line 53 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::MSIZE

Flash and SRAM Memory size in kB

Definition at line 57 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA0CAL0

OPA0 Calibration Register for DRIVESTRENGTH 0, INCBW=1

Definition at line 107 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA0CAL1

OPA0 Calibration Register for DRIVESTRENGTH 1, INCBW=1

Definition at line 108 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA0CAL2

OPA0 Calibration Register for DRIVESTRENGTH 2, INCBW=1

Definition at line 109 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA0CAL3

OPA0 Calibration Register for DRIVESTRENGTH 3, INCBW=1

Definition at line 110 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA0CAL4

OPA0 Calibration Register for DRIVESTRENGTH 0, INCBW=0

Definition at line 111 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA0CAL5

OPA0 Calibration Register for DRIVESTRENGTH 1, INCBW=0

Definition at line 112 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA0CAL6

OPA0 Calibration Register for DRIVESTRENGTH 2, INCBW=0

Definition at line 113 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA0CAL7

OPA0 Calibration Register for DRIVESTRENGTH 3, INCBW=0

Definition at line 114 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA1CAL0

OPA1 Calibration Register for DRIVESTRENGTH 0, INCBW=1

Definition at line 115 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA1CAL1

OPA1 Calibration Register for DRIVESTRENGTH 1, INCBW=1

Definition at line 116 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA1CAL2

OPA1 Calibration Register for DRIVESTRENGTH 2, INCBW=1

Definition at line 117 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA1CAL3

OPA1 Calibration Register for DRIVESTRENGTH 3, INCBW=1

Definition at line 118 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA1CAL4

OPA1 Calibration Register for DRIVESTRENGTH 0, INCBW=0

Definition at line 119 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA1CAL5

OPA1 Calibration Register for DRIVESTRENGTH 1, INCBW=0

Definition at line 120 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA1CAL6

OPA1 Calibration Register for DRIVESTRENGTH 2, INCBW=0

Definition at line 121 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA1CAL7

OPA1 Calibration Register for DRIVESTRENGTH 3, INCBW=0

Definition at line 122 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA2CAL0

OPA2 Calibration Register for DRIVESTRENGTH 0, INCBW=1

Definition at line 123 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA2CAL1

OPA2 Calibration Register for DRIVESTRENGTH 1, INCBW=1

Definition at line 124 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA2CAL2

OPA2 Calibration Register for DRIVESTRENGTH 2, INCBW=1

Definition at line 125 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA2CAL3

OPA2 Calibration Register for DRIVESTRENGTH 3, INCBW=1

Definition at line 126 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA2CAL4

OPA2 Calibration Register for DRIVESTRENGTH 0, INCBW=0

Definition at line 127 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA2CAL5

OPA2 Calibration Register for DRIVESTRENGTH 1, INCBW=0

Definition at line 128 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA2CAL6

OPA2 Calibration Register for DRIVESTRENGTH 2, INCBW=0

Definition at line 129 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA2CAL7

OPA2 Calibration Register for DRIVESTRENGTH 3, INCBW=0

Definition at line 130 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA3CAL0

OPA3 Calibration Register for DRIVESTRENGTH 0, INCBW=1

Definition at line 131 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA3CAL1

OPA3 Calibration Register for DRIVESTRENGTH 1, INCBW=1

Definition at line 132 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA3CAL2

OPA3 Calibration Register for DRIVESTRENGTH 2, INCBW=1

Definition at line 133 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA3CAL3

OPA3 Calibration Register for DRIVESTRENGTH 3, INCBW=1

Definition at line 134 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA3CAL4

OPA3 Calibration Register for DRIVESTRENGTH 0, INCBW=0

Definition at line 135 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA3CAL5

OPA3 Calibration Register for DRIVESTRENGTH 1, INCBW=0

Definition at line 136 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA3CAL6

OPA3 Calibration Register for DRIVESTRENGTH 2, INCBW=0

Definition at line 137 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::OPA3CAL7

OPA3 Calibration Register for DRIVESTRENGTH 3, INCBW=0

Definition at line 138 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::PART

Part description

Definition at line 58 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED0[11]

Reserved for future use

Definition at line 51 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED1[2]

Reserved for future use

Definition at line 54 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED10[1]

Reserved for future use

Definition at line 87 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED11[10]

Reserved for future use

Definition at line 92 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED12[7]

Reserved for future use

Definition at line 96 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED2[2]

Reserved for future use

Definition at line 61 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED3[4]

Reserved for future use

Definition at line 66 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED4[2]

Reserved for future use

Definition at line 68 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED5[2]

Reserved for future use

Definition at line 70 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED6[1]

Reserved for future use

Definition at line 74 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED7[10]

Reserved for future use

Definition at line 79 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED8[2]

Reserved for future use

Definition at line 81 of file efm32tg11b_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED9[2]

Reserved for future use

Definition at line 83 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::UNIQUEH

High 32 bits of device unique number

Definition at line 56 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::UNIQUEL

Low 32 bits of device unique number

Definition at line 55 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::VDAC0ALTCAL

VDAC0 Cals for Alternate Path

Definition at line 105 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::VDAC0CH1CAL

VDAC0 CH1 Error Cal

Definition at line 106 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::VDAC0MAINCAL

VDAC0 Cals for Main Path

Definition at line 104 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::VMONCAL0

VMON Calibration Register 0

Definition at line 93 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::VMONCAL1

VMON Calibration Register 1

Definition at line 94 of file efm32tg11b_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::VMONCAL2

VMON Calibration Register 2

Definition at line 95 of file efm32tg11b_devinfo.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/ efm32tg11b_devinfo.h