MSC_TypeDef Struct ReferenceDevices > MSC
MSC Register Declaration
Definition at line 49
of file efm32tg11b_msc.h
.
#include <
efm32tg11b_msc.h
>
Data Fields | |
__IOM uint32_t | AAPUNLOCKCMD |
__IOM uint32_t | ADDRB |
__IOM uint32_t | BOOTLOADERCTRL |
__IOM uint32_t | CACHECMD |
__IOM uint32_t | CACHECONFIG0 |
__IM uint32_t | CACHEHITS |
__IM uint32_t | CACHEMISSES |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | IRQLATENCY |
__IOM uint32_t | LOCK |
__IOM uint32_t | MASSLOCK |
__IOM uint32_t | READCTRL |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [4] |
uint32_t | RESERVED2 [1] |
uint32_t | RESERVED3 [5] |
uint32_t | RESERVED4 [6] |
__IOM uint32_t | STARTUP |
__IM uint32_t | STATUS |
__IOM uint32_t | WDATA |
__IOM uint32_t | WRITECMD |
__IOM uint32_t | WRITECTRL |
Field Documentation
__IOM uint32_t MSC_TypeDef::AAPUNLOCKCMD |
Software Unlock AAP Command Register
Definition at line 79
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::ADDRB |
Page Erase/Write Address Buffer
Definition at line 54
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::BOOTLOADERCTRL |
Bootloader Read and Write Enable, Write Once Register
Definition at line 78
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::CACHECMD |
Flash Cache Command Register
Definition at line 65
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::CACHECONFIG0 |
Cache Configuration Register 0
Definition at line 80
of file efm32tg11b_msc.h
.
__IM uint32_t MSC_TypeDef::CACHEHITS |
Cache Hits Performance Counter
Definition at line 66
of file efm32tg11b_msc.h
.
__IM uint32_t MSC_TypeDef::CACHEMISSES |
Cache Misses Performance Counter
Definition at line 67
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::CMD |
Command Register
Definition at line 75
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::CTRL |
Memory System Control Register
Definition at line 50
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 63
of file efm32tg11b_msc.h
.
__IM uint32_t MSC_TypeDef::IF |
Interrupt Flag Register
Definition at line 60
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 62
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 61
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::IRQLATENCY |
Irq Latency Register
Definition at line 71
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::LOCK |
Configuration Lock Register
Definition at line 64
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::MASSLOCK |
Mass Erase Lock Register
Definition at line 70
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::READCTRL |
Read Control Register
Definition at line 51
of file efm32tg11b_msc.h
.
uint32_t MSC_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 55
of file efm32tg11b_msc.h
.
uint32_t MSC_TypeDef::RESERVED1[4] |
Reserved for future use
Definition at line 59
of file efm32tg11b_msc.h
.
uint32_t MSC_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 69
of file efm32tg11b_msc.h
.
uint32_t MSC_TypeDef::RESERVED3[5] |
Reserved for future use
Definition at line 74
of file efm32tg11b_msc.h
.
uint32_t MSC_TypeDef::RESERVED4[6] |
Reserved for future use
Definition at line 77
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::STARTUP |
Startup Control
Definition at line 72
of file efm32tg11b_msc.h
.
__IM uint32_t MSC_TypeDef::STATUS |
Status Register
Definition at line 57
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::WDATA |
Write Data Register
Definition at line 56
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::WRITECMD |
Write Command Register
Definition at line 53
of file efm32tg11b_msc.h
.
__IOM uint32_t MSC_TypeDef::WRITECTRL |
Write Control Register
Definition at line 52
of file efm32tg11b_msc.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/
efm32tg11b_msc.h