CAN_MIR_TypeDef Struct ReferenceDevicesDevices > | CAN
CAN_MIR CAN MIR Register
.
Definition at line 47
of file efm32tg11b_can_mir.h
.
#include <
efm32tg11b_can_mir.h
>
Data Fields | |
__IOM uint32_t | ARB |
__IOM uint32_t | CMDMASK |
__IOM uint32_t | CMDREQ |
__IOM uint32_t | CTRL |
__IOM uint32_t | DATAH |
__IOM uint32_t | DATAL |
__IOM uint32_t | MASK |
uint32_t | RESERVED0 [1] |
Field Documentation
__IOM uint32_t CAN_MIR_TypeDef::ARB |
Interface Arbitration Register
Definition at line 50
of file efm32tg11b_can_mir.h
.
Referenced by CAN_AbortSendMessage(), CAN_ConfigureMessageObject(), CAN_Reset(), CAN_ResetMessages(), CAN_SendMessage(), and CAN_SetIdAndFilter().
__IOM uint32_t CAN_MIR_TypeDef::CMDMASK |
Interface Command Mask Register
Definition at line 48
of file efm32tg11b_can_mir.h
.
Referenced by CAN_AbortSendMessage(), CAN_ConfigureMessageObject(), CAN_MessageLost(), CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), CAN_SendMessage(), and CAN_SetIdAndFilter().
__IOM uint32_t CAN_MIR_TypeDef::CMDREQ |
Interface Command Request Register
Definition at line 54
of file efm32tg11b_can_mir.h
.
Referenced by CAN_ReadyWait(), CAN_Reset(), and CAN_SendRequest().
__IOM uint32_t CAN_MIR_TypeDef::CTRL |
Interface Message Control Register
Definition at line 51
of file efm32tg11b_can_mir.h
.
Referenced by CAN_ConfigureMessageObject(), CAN_MessageLost(), CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), CAN_SendMessage(), and CAN_SetIdAndFilter().
__IOM uint32_t CAN_MIR_TypeDef::DATAH |
Interface Data B Register
Definition at line 53
of file efm32tg11b_can_mir.h
.
Referenced by CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), and CAN_WriteData().
__IOM uint32_t CAN_MIR_TypeDef::DATAL |
Interface Data a Register
Definition at line 52
of file efm32tg11b_can_mir.h
.
Referenced by CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), and CAN_WriteData().
__IOM uint32_t CAN_MIR_TypeDef::MASK |
Interface Mask Register
Definition at line 49
of file efm32tg11b_can_mir.h
.
Referenced by CAN_Reset(), CAN_ResetMessages(), and CAN_SetIdAndFilter().
uint32_t CAN_MIR_TypeDef::RESERVED0[1] |
Reserved future
Definition at line 55
of file efm32tg11b_can_mir.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/
efm32tg11b_can_mir.h