LCD_TypeDef Struct ReferenceDevices > LCD
LCD Register Declaration
Definition at line 49
of file efm32tg11b_lcd.h
.
#include <
efm32tg11b_lcd.h
>
Data Fields | |
__IOM uint32_t | AREGA |
__IOM uint32_t | AREGB |
__IOM uint32_t | BACTRL |
__IOM uint32_t | BIASCTRL |
__IOM uint32_t | CTRL |
__IOM uint32_t | DISPCTRL |
__IOM uint32_t | FRAMERATE |
__IOM uint32_t | FREEZE |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [3] |
uint32_t | RESERVED2 [16] |
uint32_t | RESERVED3 [10] |
__IOM uint32_t | SEGD0H |
__IOM uint32_t | SEGD0L |
__IOM uint32_t | SEGD1H |
__IOM uint32_t | SEGD1L |
__IOM uint32_t | SEGD2H |
__IOM uint32_t | SEGD2L |
__IOM uint32_t | SEGD3H |
__IOM uint32_t | SEGD3L |
__IOM uint32_t | SEGD4H |
__IOM uint32_t | SEGD4L |
__IOM uint32_t | SEGD5H |
__IOM uint32_t | SEGD5L |
__IOM uint32_t | SEGD6H |
__IOM uint32_t | SEGD6L |
__IOM uint32_t | SEGD7H |
__IOM uint32_t | SEGD7L |
__IOM uint32_t | SEGEN |
__IOM uint32_t | SEGEN2 |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
Field Documentation
__IOM uint32_t LCD_TypeDef::AREGA |
Animation Register a
Definition at line 55
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::AREGB |
Animation Register B
Definition at line 56
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::BACTRL |
Blink and Animation Control Register
Definition at line 53
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::BIASCTRL |
Analog BIAS Control
Definition at line 63
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::CTRL |
Control Register
Definition at line 50
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::DISPCTRL |
Display Control Register
Definition at line 51
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::FRAMERATE |
Frame Rate
Definition at line 86
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::FREEZE |
Freeze Register
Definition at line 83
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::IEN |
Interrupt Enable Register
Definition at line 60
of file efm32tg11b_lcd.h
.
__IM uint32_t LCD_TypeDef::IF |
Interrupt Flag Register
Definition at line 57
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 59
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 58
of file efm32tg11b_lcd.h
.
uint32_t LCD_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 62
of file efm32tg11b_lcd.h
.
uint32_t LCD_TypeDef::RESERVED1[3] |
Reserved for future use
Definition at line 65
of file efm32tg11b_lcd.h
.
uint32_t LCD_TypeDef::RESERVED2[16] |
Reserved for future use
Definition at line 82
of file efm32tg11b_lcd.h
.
uint32_t LCD_TypeDef::RESERVED3[10] |
Reserved for future use
Definition at line 85
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD0H |
Segment Data High Register 0
Definition at line 70
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD0L |
Segment Data Low Register 0
Definition at line 66
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD1H |
Segment Data High Register 1
Definition at line 71
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD1L |
Segment Data Low Register 1
Definition at line 67
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD2H |
Segment Data High Register 2
Definition at line 72
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD2L |
Segment Data Low Register 2
Definition at line 68
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD3H |
Segment Data High Register 3
Definition at line 73
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD3L |
Segment Data Low Register 3
Definition at line 69
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD4H |
Segment Data High Register 4
Definition at line 78
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD4L |
Segment Data Low Register 4
Definition at line 74
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD5H |
Segment Data High Register 5
Definition at line 79
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD5L |
Segment Data Low Register 5
Definition at line 75
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD6H |
Segment Data High Register 6
Definition at line 80
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD6L |
Segment Data Low Register 6
Definition at line 76
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD7H |
Segment Data High Register 7
Definition at line 81
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGD7L |
Segment Data Low Register 7
Definition at line 77
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGEN |
Segment Enable Register
Definition at line 52
of file efm32tg11b_lcd.h
.
__IOM uint32_t LCD_TypeDef::SEGEN2 |
Segment Enable (32 to 39)
Definition at line 87
of file efm32tg11b_lcd.h
.
__IM uint32_t LCD_TypeDef::STATUS |
Status Register
Definition at line 54
of file efm32tg11b_lcd.h
.
__IM uint32_t LCD_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 84
of file efm32tg11b_lcd.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/
efm32tg11b_lcd.h