EMU_TypeDef Struct ReferenceDevices > EMU
EMU Register Declaration
Definition at line 49
of file efm32tg11b_emu.h
.
#include <
efm32tg11b_emu.h
>
Data Fields | |
__IOM uint32_t | BUCTRL |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | DCDCCLIMCTRL |
__IOM uint32_t | DCDCCTRL |
__IOM uint32_t | DCDCLNCOMPCTRL |
__IOM uint32_t | DCDCLNFREQCTRL |
__IOM uint32_t | DCDCLNVCTRL |
__IOM uint32_t | DCDCLPCTRL |
__IOM uint32_t | DCDCLPEM01CFG |
__IOM uint32_t | DCDCLPVCTRL |
__IOM uint32_t | DCDCMISCCTRL |
__IM uint32_t | DCDCSYNC |
__IOM uint32_t | DCDCZDETCTRL |
__IOM uint32_t | EM23PERNORETAINCMD |
__IOM uint32_t | EM23PERNORETAINCTRL |
__IM uint32_t | EM23PERNORETAINSTATUS |
__IOM uint32_t | EM4CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | LOCK |
__IOM uint32_t | PWRCTRL |
__IOM uint32_t | PWRLOCK |
__IOM uint32_t | RAM0CTRL |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [1] |
uint32_t | RESERVED10 [4] |
uint32_t | RESERVED2 [2] |
uint32_t | RESERVED3 [1] |
uint32_t | RESERVED4 [1] |
uint32_t | RESERVED5 [1] |
uint32_t | RESERVED6 [5] |
uint32_t | RESERVED7 [1] |
uint32_t | RESERVED8 [5] |
uint32_t | RESERVED9 [11] |
__IM uint32_t | STATUS |
__IM uint32_t | TEMP |
__IOM uint32_t | TEMPLIMITS |
__IOM uint32_t | VMONALTAVDDCTRL |
__IOM uint32_t | VMONAVDDCTRL |
__IOM uint32_t | VMONBUVDDCTRL |
__IOM uint32_t | VMONDVDDCTRL |
__IOM uint32_t | VMONIO0CTRL |
Field Documentation
__IOM uint32_t EMU_TypeDef::BUCTRL |
Backup Power Configuration Register
Definition at line 97
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::CMD |
Command Register
Definition at line 54
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::CTRL |
Control Register
Definition at line 50
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCCLIMCTRL |
DCDC Power Train PFET Current Limiter Control Register
Definition at line 73
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCCTRL |
DCDC Control
Definition at line 68
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCLNCOMPCTRL |
DCDC Low Noise Compensator Control Register
Definition at line 74
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCLNFREQCTRL |
DCDC Low Noise Controller Frequency Control
Definition at line 82
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCLNVCTRL |
DCDC Low Noise Voltage Register
Definition at line 75
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCLPCTRL |
DCDC Low Power Control Register
Definition at line 81
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCLPEM01CFG |
Configuration Bits for Low Power Mode to Be Applied During EM01, This Field is Only Relevant If LP Mode is Used in EM01
Definition at line 100
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCLPVCTRL |
DCDC Low Power Voltage Register
Definition at line 78
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCMISCCTRL |
DCDC Miscellaneous Control Register
Definition at line 71
of file efm32tg11b_emu.h
.
__IM uint32_t EMU_TypeDef::DCDCSYNC |
DCDC Read Status Register
Definition at line 85
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::DCDCZDETCTRL |
DCDC Power Train NFET Zero Current Detector Control Register
Definition at line 72
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::EM23PERNORETAINCMD |
Clears Corresponding Bits in EM23PERNORETAINSTATUS Unlocking Access to Peripheral
Definition at line 103
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::EM23PERNORETAINCTRL |
When Set Corresponding Peripherals May Get Powered Down in EM23
Definition at line 105
of file efm32tg11b_emu.h
.
__IM uint32_t EMU_TypeDef::EM23PERNORETAINSTATUS |
Status Indicating If Peripherals Were Powered Down in EM23, Subsequently Locking Access to It
Definition at line 104
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::EM4CTRL |
EM4 Control Register
Definition at line 57
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line 63
of file efm32tg11b_emu.h
.
__IM uint32_t EMU_TypeDef::IF |
Interrupt Flag Register
Definition at line 60
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 62
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 61
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line 52
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::PWRCTRL |
Power Control Register
Definition at line 67
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::PWRLOCK |
Regulator and Supply Lock Register
Definition at line 64
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::RAM0CTRL |
Memory Control Register
Definition at line 53
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 56
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED1[1] |
Reserved for future use
Definition at line 66
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED10[4] |
Reserved for future use
Definition at line 102
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED2[2] |
Reserved for future use
Definition at line 70
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED3[1] |
Reserved for future use
Definition at line 77
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED4[1] |
Reserved for future use
Definition at line 80
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED5[1] |
Reserved for future use
Definition at line 84
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED6[5] |
Reserved for future use
Definition at line 87
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED7[1] |
Reserved for future use
Definition at line 93
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED8[5] |
Reserved for future use
Definition at line 96
of file efm32tg11b_emu.h
.
uint32_t EMU_TypeDef::RESERVED9[11] |
Reserved for future use
Definition at line 99
of file efm32tg11b_emu.h
.
__IM uint32_t EMU_TypeDef::STATUS |
Status Register
Definition at line 51
of file efm32tg11b_emu.h
.
__IM uint32_t EMU_TypeDef::TEMP |
Value of Last Temperature Measurement
Definition at line 59
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::TEMPLIMITS |
Temperature Limits for Interrupt Generation
Definition at line 58
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::VMONALTAVDDCTRL |
Alternate VMON AVDD Channel Control
Definition at line 89
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::VMONAVDDCTRL |
VMON AVDD Channel Control
Definition at line 88
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::VMONBUVDDCTRL |
VMON BUVDD Channel Control
Definition at line 94
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::VMONDVDDCTRL |
VMON DVDD Channel Control
Definition at line 90
of file efm32tg11b_emu.h
.
__IOM uint32_t EMU_TypeDef::VMONIO0CTRL |
VMON IOVDD0 Channel Control
Definition at line 91
of file efm32tg11b_emu.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/
efm32tg11b_emu.h