WDOG_PCH_TypeDef Struct ReferenceDevicesDevices > | WDOG

WDOG_PCH WDOG PCH Register


      

.

Definition at line 47 of file efm32tg11b_wdog_pch.h .

#include < efm32tg11b_wdog_pch.h >

Data Fields

__IOM uint32_t PRSCTRL

Field Documentation

__IOM uint32_t WDOG_PCH_TypeDef::PRSCTRL

PRS Control Register

Definition at line 48 of file efm32tg11b_wdog_pch.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/ efm32tg11b_wdog_pch.h