LEUART_TypeDef Struct ReferenceDevices > LEUART
LEUART Register Declaration
Definition at line 49
of file efm32tg11b_leuart.h
.
#include <
efm32tg11b_leuart.h
>
Data Fields | |
__IOM uint32_t | CLKDIV |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | FREEZE |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | INPUT |
__IOM uint32_t | PULSECTRL |
uint32_t | RESERVED0 [3] |
uint32_t | RESERVED1 [2] |
__IOM uint32_t | ROUTELOC0 |
__IOM uint32_t | ROUTEPEN |
__IM uint32_t | RXDATA |
__IM uint32_t | RXDATAX |
__IM uint32_t | RXDATAXP |
__IOM uint32_t | SIGFRAME |
__IOM uint32_t | STARTFRAME |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
__IOM uint32_t | TXDATA |
__IOM uint32_t | TXDATAX |
Field Documentation
__IOM uint32_t LEUART_TypeDef::CLKDIV |
Clock Control Register
Definition at line 53
of file efm32tg11b_leuart.h
.
Referenced by LEUART_BaudrateGet(), LEUART_BaudrateSet(), and LEUART_Reset().
__IOM uint32_t LEUART_TypeDef::CMD |
Command Register
Definition at line 51
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Enable(), LEUART_Init(), LEUART_Reset(), LEUART_RxDmaInEM2Enable(), LEUART_TxDmaInEM2Enable(), and UARTDRV_InitLeuart().
__IOM uint32_t LEUART_TypeDef::CTRL |
Control Register
Definition at line 50
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Init(), LEUART_Reset(), LEUART_RxDmaInEM2Enable(), and LEUART_TxDmaInEM2Enable().
__IOM uint32_t LEUART_TypeDef::FREEZE |
Freeze Register
Definition at line 67
of file efm32tg11b_leuart.h
.
Referenced by LEUART_FreezeEnable().
__IOM uint32_t LEUART_TypeDef::IEN |
Interrupt Enable Register
Definition at line 64
of file efm32tg11b_leuart.h
.
Referenced by LEUART_IntDisable(), LEUART_IntEnable(), LEUART_IntGetEnabled(), and LEUART_Reset().
__IM uint32_t LEUART_TypeDef::IF |
Interrupt Flag Register
Definition at line 61
of file efm32tg11b_leuart.h
.
Referenced by LEUART_IntGet(), and LEUART_IntGetEnabled().
__IOM uint32_t LEUART_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 63
of file efm32tg11b_leuart.h
.
Referenced by LEUART_IntClear(), and LEUART_Reset().
__IOM uint32_t LEUART_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 62
of file efm32tg11b_leuart.h
.
Referenced by LEUART_IntSet().
__IOM uint32_t LEUART_TypeDef::INPUT |
LEUART Input Register
Definition at line 74
of file efm32tg11b_leuart.h
.
__IOM uint32_t LEUART_TypeDef::PULSECTRL |
Pulse Control Register
Definition at line 65
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Reset().
uint32_t LEUART_TypeDef::RESERVED0[3] |
Reserved for future use
Definition at line 70
of file efm32tg11b_leuart.h
.
uint32_t LEUART_TypeDef::RESERVED1[2] |
Reserved for future use
Definition at line 73
of file efm32tg11b_leuart.h
.
__IOM uint32_t LEUART_TypeDef::ROUTELOC0 |
I/O Routing Location Register
Definition at line 72
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Reset(), RETARGET_SerialInit(), and UARTDRV_InitLeuart().
__IOM uint32_t LEUART_TypeDef::ROUTEPEN |
I/O Routing Pin Enable Register
Definition at line 71
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Reset(), RETARGET_SerialInit(), and UARTDRV_InitLeuart().
__IM uint32_t LEUART_TypeDef::RXDATA |
Receive Buffer Data Register
Definition at line 57
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Rx(), and LEUART_RxDataGet().
__IM uint32_t LEUART_TypeDef::RXDATAX |
Receive Buffer Data Extended Register
Definition at line 56
of file efm32tg11b_leuart.h
.
Referenced by LEUART_RxDataXGet(), and LEUART_RxExt().
__IM uint32_t LEUART_TypeDef::RXDATAXP |
Receive Buffer Data Extended Peek Register
Definition at line 58
of file efm32tg11b_leuart.h
.
__IOM uint32_t LEUART_TypeDef::SIGFRAME |
Signal Frame Register
Definition at line 55
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Reset().
__IOM uint32_t LEUART_TypeDef::STARTFRAME |
Start Frame Register
Definition at line 54
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Reset().
__IM uint32_t LEUART_TypeDef::STATUS |
Status Register
Definition at line 52
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Rx(), LEUART_RxDmaInEM2Enable(), LEUART_RxExt(), LEUART_StatusGet(), LEUART_Tx(), LEUART_TxDmaInEM2Enable(), and LEUART_TxExt().
__IM uint32_t LEUART_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 68
of file efm32tg11b_leuart.h
.
Referenced by LEUART_FreezeEnable(), and UARTDRV_InitLeuart().
__IOM uint32_t LEUART_TypeDef::TXDATA |
Transmit Buffer Data Register
Definition at line 60
of file efm32tg11b_leuart.h
.
Referenced by LEUART_Tx().
__IOM uint32_t LEUART_TypeDef::TXDATAX |
Transmit Buffer Data Extended Register
Definition at line 59
of file efm32tg11b_leuart.h
.
Referenced by LEUART_TxExt().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG11B/Include/
efm32tg11b_leuart.h