ADC_InitScan_TypeDef Struct ReferenceEMLIB > ADC
Scan sequence init structure.
Definition at line 862
of file em_adc.h
.
#include <
em_adc.h
>
Data Fields | |
ADC_AcqTime_TypeDef | acqTime |
bool | diff |
uint32_t | input |
bool | leftAdjust |
bool | prsEnable |
ADC_PRSSEL_TypeDef | prsSel |
ADC_Ref_TypeDef | reference |
bool | rep |
ADC_Res_TypeDef | resolution |
Field Documentation
ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
Definition at line 870
of file em_adc.h
.
Referenced by ADC_InitScan().
bool ADC_InitScan_TypeDef::diff |
Select if single ended or differential input.
Definition at line 900
of file em_adc.h
.
Referenced by ADC_InitScan().
uint32_t ADC_InitScan_TypeDef::input |
Scan input selection. If single ended (diff
is false), use logical combination of ADC_SCANCTRL_INPUTMASK_CHx defines. If differential input (diff
is true), use logical combination of ADC_SCANCTRL_INPUTMASK_CHxCHy defines. (Notice underscore prefix for defines used.)
Definition at line 888
of file em_adc.h
.
Referenced by ADC_InitScan().
bool ADC_InitScan_TypeDef::leftAdjust |
Select if left adjustment should be done.
Definition at line 906
of file em_adc.h
.
Referenced by ADC_InitScan().
bool ADC_InitScan_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
Definition at line 903
of file em_adc.h
.
Referenced by ADC_InitScan(), and MIC_init().
ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if prsEnable
is enabled.
Definition at line 867
of file em_adc.h
.
Referenced by ADC_InitScan(), and MIC_init().
ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference |
Sample reference selection. Notice that for external references, the ADC calibration register must be set explicitly.
Definition at line 876
of file em_adc.h
.
Referenced by ADC_InitScan(), and MIC_init().
bool ADC_InitScan_TypeDef::rep |
Select if continuous conversion until explicit stop.
Definition at line 909
of file em_adc.h
.
Referenced by ADC_InitScan().
ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_adc.h