USBD_Init_TypeDef Struct ReferencePlatform Middleware > USB > USB_DEVICE
USB Device stack initialization structure.
This structure is passed to USBD_Init() when starting up the device.
Definition at line 756
of file em_usb.h
.
#include <
em_usb.h
>
Data Fields | |
const uint8_t * | bufferingMultiplier |
USBD_Callbacks_TypeDef_Pointer | callbacks |
const uint8_t * | configDescriptor |
const USB_DeviceDescriptor_TypeDef * | deviceDescriptor |
const uint8_t | numberOfStrings |
const uint32_t | reserved |
const void *const * | stringDescriptors |
Field Documentation
const uint8_t* USBD_Init_TypeDef::bufferingMultiplier |
Pointer to an array defining the size of the endpoint buffers. The size is given in multiples of endpoint size. Generally a value of 1 (single) or 2 (double) buffering should be used.
Definition at line 761
of file em_usb.h
.
Referenced by USBD_Init().
USBD_Callbacks_TypeDef_Pointer USBD_Init_TypeDef::callbacks |
Pointer to struct with callbacks (USBD_Callbacks_TypeDef). These callbacks are used by the device stack to signal events to or query the application.
Definition at line 766
of file em_usb.h
.
Referenced by USBD_Init().
const uint8_t* USBD_Init_TypeDef::configDescriptor |
Pointer to a configuration descriptor.
Definition at line 758
of file em_usb.h
.
Referenced by USBD_Init().
const USB_DeviceDescriptor_TypeDef* USBD_Init_TypeDef::deviceDescriptor |
Pointer to a device descriptor.
Definition at line 757
of file em_usb.h
.
Referenced by USBD_Init(), and USBX_init().
const uint8_t USBD_Init_TypeDef::numberOfStrings |
Number of strings in string descriptor array.
Definition at line 760
of file em_usb.h
.
Referenced by USBD_Init().
const uint32_t USBD_Init_TypeDef::reserved |
Reserved for future use.
Definition at line 770
of file em_usb.h
.
const void* const* USBD_Init_TypeDef::stringDescriptors |
Pointer to an array of string descriptor pointers.
Definition at line 759
of file em_usb.h
.
Referenced by USBD_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
em_usb.h