BURTC_TypeDef Struct ReferenceDevices > EZR32LG_BURTC
Definition at line 48
of file ezr32lg_burtc.h
.
Data Fields | |
__IOM uint32_t | CMD |
__IM uint32_t | CNT |
__IOM uint32_t | COMP0 |
__IOM uint32_t | CTRL |
__IOM uint32_t | FREEZE |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | LFXOFDET |
__IOM uint32_t | LOCK |
__IOM uint32_t | LPMODE |
__IOM uint32_t | POWERDOWN |
uint32_t | RESERVED0 [48] |
BURTC_RET_TypeDef | RET [128] |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
__IM uint32_t | TIMESTAMP |
Field Documentation
__IOM uint32_t BURTC_TypeDef::CMD |
Command Register
Definition at line 56
of file ezr32lg_burtc.h
.
__IM uint32_t BURTC_TypeDef::CNT |
Counter Value Register
Definition at line 51
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::COMP0 |
Counter Compare Value
Definition at line 52
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::CTRL |
Control Register
Definition at line 49
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::FREEZE |
Freeze Register
Definition at line 64
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 62
of file ezr32lg_burtc.h
.
__IM uint32_t BURTC_TypeDef::IF |
Interrupt Flag Register
Definition at line 59
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 61
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 60
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::LFXOFDET |
LFXO
Definition at line 54
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::LOCK |
Configuration Lock Register
Definition at line 58
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::LPMODE |
Low power mode configuration
Definition at line 50
of file ezr32lg_burtc.h
.
__IOM uint32_t BURTC_TypeDef::POWERDOWN |
Retention RAM power-down Register
Definition at line 57
of file ezr32lg_burtc.h
.
uint32_t BURTC_TypeDef::RESERVED0[48] |
Reserved registers
Definition at line 67
of file ezr32lg_burtc.h
.
BURTC_RET_TypeDef BURTC_TypeDef::RET[128] |
RetentionReg
Definition at line 68
of file ezr32lg_burtc.h
.
__IM uint32_t BURTC_TypeDef::STATUS |
Status Register
Definition at line 55
of file ezr32lg_burtc.h
.
__IM uint32_t BURTC_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 65
of file ezr32lg_burtc.h
.
__IM uint32_t BURTC_TypeDef::TIMESTAMP |
Backup mode timestamp
Definition at line 53
of file ezr32lg_burtc.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/
ezr32lg_burtc.h