TIMER_InitCC_TypeDef Struct ReferenceEMLIB > TIMER
TIMER compare/capture initialization structure.
Definition at line
316
of file
em_timer.h
.
#include <
em_timer.h
>
Field Documentation
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cmoa |
Counter match output action.
Definition at line
336
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cofoa |
Counter overflow output action.
Definition at line
333
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
bool TIMER_InitCC_TypeDef::coist |
Compare output initial state. Only used in Output Compare and PWM mode. When true, the compare/PWM output is set high when the counter is disabled. When counting resumes, this value will represent the initial value for the compare/PWM output. If the bit is cleared, the output will be cleared when the counter is disabled.
Definition at line
354
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cufoa |
Counter underflow output action.
Definition at line
330
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_Edge_TypeDef TIMER_InitCC_TypeDef::edge |
Input capture edge select.
Definition at line
321
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_Event_TypeDef TIMER_InitCC_TypeDef::eventCtrl |
Input capture event control.
Definition at line
318
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
bool TIMER_InitCC_TypeDef::filter |
TIMER_CCMode_TypeDef TIMER_InitCC_TypeDef::mode |
Compare/capture channel mode.
Definition at line
339
of file
em_timer.h
.
Referenced by BOARD_init() , TIMER_InitCC() , USBTIMER_Init() , and USTIMER_Init() .
bool TIMER_InitCC_TypeDef::outInvert |
Invert output from compare/capture channel.
Definition at line
357
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
bool TIMER_InitCC_TypeDef::prsInput |
Select TIMERnCCx (false) or PRS input (true).
Definition at line
345
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
TIMER_PRSSEL_TypeDef TIMER_InitCC_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if
prsInput
is enabled.
Definition at line
327
of file
em_timer.h
.
Referenced by TIMER_InitCC() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_timer.h