ETM_TypeDef Struct ReferenceDevices > EZR32LG_ETM

Definition at line 48 of file ezr32lg_etm.h.

Data Fields

__IM uint32_t ETMAUTHSTATUS
 
__IM uint32_t ETMCCER
 
__IM uint32_t ETMCCR
 
__IM uint32_t ETMCIDR0
 
__IM uint32_t ETMCIDR1
 
__IM uint32_t ETMCIDR2
 
__IM uint32_t ETMCIDR3
 
__IOM uint32_t ETMCLAIMCLR
 
__IOM uint32_t ETMCLAIMSET
 
__IOM uint32_t ETMCNTRLDVR1
 
__IOM uint32_t ETMCR
 
__IM uint32_t ETMDEVTYPE
 
__IOM uint32_t ETMFFLR
 
__IM uint32_t ETMIDR
 
__IM uint32_t ETMIDR2
 
__IOM uint32_t ETMISCIN
 
__OM uint32_t ETMITATBCTR0
 
__IM uint32_t ETMITATBCTR2
 
__IOM uint32_t ETMITCTRL
 
__IOM uint32_t ETMLAR
 
__IM uint32_t ETMLSR
 
__IM uint32_t ETMPDSR
 
__IM uint32_t ETMPIDR0
 
__IM uint32_t ETMPIDR1
 
__IM uint32_t ETMPIDR2
 
__IM uint32_t ETMPIDR3
 
__IM uint32_t ETMPIDR4
 
__OM uint32_t ETMPIDR5
 
__OM uint32_t ETMPIDR6
 
__OM uint32_t ETMPIDR7
 
__IM uint32_t ETMSCR
 
__IOM uint32_t ETMSR
 
__IOM uint32_t ETMSYNCFR
 
__IOM uint32_t ETMTECR1
 
__IOM uint32_t ETMTEEVR
 
__IOM uint32_t ETMTESSEICR
 
__IOM uint32_t ETMTRACEIDR
 
__IOM uint32_t ETMTRIGGER
 
__IOM uint32_t ETMTSEVR
 
__OM uint32_t ITTRIGOUT
 
uint32_t RESERVED0 [1]
 
uint32_t RESERVED1 [2]
 
uint32_t RESERVED10 [754]
 
uint32_t RESERVED11 [1]
 
uint32_t RESERVED12 [1]
 
uint32_t RESERVED13 [1]
 
uint32_t RESERVED14 [1]
 
uint32_t RESERVED15 [39]
 
uint32_t RESERVED16 [2]
 
uint32_t RESERVED17 [4]
 
uint32_t RESERVED2 [1]
 
uint32_t RESERVED3 [68]
 
uint32_t RESERVED4 [39]
 
uint32_t RESERVED5 [1]
 
uint32_t RESERVED6 [1]
 
uint32_t RESERVED7 [1]
 
uint32_t RESERVED8 [1]
 
uint32_t RESERVED9 [66]
 

Field Documentation

__IM uint32_t ETM_TypeDef::ETMAUTHSTATUS

ETM Authentication Status Register

Definition at line 92 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMCCER

Configuration Code Extension Register

Definition at line 65 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMCCR

Configuration Code Register

Definition at line 50 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMCIDR0

Component ID0 Register

Definition at line 103 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMCIDR1

Component ID1 Register

Definition at line 104 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMCIDR2

Component ID2 Register

Definition at line 105 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMCIDR3

Component ID3 Register

Definition at line 106 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMCLAIMCLR

ETM Claim Tag Clear Register

Definition at line 88 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMCLAIMSET

ETM Claim Tag Set Register

Definition at line 87 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMCNTRLDVR1

Counter Reload Value

Definition at line 61 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMCR

Main Control Register

Definition at line 49 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMDEVTYPE

CoreSight Device Type Register

Definition at line 94 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMFFLR

ETM Fifo Full Level Register

Definition at line 59 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMIDR

ID Register

Definition at line 64 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMIDR2

ETM ID Register 2

Definition at line 73 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMISCIN

Integration Test Miscellaneous Inputs Register

Definition at line 77 of file ezr32lg_etm.h.

__OM uint32_t ETM_TypeDef::ETMITATBCTR0

ETM Integration Test ATB Control 0 Register

Definition at line 83 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMITATBCTR2

ETM Integration Test ATB Control 2 Register

Definition at line 81 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMITCTRL

ETM Integration Control Register

Definition at line 85 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMLAR

ETM Lock Access Register

Definition at line 90 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMLSR

Lock Status Register

Definition at line 91 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMPDSR

Device Power-down Status Register

Definition at line 75 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMPIDR0

Peripheral ID0 Register

Definition at line 99 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMPIDR1

Peripheral ID1 Register

Definition at line 100 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMPIDR2

Peripheral ID2 Register

Definition at line 101 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMPIDR3

Peripheral ID3 Register

Definition at line 102 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMPIDR4

Peripheral ID4 Register

Definition at line 95 of file ezr32lg_etm.h.

__OM uint32_t ETM_TypeDef::ETMPIDR5

Peripheral ID5 Register

Definition at line 96 of file ezr32lg_etm.h.

__OM uint32_t ETM_TypeDef::ETMPIDR6

Peripheral ID6 Register

Definition at line 97 of file ezr32lg_etm.h.

__OM uint32_t ETM_TypeDef::ETMPIDR7

Peripheral ID7 Register

Definition at line 98 of file ezr32lg_etm.h.

__IM uint32_t ETM_TypeDef::ETMSCR

ETM System Configuration Register

Definition at line 54 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMSR

ETM Status Register

Definition at line 53 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMSYNCFR

Synchronisation Frequency Register

Definition at line 63 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMTECR1

ETM Trace control Register

Definition at line 57 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMTEEVR

ETM TraceEnable Event Register

Definition at line 56 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMTESSEICR

TraceEnable Start/Stop EmbeddedICE Control Register

Definition at line 67 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMTRACEIDR

CoreSight Trace ID Register

Definition at line 71 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMTRIGGER

ETM Trigger Event Register

Definition at line 51 of file ezr32lg_etm.h.

__IOM uint32_t ETM_TypeDef::ETMTSEVR

Timestamp Event Register

Definition at line 69 of file ezr32lg_etm.h.

__OM uint32_t ETM_TypeDef::ITTRIGOUT

Integration Test Trigger Out Register

Definition at line 79 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 52 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED1[2]

Reserved for future use

Definition at line 55 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED10[754]

Reserved for future use

Definition at line 76 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED11[1]

Reserved for future use

Definition at line 78 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED12[1]

Reserved for future use

Definition at line 80 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED13[1]

Reserved for future use

Definition at line 82 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED14[1]

Reserved for future use

Definition at line 84 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED15[39]

Reserved for future use

Definition at line 86 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED16[2]

Reserved for future use

Definition at line 89 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED17[4]

Reserved for future use

Definition at line 93 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED2[1]

Reserved for future use

Definition at line 58 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED3[68]

Reserved for future use

Definition at line 60 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED4[39]

Reserved for future use

Definition at line 62 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED5[1]

Reserved for future use

Definition at line 66 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED6[1]

Reserved for future use

Definition at line 68 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED7[1]

Reserved for future use

Definition at line 70 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED8[1]

Reserved for future use

Definition at line 72 of file ezr32lg_etm.h.

uint32_t ETM_TypeDef::RESERVED9[66]

Reserved for future use

Definition at line 74 of file ezr32lg_etm.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/ezr32lg_etm.h