MSDSCSI_StartStopUnit_TypeDef Struct ReferenceKit Drivers > Msd

SCSI Start Stop Unit Command Descriptor Block (CDB) typedef.

Definition at line 277 of file msdscsi.h.

#include <msdscsi.h>

Data Fields

struct {
   uint8_t   Immed: 1
 
   uint8_t   Reserved1: 7
 
}; 
 
struct {
   uint8_t   PowerConditionModifier: 4
 
   uint8_t   Reserved3: 4
 
}; 
 
struct {
   uint8_t   LoEj: 1
 
   uint8_t   No_Flush: 1
 
   uint8_t   PowerCondition: 4
 
   uint8_t   Reserved4: 1
 
   uint8_t   Start: 1
 
}; 
 
uint8_t Control
 
uint8_t OpCode
 
uint8_t Reserved2
 

Field Documentation

uint8_t MSDSCSI_StartStopUnit_TypeDef::Control

Control byte.

Definition at line 295 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::Immed

Immediate bit.

Definition at line 280 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::LoEj

Load Eject.

Definition at line 290 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::No_Flush

Dont flush cached data to the medium.

Definition at line 291 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::OpCode

Command opcode.

Definition at line 278 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::PowerCondition

Power Condition field.

Definition at line 293 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::PowerConditionModifier

Additional power condition info.

Definition at line 285 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved1

Reserved, expect 0.

Definition at line 281 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved2

Reserved, expect 0.

Definition at line 283 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved3

Reserved, expect 0.

Definition at line 286 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::Reserved4

Reserved, expect 0.

Definition at line 292 of file msdscsi.h.

uint8_t MSDSCSI_StartStopUnit_TypeDef::Start

Start bit.

Definition at line 289 of file msdscsi.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/hardware/kit/common/drivers/msdscsi.h