MSC_TypeDef Struct ReferenceDevices > EZR32LG_MSC

Definition at line 48 of file ezr32lg_msc.h .

Data Fields

__IOM uint32_t ADDRB
__IM uint32_t CACHEHITS
__IM uint32_t CACHEMISSES
__IOM uint32_t CMD
__IOM uint32_t CTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t LOCK
__IOM uint32_t MASSLOCK
__IOM uint32_t READCTRL
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [3]
uint32_t RESERVED2 [1]
__IM uint32_t STATUS
__IOM uint32_t TIMEBASE
__IOM uint32_t WDATA
__IOM uint32_t WRITECMD
__IOM uint32_t WRITECTRL

Field Documentation

__IOM uint32_t MSC_TypeDef::ADDRB

Page Erase/Write Address Buffer

Definition at line 53 of file ezr32lg_msc.h .

__IM uint32_t MSC_TypeDef::CACHEHITS

Cache Hits Performance Counter

Definition at line 66 of file ezr32lg_msc.h .

__IM uint32_t MSC_TypeDef::CACHEMISSES

Cache Misses Performance Counter

Definition at line 67 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::CMD

Command Register

Definition at line 65 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::CTRL

Memory System Control Register

Definition at line 49 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::IEN

Interrupt Enable Register

Definition at line 63 of file ezr32lg_msc.h .

__IM uint32_t MSC_TypeDef::IF

Interrupt Flag Register

Definition at line 60 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 62 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 61 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::LOCK

Configuration Lock Register

Definition at line 64 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::MASSLOCK

Mass Erase Lock Register

Definition at line 70 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::READCTRL

Read Control Register

Definition at line 50 of file ezr32lg_msc.h .

uint32_t MSC_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 55 of file ezr32lg_msc.h .

uint32_t MSC_TypeDef::RESERVED1[3]

Reserved for future use

Definition at line 59 of file ezr32lg_msc.h .

uint32_t MSC_TypeDef::RESERVED2[1]

Reserved for future use

Definition at line 68 of file ezr32lg_msc.h .

__IM uint32_t MSC_TypeDef::STATUS

Status Register

Definition at line 57 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::TIMEBASE

Flash Write and Erase Timebase

Definition at line 69 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::WDATA

Write Data Register

Definition at line 56 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::WRITECMD

Write Command Register

Definition at line 52 of file ezr32lg_msc.h .

__IOM uint32_t MSC_TypeDef::WRITECTRL

Write Control Register

Definition at line 51 of file ezr32lg_msc.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32LG/Include/ ezr32lg_msc.h