hidkbd.h File Reference
USB Human Interface Devices (HID) class keyboard driver.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
hidkbd.h
.
#include <stdint.h>
#include "
em_usb.h
"
Data Structures |
|
| struct | HIDKBD_Init_t |
| struct | HIDKBD_KeyReport_t |
Typedefs |
|
| typedef void(* | HIDKBD_SetReportFunc_t ) (uint8_t report) |
|
Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device.
|
|
Functions |
|
| void | HIDKBD_Init ( HIDKBD_Init_t *init) |
|
Initialize HID Keyboard driver.
|
|
| void | HIDKBD_KeyboardEvent ( HIDKBD_KeyReport_t *report) |
|
Report a keyboard press/release event.
|
|
| int | HIDKBD_SetupCmd (const USB_Setup_TypeDef *setup) |
|
Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.
|
|
| void | HIDKBD_StateChangeEvent ( USBD_State_TypeDef oldState, USBD_State_TypeDef newState) |
|
Handle USB state change events, this function must be called each time the USB device state is changed.
|
|
Variables |
|
| const char | HIDKBD_ReportDescriptor [69] |