USB_DIEP_TypeDef Struct ReferenceDevices
USB_DIEP EFM32HG USB DIEP.
Definition at line 46
of file efm32hg_usb_diep.h
.
#include <
efm32hg_usb_diep.h
>
Data Fields | |
__IOM uint32_t | CTL |
__IOM uint32_t | DMAADDR |
__IOM uint32_t | INT |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [1] |
uint32_t | RESERVED2 [1] |
__IOM uint32_t | TSIZ |
__IM uint32_t | TXFSTS |
Field Documentation
__IOM uint32_t USB_DIEP_TypeDef::CTL |
Device IN Endpoint x+1 Control Register
Definition at line 47
of file efm32hg_usb_diep.h
.
__IOM uint32_t USB_DIEP_TypeDef::DMAADDR |
Device IN Endpoint x+1 DMA Address Register
Definition at line 52
of file efm32hg_usb_diep.h
.
__IOM uint32_t USB_DIEP_TypeDef::INT |
Device IN Endpoint x+1 Interrupt Register
Definition at line 49
of file efm32hg_usb_diep.h
.
uint32_t USB_DIEP_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 48
of file efm32hg_usb_diep.h
.
uint32_t USB_DIEP_TypeDef::RESERVED1[1] |
Reserved for future use
Definition at line 50
of file efm32hg_usb_diep.h
.
uint32_t USB_DIEP_TypeDef::RESERVED2[1] |
Reserved future
Definition at line 54
of file efm32hg_usb_diep.h
.
__IOM uint32_t USB_DIEP_TypeDef::TSIZ |
Device IN Endpoint x+1 Transfer Size Register
Definition at line 51
of file efm32hg_usb_diep.h
.
__IM uint32_t USB_DIEP_TypeDef::TXFSTS |
Device IN Endpoint x+1 Transmit FIFO Status Register
Definition at line 53
of file efm32hg_usb_diep.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/
efm32hg_usb_diep.h