VCMP_Init_TypeDef Struct ReferenceEMLIB > VCMP

VCMP Initialization structure.

Definition at line 94 of file em_vcmp.h.

#include <em_vcmp.h>

Data Fields

int biasProg
 
bool enable
 
bool halfBias
 
VCMP_Hysteresis_TypeDef hyst
 
int inactive
 
bool irqFalling
 
bool irqRising
 
bool lowPowerRef
 
int triggerLevel
 
VCMP_WarmTime_TypeDef warmup
 

Field Documentation

int VCMP_Init_TypeDef::biasProg

BIAS current configuration, depends on Half Bias setting above, see reference manual for more information.

Definition at line 99 of file em_vcmp.h.

Referenced by VCMP_Init().

bool VCMP_Init_TypeDef::enable

Enable VCMP after configuration.

Definition at line 116 of file em_vcmp.h.

Referenced by VCMP_Init(), and VDDCHECK_LowVoltage().

bool VCMP_Init_TypeDef::halfBias

If set to true, reduces the bias current by half.

Definition at line 96 of file em_vcmp.h.

Referenced by VCMP_Init().

VCMP_Hysteresis_TypeDef VCMP_Init_TypeDef::hyst

Hysteresis configuration

Definition at line 107 of file em_vcmp.h.

Referenced by VCMP_Init().

int VCMP_Init_TypeDef::inactive

Output value when comparator is inactive, should be 0 or 1.

Definition at line 109 of file em_vcmp.h.

Referenced by VCMP_Init().

bool VCMP_Init_TypeDef::irqFalling

Enable interrupt for falling edge.

Definition at line 101 of file em_vcmp.h.

Referenced by VCMP_Init().

bool VCMP_Init_TypeDef::irqRising

Enable interrupt for rising edge.

Definition at line 103 of file em_vcmp.h.

Referenced by VCMP_Init().

bool VCMP_Init_TypeDef::lowPowerRef

Enable low power mode for VDD and band gap reference.

Definition at line 111 of file em_vcmp.h.

Referenced by VCMP_Init(), and VDDCHECK_LowVoltage().

int VCMP_Init_TypeDef::triggerLevel

Trigger level, according to formula: VDD Trigger Level = 1.667V + 0.034V x triggerLevel

Definition at line 114 of file em_vcmp.h.

Referenced by VCMP_Init(), and VDDCHECK_LowVoltage().

VCMP_WarmTime_TypeDef VCMP_Init_TypeDef::warmup

Warm-up time in clock cycles.

Definition at line 105 of file em_vcmp.h.

Referenced by VCMP_Init(), and VDDCHECK_LowVoltage().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_vcmp.h