USART_InitSync_TypeDef Struct ReferenceEMLIB > USART

Synchronous mode initialization structure.

Definition at line 463 of file em_usart.h.

#include <em_usart.h>

Data Fields

bool autoCsEnable
 
bool autoTx
 
uint32_t baudrate
 
USART_ClockMode_TypeDef clockMode
 
USART_Databits_TypeDef databits
 
USART_Enable_TypeDef enable
 
bool master
 
bool msbf
 
USART_PrsRxCh_TypeDef prsRxCh
 
bool prsRxEnable
 
uint32_t refFreq
 

Field Documentation

bool USART_InitSync_TypeDef::autoCsEnable

Auto CS enabling

Definition at line 501 of file em_usart.h.

Referenced by USART_InitSync().

bool USART_InitSync_TypeDef::autoTx

Enable AUTOTX mode. Transmits as long as RX is not full. Generates underflows if TX is empty.

Definition at line 497 of file em_usart.h.

Referenced by MIC_init(), and USART_InitSync().

uint32_t USART_InitSync_TypeDef::baudrate

Desired baud rate.

Definition at line 474 of file em_usart.h.

Referenced by MIC_init(), MICROSD_Init(), SPIDRV_Init(), and USART_InitSync().

USART_ClockMode_TypeDef USART_InitSync_TypeDef::clockMode

Clock polarity/phase mode.

Definition at line 486 of file em_usart.h.

Referenced by SPIDRV_Init(), and USART_InitSync().

USART_Databits_TypeDef USART_InitSync_TypeDef::databits

Number of data bits in frame.

Definition at line 477 of file em_usart.h.

Referenced by USART_InitSync().

USART_Enable_TypeDef USART_InitSync_TypeDef::enable

Specifies whether TX and/or RX shall be enabled when initialization is completed.

Definition at line 465 of file em_usart.h.

Referenced by MIC_init(), USART_InitI2s(), and USART_InitSync().

bool USART_InitSync_TypeDef::master

Select if to operate in master or slave mode.

Definition at line 480 of file em_usart.h.

Referenced by SPIDRV_Init(), and USART_InitSync().

bool USART_InitSync_TypeDef::msbf

Select if to send most or least significant bit first.

Definition at line 483 of file em_usart.h.

Referenced by MICROSD_Init(), SPIDRV_Init(), and USART_InitSync().

USART_PrsRxCh_TypeDef USART_InitSync_TypeDef::prsRxCh

Select PRS channel for USART Rx. (Only valid if prsRxEnable is true).

Definition at line 493 of file em_usart.h.

Referenced by USART_InitSync().

bool USART_InitSync_TypeDef::prsRxEnable

Enable USART Rx via PRS.

Definition at line 490 of file em_usart.h.

Referenced by USART_InitSync().

uint32_t USART_InitSync_TypeDef::refFreq

USART/UART reference clock assumed when configuring baud rate setup. Set to 0 to use the currently configured reference clock.

Definition at line 471 of file em_usart.h.

Referenced by USART_InitSync().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_usart.h