CMU_TypeDef Struct ReferenceDevices > EFM32HG_CMU
Definition at line 48
of file efm32hg_cmu.h
.
Data Fields | |
__IOM uint32_t | AUXHFRCOCTRL |
__IOM uint32_t | CALCNT |
__IOM uint32_t | CALCTRL |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | FREEZE |
__IOM uint32_t | HFCORECLKDIV |
__IOM uint32_t | HFCORECLKEN0 |
__IOM uint32_t | HFPERCLKDIV |
__IOM uint32_t | HFPERCLKEN0 |
__IOM uint32_t | HFRCOCTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | LFACLKEN0 |
__IOM uint32_t | LFAPRESC0 |
__IOM uint32_t | LFBCLKEN0 |
__IOM uint32_t | LFBPRESC0 |
__IOM uint32_t | LFCCLKEN0 |
__IOM uint32_t | LFCLKSEL |
__IOM uint32_t | LFRCOCTRL |
__IOM uint32_t | LOCK |
__IOM uint32_t | OSCENCMD |
__IOM uint32_t | PCNTCTRL |
uint32_t | RESERVED0 [2] |
uint32_t | RESERVED1 [1] |
uint32_t | RESERVED2 [1] |
uint32_t | RESERVED3 [1] |
uint32_t | RESERVED4 [1] |
uint32_t | RESERVED5 [18] |
__IOM uint32_t | ROUTE |
__IM uint32_t | STATUS |
__IM uint32_t | SYNCBUSY |
__IOM uint32_t | USBCRCTRL |
__IOM uint32_t | USHFRCOCONF |
__IOM uint32_t | USHFRCOCTRL |
__IOM uint32_t | USHFRCOTUNE |
Field Documentation
__IOM uint32_t CMU_TypeDef::AUXHFRCOCTRL |
AUXHFRCO Control Register
Definition at line 54
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::CALCNT |
Calibration Counter Register
Definition at line 56
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::CALCTRL |
Calibration Control Register
Definition at line 55
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::CMD |
Command Register
Definition at line 58
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::CTRL |
CMU Control Register
Definition at line 49
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::FREEZE |
Freeze Register
Definition at line 69
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFCORECLKDIV |
High Frequency Core Clock Division Register
Definition at line 50
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFCORECLKEN0 |
High Frequency Core Clock Enable Register 0
Definition at line 65
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFPERCLKDIV |
High Frequency Peripheral Clock Division Register
Definition at line 51
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFPERCLKEN0 |
High Frequency Peripheral Clock Enable Register 0
Definition at line 66
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::HFRCOCTRL |
HFRCO Control Register
Definition at line 52
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::IEN |
Interrupt Enable Register
Definition at line 64
of file efm32hg_cmu.h
.
__IM uint32_t CMU_TypeDef::IF |
Interrupt Flag Register
Definition at line 61
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 63
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 62
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFACLKEN0 |
Low Frequency A Clock Enable Register 0 (Async Reg)
Definition at line 70
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFAPRESC0 |
Low Frequency A Prescaler Register 0 (Async Reg)
Definition at line 74
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFBCLKEN0 |
Low Frequency B Clock Enable Register 0 (Async Reg)
Definition at line 72
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFBPRESC0 |
Low Frequency B Prescaler Register 0 (Async Reg)
Definition at line 76
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFCCLKEN0 |
Low Frequency C Clock Enable Register 0 (Async Reg)
Definition at line 73
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFCLKSEL |
Low Frequency Clock Select Register
Definition at line 59
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::LFRCOCTRL |
LFRCO Control Register
Definition at line 53
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::LOCK |
Configuration Lock Register
Definition at line 82
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::OSCENCMD |
Oscillator Enable/Disable Command Register
Definition at line 57
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::PCNTCTRL |
PCNT Control Register
Definition at line 78
of file efm32hg_cmu.h
.
uint32_t CMU_TypeDef::RESERVED0[2] |
Reserved for future use
Definition at line 67
of file efm32hg_cmu.h
.
uint32_t CMU_TypeDef::RESERVED1[1] |
Reserved for future use
Definition at line 71
of file efm32hg_cmu.h
.
uint32_t CMU_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 75
of file efm32hg_cmu.h
.
uint32_t CMU_TypeDef::RESERVED3[1] |
Reserved for future use
Definition at line 77
of file efm32hg_cmu.h
.
uint32_t CMU_TypeDef::RESERVED4[1] |
Reserved for future use
Definition at line 80
of file efm32hg_cmu.h
.
uint32_t CMU_TypeDef::RESERVED5[18] |
Reserved for future use
Definition at line 84
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::ROUTE |
I/O Routing Register
Definition at line 81
of file efm32hg_cmu.h
.
__IM uint32_t CMU_TypeDef::STATUS |
Status Register
Definition at line 60
of file efm32hg_cmu.h
.
__IM uint32_t CMU_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 68
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::USBCRCTRL |
USB Clock Recovery Control
Definition at line 85
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::USHFRCOCONF |
USHFRCO Configuration
Definition at line 88
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::USHFRCOCTRL |
USHFRCO Control
Definition at line 86
of file efm32hg_cmu.h
.
__IOM uint32_t CMU_TypeDef::USHFRCOTUNE |
USHFRCO Frequency Tune
Definition at line 87
of file efm32hg_cmu.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/
efm32hg_cmu.h