GPIO_TypeDef Struct ReferenceDevices > EFM32HG_GPIO
Definition at line 48
of file efm32hg_gpio.h
.
Data Fields | |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IM uint32_t | EM4WUCAUSE |
__IOM uint32_t | EM4WUEN |
__IOM uint32_t | EM4WUPOL |
__IOM uint32_t | EXTIFALL |
__IOM uint32_t | EXTIPSELH |
__IOM uint32_t | EXTIPSELL |
__IOM uint32_t | EXTIRISE |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | INSENSE |
__IOM uint32_t | LOCK |
GPIO_P_TypeDef | P [6] |
uint32_t | RESERVED0 [10] |
__IOM uint32_t | ROUTE |
Field Documentation
__IOM uint32_t GPIO_TypeDef::CMD |
GPIO Command Register
Definition at line 65
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::CTRL |
GPIO Control Register
Definition at line 64
of file efm32hg_gpio.h
.
__IM uint32_t GPIO_TypeDef::EM4WUCAUSE |
EM4 Wake-up Cause Register
Definition at line 68
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EM4WUEN |
EM4 Wake-up Enable Register
Definition at line 66
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EM4WUPOL |
EM4 Wake-up Polarity Register
Definition at line 67
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIFALL |
External Interrupt Falling Edge Trigger Register
Definition at line 55
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIPSELH |
External Interrupt Port Select High Register
Definition at line 53
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIPSELL |
External Interrupt Port Select Low Register
Definition at line 52
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::EXTIRISE |
External Interrupt Rising Edge Trigger Register
Definition at line 54
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::IEN |
Interrupt Enable Register
Definition at line 56
of file efm32hg_gpio.h
.
__IM uint32_t GPIO_TypeDef::IF |
Interrupt Flag Register
Definition at line 57
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 59
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 58
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::INSENSE |
Input Sense Register
Definition at line 62
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::LOCK |
Configuration Lock Register
Definition at line 63
of file efm32hg_gpio.h
.
GPIO_P_TypeDef GPIO_TypeDef::P[6] |
Port configuration bits
Definition at line 49
of file efm32hg_gpio.h
.
uint32_t GPIO_TypeDef::RESERVED0[10] |
Reserved for future use
Definition at line 51
of file efm32hg_gpio.h
.
__IOM uint32_t GPIO_TypeDef::ROUTE |
I/O Routing Register
Definition at line 61
of file efm32hg_gpio.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/
efm32hg_gpio.h