EMU_TypeDef Struct ReferenceDevices > EFM32HG_EMU

Definition at line 48 of file efm32hg_emu.h .

Data Fields

__IOM uint32_t AUXCTRL
__IOM uint32_t CTRL
__IOM uint32_t LOCK
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [6]

Field Documentation

__IOM uint32_t EMU_TypeDef::AUXCTRL

Auxiliary Control Register

Definition at line 55 of file efm32hg_emu.h .

__IOM uint32_t EMU_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32hg_emu.h .

__IOM uint32_t EMU_TypeDef::LOCK

Configuration Lock Register

Definition at line 52 of file efm32hg_emu.h .

uint32_t EMU_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 51 of file efm32hg_emu.h .

uint32_t EMU_TypeDef::RESERVED1[6]

Reserved for future use

Definition at line 54 of file efm32hg_emu.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/ efm32hg_emu.h