TIMER_CC_TypeDef Struct ReferenceDevices

TIMER_CC EFM32HG TIMER CC.

Definition at line 46 of file efm32hg_timer_cc.h.

#include <efm32hg_timer_cc.h>

Data Fields

__IOM uint32_t CCV
 
__IOM uint32_t CCVB
 
__IM uint32_t CCVP
 
__IOM uint32_t CTRL
 

Field Documentation

__IOM uint32_t TIMER_CC_TypeDef::CCV

CC Channel Value Register

Definition at line 48 of file efm32hg_timer_cc.h.

Referenced by TIMER_CaptureGet(), TIMER_CompareSet(), and TIMER_Reset().

__IOM uint32_t TIMER_CC_TypeDef::CCVB

CC Channel Buffer Register

Definition at line 50 of file efm32hg_timer_cc.h.

Referenced by TIMER_CompareBufSet(), and TIMER_Reset().

__IM uint32_t TIMER_CC_TypeDef::CCVP

CC Channel Value Peek Register

Definition at line 49 of file efm32hg_timer_cc.h.

__IOM uint32_t TIMER_CC_TypeDef::CTRL

CC Channel Control Register

Definition at line 47 of file efm32hg_timer_cc.h.

Referenced by TIMER_InitCC(), and TIMER_Reset().


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32HG/Include/efm32hg_timer_cc.h