textdisplay.h File Reference
Text display interface.
- Version
- 5.5.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
textdisplay.h
.
#include <stdbool.h>
#include "
emstatus.h
"
Data Structures |
|
struct | TEXTDISPLAY_Config_t |
Macros |
|
#define | TEXTDISPLAY_EMSTATUS_ALREADY_INITIALIZED ( TEXTDISPLAY_EMSTATUS_BASE | 3) |
#define | TEXTDISPLAY_EMSTATUS_INVALID_PARAM ( TEXTDISPLAY_EMSTATUS_BASE | 1) |
#define | TEXTDISPLAY_EMSTATUS_NOT_ENOUGH_MEMORY ( TEXTDISPLAY_EMSTATUS_BASE | 5) |
#define | TEXTDISPLAY_EMSTATUS_NOT_INITIALIZED ( TEXTDISPLAY_EMSTATUS_BASE | 6) |
#define | TEXTDISPLAY_EMSTATUS_NOT_SUPPORTED ( TEXTDISPLAY_EMSTATUS_BASE | 4) |
#define | TEXTDISPLAY_EMSTATUS_OK (0) |
#define | TEXTDISPLAY_EMSTATUS_OUT_OF_RANGE ( TEXTDISPLAY_EMSTATUS_BASE | 2) |
Typedefs |
|
typedef struct TEXTDISPLAY_Config_t | TEXTDISPLAY_Config_t |
typedef void * | TEXTDISPLAY_Handle_t |
Functions |
|
EMSTATUS | TEXTDISPLAY_Delete ( TEXTDISPLAY_Handle_t handle) |
Delete a text display device.
|
|
EMSTATUS | TEXTDISPLAY_LfToCrLf ( TEXTDISPLAY_Handle_t handle, bool on) |
Enable or disable LF to CR+LF conversion.
|
|
EMSTATUS | TEXTDISPLAY_New ( TEXTDISPLAY_Config_t *config, TEXTDISPLAY_Handle_t *handle) |
Create a new text display device.
|
|
EMSTATUS | TEXTDISPLAY_WriteChar ( TEXTDISPLAY_Handle_t handle, char c) |
Write a single character to a text display.
|
|
EMSTATUS | TEXTDISPLAY_WriteString ( TEXTDISPLAY_Handle_t handle, const char *str) |
Write a string of characters to a text display.
|
|