em_usbxpress.c File Reference
USBXpress global variable declaration, initialization, and call-back function definitions.
- Version
- 5.6.0
License
Copyright 2016 Silicon Laboratories, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
em_usbxpress.c
.
#include <stddef.h>
#include <stdbool.h>
#include "
em_usbxpress_internal.h
"
#include "
em_usbxpress_descriptors.h
"
#include "
em_usbxpress.h
"
Functions |
|
| USB_DeviceDescriptor_TypeDef USBXCORE_deviceDesc | SL_ATTRIBUTE_ALIGN (4) |
|
Copy of device descriptor, so it can be edited.
|
|
| void | USBX_apiCallbackDisable (void) |
|
Inhibits user API call-backs and does NOT disable the USB interrupt.
|
|
| void | USBX_apiCallbackEnable ( USBX_apiCallback_t f) |
|
Enables user API call-backs.
|
|
| int | USBX_blockRead (uint8_t *block, uint32_t numBytes, uint32_t *countPtr) |
|
User API function to get data from host.
|
|
| int | USBX_blockWrite (uint8_t *block, uint32_t numBytes, uint32_t *countPtr) |
|
User API function to send data to host.
|
|
| USBX_BUF (USBXCORE_overflowBuffer, USB_FS_BULK_EP_MAXSIZE ) | |
|
Buffer to hold overflow rx data if a ZLP read returns more than zero bytes.
|
|
| void | USBX_disable (void) |
|
Disables the USB interface.
|
|
| uint32_t | USBX_getCallbackSource (void) |
|
User API function to get the call-back source.
|
|
| uint_least16_t | USBX_getLibraryVersion (void) |
|
Returns the USBXpress library version.
|
|
| void | USBX_init ( USBX_Init_t *p) |
|
User API USB initialization function.
|
|
| void | USBX_jumpCallback (void) |
|
Conditionally jumps to the user call-back routine.
|
|
| void | USBXCORE_resetState (void) |
|
Resets internal USBXpress variables.
|
|
Variables |
|
| uint32_t | USBXCORE_apiEa |
|
Enable or disable status of USB_API interrupts.
|
|
| uint32_t | USBXCORE_apiIntValue |
|
Byte holding the current USB_API interrupts.
|
|
| uint32_t * | USBXCORE_byteCountInPtr |
|
Pointer to variable holding number of bytes written.
|
|
| uint32_t * | USBXCORE_byteCountOutPtr |
|
Pointer to variable holding number of bytes read.
|
|
| uint32_t | USBXCORE_readSize |
|
Number of bytes sent to
USBX_blockRead()
as numBytes.
|
|
| bool | USBXCORE_rxOverflowPacketAvailable = false |
|
Boolean indicating if data was received while expecting a ZLP.
|
|
| uint32_t | USBXCORE_rxOverflowPacketSize = 0 |
|
Size of Rx Overflow Packet.
|
|
| USB_StringDescriptor_TypeDef const * | USBXCORE_stringDescTable [4] |
|
Table of pointers to various string descriptors.
|
|
| uint32_t | USBXCORE_writeSize |
|
Number of bytes sent to
USBX_blockWrite()
as numBytes.
|
|
| bool | USBXCORE_zlpActive = false |
|
Boolean indicating whether a ZLP read is active.
|
|
Function Documentation
| const USB_ExtendedPropertiesDescriptor_t USBXCORE_extendedPropertiesDesc SL_ATTRIBUTE_ALIGN | ( | 4 |
|
) |
EXT_COMP_DESC_SIZE
,
FEATURE_EXTENDED_COMPATIBILITY_ID
,
NUM_IFCS_WITH_EXT_COMPAT
,
FEATURE_EXTENDED_COMPATIBILITY_ID
em_usbxpress_descriptors.h:45
NUM_IFCS_WITH_EXT_COMPAT
em_usbxpress_descriptors.h:54
EXT_COMP_DESC_SIZE
em_usbxpress_descriptors.h:49
Copy of device descriptor, so it can be edited.
Extended Properties Descriptor.
Compatible ID Feature Descriptor.
Copy of configuration descriptor.
| void USBX_jumpCallback | ( | void |
|
) |
Conditionally jumps to the user call-back routine.
If the user call-back routine is already in progress, this function does nothing. Otherwise, this function jumps to the call-back defined via USBX_callbackEnable().
Definition at line
254
of file
em_usbxpress.c
.
Referenced by USBX_DeviceStateChangeCb() , USBX_inXferCompleteCb() , USBX_outXferCompleteCb() , USBX_ResetCb() , and USBX_SetupCmdCb() .
| void USBXCORE_resetState | ( | void |
|
) |
Resets internal USBXpress variables.
This function resets the internal USBXpress variables. It should be called after a cancel-type event (USBXpress Close, USB de-configure, FIFO flush, etc.).
Definition at line
266
of file
em_usbxpress.c
.
References USBXCORE_rxOverflowPacketAvailable , and USBXCORE_zlpActive .
Referenced by USBX_DeviceStateChangeCb() , USBX_ResetCb() , and USBX_SetupCmdCb() .