nvm_hal.c File Reference

Non-Volatile Memory Wear-Leveling driver HAL implementation.

License

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

Definition in file nvm_hal.c .

#include <stdbool.h>
#include " em_msc.h "
#include " nvm.h "
#include " nvm_hal.h "

Functions

void NVMHAL_Checksum (uint16_t *pChecksum, void *pMemory, uint16_t len)
Calculate checksum according to CCITT CRC16.
void NVMHAL_DeInit (void)
De-initialize NVM .
void NVMHAL_Init (void)
Initialize NVM driver.
Ecode_t NVMHAL_PageErase (uint8_t *pAddress)
Erase a page in the NVM.
void NVMHAL_Read (uint8_t *pAddress, void *pObject, uint16_t len)
Read data from NVM.
Ecode_t NVMHAL_Write (uint8_t *pAddress, void const *pObject, uint16_t len)
Write data to NVM.

Function Documentation

void NVMHAL_Checksum ( uint16_t * pChecksum,
void * pMemory,
uint16_t len
)

Calculate checksum according to CCITT CRC16.

This function calculates a checksum of the supplied buffer. The checksum is calculated using CCITT CRC16 plynomial x^16+x^12+x^5+1.

This functionality is also present internally in the API, but is duplicated here to allow for much more efficient calculations specific to the hardware.

Parameters
[in] pChecksum Pointer to where the checksum should be calculated and stored. This buffer should be initialized. A good consistent starting point would be NVM_CHECKSUM_INITIAL.
[in] pMemory Pointer to the data you want to calculate a checksum for.
[in] len The length of the data.

Definition at line 305 of file nvm_hal.c .

void NVMHAL_DeInit ( void )

De-initialize NVM .

This function is run when the API deinit function is run. This should be done before any graceful halts.

Definition at line 134 of file nvm_hal.c .

References MSC_Deinit() .

void NVMHAL_Init ( void )

Initialize NVM driver.

This function is run upon initialization, at least once before any other functions. It can be used to call necessary startup routines before the hardware can be accessed.

Definition at line 121 of file nvm_hal.c .

References MSC_Init() .

Referenced by NVM_Init() .

Ecode_t NVMHAL_PageErase ( uint8_t * pAddress )

Erase a page in the NVM.

This function calls MSC_ErasePage and converts the return status.

Parameters
[in] *pAddress Memory address pointing to the start of the page to erase.
Returns
Returns the result of the erase operation.

Definition at line 276 of file nvm_hal.c .

References MSC_ErasePage() .

Referenced by NVM_Erase() .

void NVMHAL_Read ( uint8_t * pAddress,
void * pObject,
uint16_t len
)

Read data from NVM.

This function is used to read data from the NVM hardware. It should be a blocking call, since the thread asking for data to be read cannot continue without the data.

Another requirement is the ability to read unaligned blocks of data with single byte precision.

Parameters
[in] *pAddress Memory address in hardware for the data to read.
[in] *pObject RAM buffer to store the data from NVM.
[in] len The length of the data.

Definition at line 160 of file nvm_hal.c .

Referenced by NVM_Erase() , NVM_Init() , NVM_Read() , and NVM_Write() .

Ecode_t NVMHAL_Write ( uint8_t * pAddress,
void const * pObject,
uint16_t len
)

Write data to NVM.

This function is used to write data to the NVM. This is a blocking function.

Parameters
[in] *pAddress NVM address to write to.
[in] *pObject Pointer to source data.
[in] len The length of the data in bytes.
Returns
Returns the result of the write operation.

Definition at line 197 of file nvm_hal.c .

References MSC_WriteWord() , and mscReturnOk .

Referenced by NVM_Erase() , and NVM_Write() .