retargettft.c File Reference

Provide stdio retargeting to TFT address mapped mode.

License

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

Definition in file retargettft.c .

#include <stdio.h>
#include <stdint.h>
#include " em_device.h "
#include " em_cmu.h "
#include " em_ebi.h "
#include " em_gpio.h "
#include "dmd/ssd2119/dmd_ssd2119.h"
#include " bsp.h "
#include " retargettft.h "
#include " displayfont8x8.h "

Macros

#define CHARS 40
#define fontBits chars_8x8_bits
#define LINES 30

Functions

int RETARGET_ReadChar (void)
Receive a byte No input method from TFT is possible, thus we always return -1.
void RETARGET_TftCrLf (int on)
Toggle LF to CRLF conversion.
void RETARGET_TftInit (void)
Intializes TFT text display.
void RETARGET_TFTTX (int c)
Transmit/display a character.
void RETARGET_TFTUpdate (bool fullFrame)
Display framebuffer.
int RETARGET_WriteChar (char c)
Transmit single byte to the TFT.
static void tftTextReset (void)
Reset TFT text display state.
static void tftTextScrollUp (void)
Scroll one line of characters up on the screen.

Variables

static bool bufferReset = true
static uint8_t charBuffer [ LINES ][ CHARS ]
static bool fullUpdate = true
static bool initialized = false
static bool LFtoCRLF = 0
static uint8_t rgbColor [3]
static bool tftReset = true
static int xpos
static int ypos

Macro Definition Documentation

#define CHARS   40

Characters

Definition at line 31 of file retargettft.c .

Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .

#define fontBits   chars_8x8_bits

Define font

Definition at line 29 of file retargettft.c .

Referenced by RETARGET_TFTUpdate() .

#define LINES   30

Lines

Definition at line 32 of file retargettft.c .

Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .

Function Documentation

int RETARGET_ReadChar ( void )

Receive a byte No input method from TFT is possible, thus we always return -1.

Returns
-1 on failure, or positive character integer on sucesss

Definition at line 351 of file retargettft.c .

int RETARGET_WriteChar ( char c )

Transmit single byte to the TFT.

Parameters
c Character to transmit
Returns
Transmitted character

Definition at line 361 of file retargettft.c .

References BC_ARB_CTRL_EBI , BC_REGISTER , BC_UIF_AEM_EFM , BSP_RegisterRead() , bufferReset , fullUpdate , initialized , LFtoCRLF , RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftReset , and tftTextReset() .

Variable Documentation

bool bufferReset = true
static

Reset buffer

Definition at line 41 of file retargettft.c .

Referenced by RETARGET_WriteChar() , and tftTextReset() .

uint8_t charBuffer[ LINES ][ CHARS ]
static

Character buffer

Definition at line 34 of file retargettft.c .

Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .

bool fullUpdate = true
static

Display updated

Definition at line 40 of file retargettft.c .

Referenced by RETARGET_WriteChar() , and tftTextScrollUp() .

bool initialized = false
static

Intialize TFT stdio retarget

Definition at line 44 of file retargettft.c .

Referenced by RETARGET_WriteChar() , and tftTextReset() .

bool LFtoCRLF = 0
static

LF to CRLF conversion disabled

Definition at line 43 of file retargettft.c .

Referenced by RETARGET_TftCrLf() , and RETARGET_WriteChar() .

uint8_t rgbColor[3]
static

Color for font

Definition at line 35 of file retargettft.c .

Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , and tftTextReset() .

bool tftReset = true
static

Reset TFT

Definition at line 42 of file retargettft.c .

Referenced by RETARGET_WriteChar() , and tftTextReset() .

int xpos
static

Cursor position

Definition at line 38 of file retargettft.c .

Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .

int ypos
static

Cursor position

Definition at line 38 of file retargettft.c .

Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .