BAP - Barometric Pressure SensorBSP > Thunderboard Sense BSP
Detailed Description
Driver for the Bosch Sensortec BMP280 pressure sensor.
Data Structures |
|
struct | __BAP_Config |
Structure to configure the BMP280 device.
|
|
Typedefs |
|
typedef struct __BAP_Config | BAP_Config |
Structure to configure the BMP280 device.
|
|
Functions |
|
uint32_t | BAP_config ( BAP_Config *cfg) |
Configure the barometric pressure sensor.
|
|
void | BAP_deInit (void) |
De-initializes the barometric pressure module.
|
|
uint32_t | BAP_getPressure (float *pressure) |
Initiates pressure measurement on the barometric pressure sensor and reads pressure from it.
|
|
uint32_t | BAP_getTemperature (float *temperature) |
Initiates temperature measurement on the barometric pressure sensor and reads pressure from it.
|
|
uint32_t | BAP_init (uint8_t *deviceId) |
Initializes the barometric pressure sensor chip.
|
|
Error Codes |
|
#define | BAP_OK 0x0000 |
#define | BAP_ERROR_DRIVER_NOT_INITIALIZED 0x0001 |
#define | BAP_ERROR_I2C_TRANSACTION_FAILED 0x0002 |
#define | BAP_ERROR_DEVICE_ID_MISMATCH 0x0003 |
Macro Definition Documentation
#define BAP_ERROR_DEVICE_ID_MISMATCH 0x0003 |
The device ID does not match the expected value
Definition at line
35
of file
bap.h
.
Referenced by BAP_init() .
#define BAP_ERROR_DRIVER_NOT_INITIALIZED 0x0001 |
The driver is not initialized
Definition at line
33
of file
bap.h
.
#define BAP_ERROR_I2C_TRANSACTION_FAILED 0x0002 |
I2C transaction failed
Definition at line
34
of file
bap.h
.
#define BAP_OK 0x0000 |
No errors
Definition at line
32
of file
bap.h
.
Referenced by BAP_getPressure() , BAP_getTemperature() , and BAP_init() .
Function Documentation
uint32_t BAP_config | ( | BAP_Config * |
cfg
|
) |
Configure the barometric pressure sensor.
- Parameters
-
[in] cfg
Structure, which holds the configuration parameters
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line
145
of file
bap.c
.
References bmp280_set_power_mode() , bmp280_set_standby_durn() , bmp280_set_work_mode() , __BAP_Config::oversampling , __BAP_Config::powerMode , and __BAP_Config::standbyTime .
void BAP_deInit | ( | void |
|
) |
De-initializes the barometric pressure module.
- Returns
- None
Definition at line
125
of file
bap.c
.
References bmp280_set_power_mode() , and BOARD_bapEnable() .
uint32_t BAP_getPressure | ( | float * |
pressure
|
) |
Initiates pressure measurement on the barometric pressure sensor and reads pressure from it.
- Parameters
-
[out] pressure
The measured pressure in millibars
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line
205
of file
bap.c
.
References BAP_OK , bmp280_compensate_pressure_int64() , bmp280_compensate_temperature_int32() , bmp280_get_forced_uncomp_pressure_temperature() , bmp280_read_uncomp_pressure() , and bmp280_read_uncomp_temperature() .
uint32_t BAP_getTemperature | ( | float * |
temperature
|
) |
Initiates temperature measurement on the barometric pressure sensor and reads pressure from it.
- Parameters
-
[out] temperature
The measured temperature in degrees Celsius
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line
170
of file
bap.c
.
References BAP_OK , bmp280_compensate_temperature_int32() , bmp280_get_forced_uncomp_pressure_temperature() , and bmp280_read_uncomp_temperature() .
uint32_t BAP_init | ( | uint8_t * |
deviceId
|
) |
Initializes the barometric pressure sensor chip.
- Parameters
-
[out] deviceId
The device ID of the connected chip
- Returns
- Returns zero on OK, non-zero otherwise
Definition at line
71
of file
bap.c
.
References BAP_ERROR_DEVICE_ID_MISMATCH , BAP_OK , bmp280_init() , bmp280_set_power_mode() , bmp280_set_work_mode() , BOARD_bapEnable() , bmp280_t::delay_msec , bmp280_t::dev_addr , and UTIL_delay() .