ETM_TypeDef Struct ReferenceDevices > ETM
ETM Register Declaration
Definition at line 48
of file efr32fg12p_etm.h
.
#include <
efr32fg12p_etm.h
>
Data Fields | |
__IM uint32_t | ETMAUTHSTATUS |
__IM uint32_t | ETMCCER |
__IM uint32_t | ETMCCR |
__IM uint32_t | ETMCIDR0 |
__IM uint32_t | ETMCIDR1 |
__IM uint32_t | ETMCIDR2 |
__IM uint32_t | ETMCIDR3 |
__IOM uint32_t | ETMCLAIMCLR |
__IOM uint32_t | ETMCLAIMSET |
__IOM uint32_t | ETMCNTRLDVR1 |
__IOM uint32_t | ETMCR |
__IM uint32_t | ETMDEVTYPE |
__IOM uint32_t | ETMFFLR |
__IM uint32_t | ETMIDR |
__IM uint32_t | ETMIDR2 |
__IOM uint32_t | ETMISCIN |
__IOM uint32_t | ETMITATBCTR0 |
__IM uint32_t | ETMITATBCTR2 |
__IOM uint32_t | ETMITCTRL |
__IOM uint32_t | ETMLAR |
__IM uint32_t | ETMLSR |
__IM uint32_t | ETMPDSR |
__IM uint32_t | ETMPIDR0 |
__IM uint32_t | ETMPIDR1 |
__IM uint32_t | ETMPIDR2 |
__IM uint32_t | ETMPIDR3 |
__IM uint32_t | ETMPIDR4 |
__OM uint32_t | ETMPIDR5 |
__OM uint32_t | ETMPIDR6 |
__OM uint32_t | ETMPIDR7 |
__IM uint32_t | ETMSCR |
__IOM uint32_t | ETMSR |
__IOM uint32_t | ETMSYNCFR |
__IOM uint32_t | ETMTECR1 |
__IOM uint32_t | ETMTEEVR |
__IOM uint32_t | ETMTESSEICR |
__IOM uint32_t | ETMTRACEIDR |
__IOM uint32_t | ETMTRIGGER |
__IOM uint32_t | ETMTSEVR |
__IOM uint32_t | ITTRIGOUT |
uint32_t | RESERVED0 [1U] |
uint32_t | RESERVED1 [2U] |
uint32_t | RESERVED10 [754U] |
uint32_t | RESERVED11 [1U] |
uint32_t | RESERVED12 [1U] |
uint32_t | RESERVED13 [1U] |
uint32_t | RESERVED14 [1U] |
uint32_t | RESERVED15 [39U] |
uint32_t | RESERVED16 [2U] |
uint32_t | RESERVED17 [4U] |
uint32_t | RESERVED2 [1U] |
uint32_t | RESERVED3 [68U] |
uint32_t | RESERVED4 [39U] |
uint32_t | RESERVED5 [1U] |
uint32_t | RESERVED6 [1U] |
uint32_t | RESERVED7 [1U] |
uint32_t | RESERVED8 [1U] |
uint32_t | RESERVED9 [66U] |
Field Documentation
__IM uint32_t ETM_TypeDef::ETMAUTHSTATUS |
ETM Authentication Status Register
Definition at line 92
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMCCER |
Configuration Code Extension Register
Definition at line 65
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMCCR |
Configuration Code Register
Definition at line 50
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMCIDR0 |
Component ID0 Register
Definition at line 103
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMCIDR1 |
Component ID1 Register
Definition at line 104
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMCIDR2 |
Component ID2 Register
Definition at line 105
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMCIDR3 |
Component ID3 Register
Definition at line 106
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMCLAIMCLR |
ETM Claim Tag Clear Register
Definition at line 88
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMCLAIMSET |
ETM Claim Tag Set Register
Definition at line 87
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMCNTRLDVR1 |
Counter Reload Value
Definition at line 61
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMCR |
Main Control Register
Definition at line 49
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMDEVTYPE |
CoreSight Device Type Register
Definition at line 94
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMFFLR |
ETM Fifo Full Level Register
Definition at line 59
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMIDR |
ID Register
Definition at line 64
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMIDR2 |
ETM ID Register 2
Definition at line 73
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMISCIN |
Integration Test Miscellaneous Inputs Register
Definition at line 77
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMITATBCTR0 |
ETM Integration Test ATB Control 0 Register
Definition at line 83
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMITATBCTR2 |
ETM Integration Test ATB Control 2 Register
Definition at line 81
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMITCTRL |
ETM Integration Control Register
Definition at line 85
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMLAR |
ETM Lock Access Register
Definition at line 90
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMLSR |
Lock Status Register
Definition at line 91
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMPDSR |
Device Power-down Status Register
Definition at line 75
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMPIDR0 |
Peripheral ID0 Register
Definition at line 99
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMPIDR1 |
Peripheral ID1 Register
Definition at line 100
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMPIDR2 |
Peripheral ID2 Register
Definition at line 101
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMPIDR3 |
Peripheral ID3 Register
Definition at line 102
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMPIDR4 |
Peripheral ID4 Register
Definition at line 95
of file efr32fg12p_etm.h
.
__OM uint32_t ETM_TypeDef::ETMPIDR5 |
Peripheral ID5 Register
Definition at line 96
of file efr32fg12p_etm.h
.
__OM uint32_t ETM_TypeDef::ETMPIDR6 |
Peripheral ID6 Register
Definition at line 97
of file efr32fg12p_etm.h
.
__OM uint32_t ETM_TypeDef::ETMPIDR7 |
Peripheral ID7 Register
Definition at line 98
of file efr32fg12p_etm.h
.
__IM uint32_t ETM_TypeDef::ETMSCR |
ETM System Configuration Register
Definition at line 54
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMSR |
ETM Status Register
Definition at line 53
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMSYNCFR |
Synchronisation Frequency Register
Definition at line 63
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMTECR1 |
ETM Trace control Register
Definition at line 57
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMTEEVR |
ETM TraceEnable Event Register
Definition at line 56
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMTESSEICR |
TraceEnable Start/Stop EmbeddedICE Control Register
Definition at line 67
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMTRACEIDR |
CoreSight Trace ID Register
Definition at line 71
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMTRIGGER |
ETM Trigger Event Register
Definition at line 51
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ETMTSEVR |
Timestamp Event Register
Definition at line 69
of file efr32fg12p_etm.h
.
__IOM uint32_t ETM_TypeDef::ITTRIGOUT |
Integration Test Trigger Out Register
Definition at line 79
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line 52
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED1[2U] |
Reserved for future use
Definition at line 55
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED10[754U] |
Reserved for future use
Definition at line 76
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED11[1U] |
Reserved for future use
Definition at line 78
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED12[1U] |
Reserved for future use
Definition at line 80
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED13[1U] |
Reserved for future use
Definition at line 82
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED14[1U] |
Reserved for future use
Definition at line 84
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED15[39U] |
Reserved for future use
Definition at line 86
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED16[2U] |
Reserved for future use
Definition at line 89
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED17[4U] |
Reserved for future use
Definition at line 93
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED2[1U] |
Reserved for future use
Definition at line 58
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED3[68U] |
Reserved for future use
Definition at line 60
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED4[39U] |
Reserved for future use
Definition at line 62
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED5[1U] |
Reserved for future use
Definition at line 66
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED6[1U] |
Reserved for future use
Definition at line 68
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED7[1U] |
Reserved for future use
Definition at line 70
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED8[1U] |
Reserved for future use
Definition at line 72
of file efr32fg12p_etm.h
.
uint32_t ETM_TypeDef::RESERVED9[66U] |
Reserved for future use
Definition at line 74
of file efr32fg12p_etm.h
.
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/
efr32fg12p_etm.h