IDAC_Init_TypeDef Struct ReferenceEMLIB > IDAC
IDAC initialization structure, common for both channels.
Definition at line
166
of file
em_idac.h
.
#include <
em_idac.h
>
Data Fields |
|
bool | enable |
IDAC_OutMode_TypeDef | outMode |
bool | prsEnable |
IDAC_PRSSEL_TypeDef | prsSel |
bool | sinkEnable |
Field Documentation
bool IDAC_Init_TypeDef::enable |
IDAC_OutMode_TypeDef IDAC_Init_TypeDef::outMode |
bool IDAC_Init_TypeDef::prsEnable |
Enables Peripheral reflex system (PRS) to control IDAC output. If false, IDAC output is controlled by writing to IDAC_OUTEN in IDAC_CTRL or by calling IDAC_OutEnable() .
Definition at line
178
of file
em_idac.h
.
Referenced by IDAC_Init() .
IDAC_PRSSEL_TypeDef IDAC_Init_TypeDef::prsSel |
Peripheral reflex system channel selection. Only applicable if
prsEnable
is enabled.
Definition at line
184
of file
em_idac.h
.
Referenced by IDAC_Init() .
bool IDAC_Init_TypeDef::sinkEnable |
Enable/disable current sink mode.
Definition at line
187
of file
em_idac.h
.
Referenced by IDAC_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_idac.h