VDAC_OPA_TypeDef Struct ReferenceDevicesDevices > | VDAC
VDAC_OPA VDAC OPA Register
.
Definition at line 46
of file efr32fg12p_vdac_opa.h
.
#include <
efr32fg12p_vdac_opa.h
>
Data Fields | |
__IM uint32_t | APORTCONFLICT |
__IM uint32_t | APORTREQ |
__IOM uint32_t | CAL |
__IOM uint32_t | CTRL |
__IOM uint32_t | MUX |
__IOM uint32_t | OUT |
uint32_t | RESERVED0 [1U] |
__IOM uint32_t | TIMER |
Field Documentation
__IM uint32_t VDAC_OPA_TypeDef::APORTCONFLICT |
Operational Amplifier APORT Conflict Status Register
Definition at line 48
of file efr32fg12p_vdac_opa.h
.
__IM uint32_t VDAC_OPA_TypeDef::APORTREQ |
Operational Amplifier APORT Request Status Register
Definition at line 47
of file efr32fg12p_vdac_opa.h
.
__IOM uint32_t VDAC_OPA_TypeDef::CAL |
Operational Amplifier Calibration Register
Definition at line 53
of file efr32fg12p_vdac_opa.h
.
__IOM uint32_t VDAC_OPA_TypeDef::CTRL |
Operational Amplifier Control Register
Definition at line 49
of file efr32fg12p_vdac_opa.h
.
__IOM uint32_t VDAC_OPA_TypeDef::MUX |
Operational Amplifier Mux Configuration Register
Definition at line 51
of file efr32fg12p_vdac_opa.h
.
__IOM uint32_t VDAC_OPA_TypeDef::OUT |
Operational Amplifier Output Configuration Register
Definition at line 52
of file efr32fg12p_vdac_opa.h
.
uint32_t VDAC_OPA_TypeDef::RESERVED0[1U] |
Reserved future
Definition at line 54
of file efr32fg12p_vdac_opa.h
.
__IOM uint32_t VDAC_OPA_TypeDef::TIMER |
Operational Amplifier Timer Control Register
Definition at line 50
of file efr32fg12p_vdac_opa.h
.
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/
efr32fg12p_vdac_opa.h