WDOG_TypeDef Struct ReferenceDevices > WDOG
WDOG Register Declaration
Definition at line 48
of file efr32fg12p_wdog.h
.
#include <
efr32fg12p_wdog.h
>
Data Fields | |
__IOM uint32_t | CMD |
__IOM uint32_t | CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
WDOG_PCH_TypeDef | PCH [2U] |
uint32_t | RESERVED0 [2U] |
__IM uint32_t | SYNCBUSY |
Field Documentation
__IOM uint32_t WDOG_TypeDef::CMD |
__IOM uint32_t WDOG_TypeDef::CTRL |
Control Register
Definition at line 49
of file efr32fg12p_wdog.h
.
Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), WDOGn_IsEnabled(), WDOGn_IsLocked(), and WDOGn_Lock().
__IOM uint32_t WDOG_TypeDef::IEN |
Interrupt Enable Register
Definition at line 60
of file efr32fg12p_wdog.h
.
Referenced by WDOGn_IntDisable(), WDOGn_IntEnable(), and WDOGn_IntGetEnabled().
__IM uint32_t WDOG_TypeDef::IF |
Watchdog Interrupt Flags
Definition at line 57
of file efr32fg12p_wdog.h
.
Referenced by WDOGn_IntGet(), and WDOGn_IntGetEnabled().
__IOM uint32_t WDOG_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 59
of file efr32fg12p_wdog.h
.
Referenced by WDOGn_IntClear().
__IOM uint32_t WDOG_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 58
of file efr32fg12p_wdog.h
.
Referenced by WDOGn_IntSet().
WDOG_PCH_TypeDef WDOG_TypeDef::PCH[2U] |
PCH
Definition at line 54
of file efr32fg12p_wdog.h
.
uint32_t WDOG_TypeDef::RESERVED0[2U] |
Reserved for future use
Definition at line 56
of file efr32fg12p_wdog.h
.
__IM uint32_t WDOG_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line 52
of file efr32fg12p_wdog.h
.
Referenced by WDOGn_Enable(), WDOGn_Feed(), WDOGn_Init(), WDOGn_Lock(), and WDOGn_SyncWait().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/
efr32fg12p_wdog.h