ADC_TypeDef Struct ReferenceDevices > ADC
ADC Register Declaration
Definition at line 48
of file efr32fg12p_adc.h
.
#include <
efr32fg12p_adc.h
>
Data Fields | |
__IM uint32_t | APORTCONFLICT |
__IOM uint32_t | APORTMASTERDIS |
__IM uint32_t | APORTREQ |
__IOM uint32_t | BIASPROG |
__IOM uint32_t | CAL |
__IOM uint32_t | CMD |
__IOM uint32_t | CMPTHR |
__IOM uint32_t | CTRL |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
uint32_t | RESERVED0 [1U] |
uint32_t | RESERVED1 [4U] |
uint32_t | RESERVED2 [3U] |
__IOM uint32_t | SCANCTRL |
__IOM uint32_t | SCANCTRLX |
__IM uint32_t | SCANDATA |
__IM uint32_t | SCANDATAP |
__IM uint32_t | SCANDATAX |
__IM uint32_t | SCANDATAXP |
__IOM uint32_t | SCANFIFOCLEAR |
__IM uint32_t | SCANFIFOCOUNT |
__IOM uint32_t | SCANINPUTSEL |
__IOM uint32_t | SCANMASK |
__IOM uint32_t | SCANNEGSEL |
__IOM uint32_t | SINGLECTRL |
__IOM uint32_t | SINGLECTRLX |
__IM uint32_t | SINGLEDATA |
__IM uint32_t | SINGLEDATAP |
__IOM uint32_t | SINGLEFIFOCLEAR |
__IM uint32_t | SINGLEFIFOCOUNT |
__IM uint32_t | STATUS |
Field Documentation
__IM uint32_t ADC_TypeDef::APORTCONFLICT |
APORT Conflict Status Register
Definition at line 77
of file efr32fg12p_adc.h
.
__IOM uint32_t ADC_TypeDef::APORTMASTERDIS |
APORT Bus Master Disable Register
Definition at line 82
of file efr32fg12p_adc.h
.
__IM uint32_t ADC_TypeDef::APORTREQ |
APORT Request Status Register
Definition at line 76
of file efr32fg12p_adc.h
.
__IOM uint32_t ADC_TypeDef::BIASPROG |
Bias Programming Register for Various Analog Blocks Used in ADC Operation
Definition at line 61
of file efr32fg12p_adc.h
.
Referenced by ADC_InitSingle(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::CAL |
Calibration Register
Definition at line 62
of file efr32fg12p_adc.h
.
__IOM uint32_t ADC_TypeDef::CMD |
Command Register
Definition at line 51
of file efr32fg12p_adc.h
.
Referenced by ADC_Init(), ADC_InitScan(), ADC_InitSingle(), ADC_Reset(), and ADC_Start().
__IOM uint32_t ADC_TypeDef::CMPTHR |
Compare Threshold Register
Definition at line 60
of file efr32fg12p_adc.h
.
__IOM uint32_t ADC_TypeDef::CTRL |
Control Register
Definition at line 49
of file efr32fg12p_adc.h
.
Referenced by ADC_Init(), ADC_InitScan(), ADC_InitSingle(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 66
of file efr32fg12p_adc.h
.
Referenced by ADC_IntDisable(), ADC_IntEnable(), ADC_IntGetEnabled(), and ADC_Reset().
__IM uint32_t ADC_TypeDef::IF |
Interrupt Flag Register
Definition at line 63
of file efr32fg12p_adc.h
.
Referenced by ADC_IntGet(), and ADC_IntGetEnabled().
__IOM uint32_t ADC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 65
of file efr32fg12p_adc.h
.
Referenced by ADC_IntClear(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 64
of file efr32fg12p_adc.h
.
Referenced by ADC_IntSet().
uint32_t ADC_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line 50
of file efr32fg12p_adc.h
.
uint32_t ADC_TypeDef::RESERVED1[4U] |
Reserved for future use
Definition at line 71
of file efr32fg12p_adc.h
.
uint32_t ADC_TypeDef::RESERVED2[3U] |
Reserved for future use
Definition at line 75
of file efr32fg12p_adc.h
.
__IOM uint32_t ADC_TypeDef::SCANCTRL |
Scan Control Register
Definition at line 55
of file efr32fg12p_adc.h
.
Referenced by ADC_InitScan(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::SCANCTRLX |
Scan Control Register Continued
Definition at line 56
of file efr32fg12p_adc.h
.
Referenced by ADC_InitScan(), and ADC_Reset().
__IM uint32_t ADC_TypeDef::SCANDATA |
Scan Conversion Result Data
Definition at line 68
of file efr32fg12p_adc.h
.
Referenced by ADC_DataScanGet().
__IM uint32_t ADC_TypeDef::SCANDATAP |
Scan Sequence Result Data Peek Register
Definition at line 70
of file efr32fg12p_adc.h
.
Referenced by ADC_DataScanPeek().
__IM uint32_t ADC_TypeDef::SCANDATAX |
Scan Sequence Result Data + Data Source Register
Definition at line 72
of file efr32fg12p_adc.h
.
Referenced by ADC_DataIdScanGet().
__IM uint32_t ADC_TypeDef::SCANDATAXP |
Scan Sequence Result Data + Data Source Peek Register
Definition at line 73
of file efr32fg12p_adc.h
.
__IOM uint32_t ADC_TypeDef::SCANFIFOCLEAR |
__IM uint32_t ADC_TypeDef::SCANFIFOCOUNT |
Scan FIFO Count Register
Definition at line 79
of file efr32fg12p_adc.h
.
__IOM uint32_t ADC_TypeDef::SCANINPUTSEL |
Input Selection Register for Scan Mode
Definition at line 58
of file efr32fg12p_adc.h
.
Referenced by ADC_InitScan(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::SCANMASK |
Scan Sequence Input Mask Register
Definition at line 57
of file efr32fg12p_adc.h
.
Referenced by ADC_InitScan(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::SCANNEGSEL |
Negative Input Select Register for Scan
Definition at line 59
of file efr32fg12p_adc.h
.
Referenced by ADC_InitScan(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::SINGLECTRL |
Single Channel Control Register
Definition at line 53
of file efr32fg12p_adc.h
.
Referenced by ADC_InitSingle(), and ADC_Reset().
__IOM uint32_t ADC_TypeDef::SINGLECTRLX |
Single Channel Control Register Continued
Definition at line 54
of file efr32fg12p_adc.h
.
Referenced by ADC_InitSingle(), and ADC_Reset().
__IM uint32_t ADC_TypeDef::SINGLEDATA |
Single Conversion Result Data
Definition at line 67
of file efr32fg12p_adc.h
.
Referenced by ADC_DataSingleGet().
__IM uint32_t ADC_TypeDef::SINGLEDATAP |
Single Conversion Result Data Peek Register
Definition at line 69
of file efr32fg12p_adc.h
.
Referenced by ADC_DataSinglePeek().
__IOM uint32_t ADC_TypeDef::SINGLEFIFOCLEAR |
Single FIFO Clear Register
Definition at line 80
of file efr32fg12p_adc.h
.
Referenced by ADC_Reset().
__IM uint32_t ADC_TypeDef::SINGLEFIFOCOUNT |
Single FIFO Count Register
Definition at line 78
of file efr32fg12p_adc.h
.
__IM uint32_t ADC_TypeDef::STATUS |
Status Register
Definition at line 52
of file efr32fg12p_adc.h
.
Referenced by ADC_InitScan(), and ADC_InitSingle().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/
efr32fg12p_adc.h