TRNG_TypeDef Struct ReferenceDevices > TRNG
TRNG Register Declaration
Definition at line 48
of file efr32fg12p_trng.h
.
#include <
efr32fg12p_trng.h
>
Data Fields | |
__IOM uint32_t | CONTROL |
__IM uint32_t | FIFO |
__IM uint32_t | FIFODEPTH |
__IM uint32_t | FIFOLEVEL |
__IOM uint32_t | INITWAITVAL |
__IOM uint32_t | KEY0 |
__IOM uint32_t | KEY1 |
__IOM uint32_t | KEY2 |
__IOM uint32_t | KEY3 |
uint32_t | RESERVED0 [1U] |
uint32_t | RESERVED1 [3U] |
uint32_t | RESERVED2 [50U] |
__IOM uint32_t | STATUS |
__IOM uint32_t | TESTDATA |
Field Documentation
__IOM uint32_t TRNG_TypeDef::CONTROL |
Main Control Register
Definition at line 49
of file efr32fg12p_trng.h
.
__IM uint32_t TRNG_TypeDef::FIFO |
FIFO Data
Definition at line 63
of file efr32fg12p_trng.h
.
__IM uint32_t TRNG_TypeDef::FIFODEPTH |
FIFO Depth Register
Definition at line 52
of file efr32fg12p_trng.h
.
__IM uint32_t TRNG_TypeDef::FIFOLEVEL |
FIFO Level Register
Definition at line 50
of file efr32fg12p_trng.h
.
__IOM uint32_t TRNG_TypeDef::INITWAITVAL |
Initial Wait Counter
Definition at line 61
of file efr32fg12p_trng.h
.
__IOM uint32_t TRNG_TypeDef::KEY0 |
Key Register 0
Definition at line 53
of file efr32fg12p_trng.h
.
__IOM uint32_t TRNG_TypeDef::KEY1 |
Key Register 1
Definition at line 54
of file efr32fg12p_trng.h
.
__IOM uint32_t TRNG_TypeDef::KEY2 |
Key Register 2
Definition at line 55
of file efr32fg12p_trng.h
.
__IOM uint32_t TRNG_TypeDef::KEY3 |
Key Register 3
Definition at line 56
of file efr32fg12p_trng.h
.
uint32_t TRNG_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line 51
of file efr32fg12p_trng.h
.
uint32_t TRNG_TypeDef::RESERVED1[3U] |
Reserved for future use
Definition at line 59
of file efr32fg12p_trng.h
.
uint32_t TRNG_TypeDef::RESERVED2[50U] |
Reserved for future use
Definition at line 62
of file efr32fg12p_trng.h
.
__IOM uint32_t TRNG_TypeDef::STATUS |
Status Register
Definition at line 60
of file efr32fg12p_trng.h
.
__IOM uint32_t TRNG_TypeDef::TESTDATA |
Test Data Register
Definition at line 57
of file efr32fg12p_trng.h
.
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/
efr32fg12p_trng.h