TIMER_TypeDef Struct ReferenceDevices > TIMER

TIMER Register Declaration

Definition at line 48 of file efr32fg12p_timer.h .

#include < efr32fg12p_timer.h >

Data Fields

TIMER_CC_TypeDef CC [4U]
__IOM uint32_t CMD
__IOM uint32_t CNT
__IOM uint32_t CTRL
__IOM uint32_t DTCTRL
__IM uint32_t DTFAULT
__IOM uint32_t DTFAULTC
__IOM uint32_t DTFC
__IOM uint32_t DTLOCK
__IOM uint32_t DTOGEN
__IOM uint32_t DTTIME
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t LOCK
uint32_t RESERVED0 [1U]
uint32_t RESERVED1 [1U]
uint32_t RESERVED2 [8U]
__IOM uint32_t ROUTELOC0
__IOM uint32_t ROUTELOC2
__IOM uint32_t ROUTEPEN
__IM uint32_t STATUS
__IOM uint32_t TOP
__IOM uint32_t TOPB

Field Documentation

TIMER_CC_TypeDef TIMER_TypeDef::CC[4U]

Compare/Capture Channel

Definition at line 67 of file efr32fg12p_timer.h .

Referenced by TIMER_CaptureBufGet() , TIMER_CaptureGet() , TIMER_CompareBufSet() , TIMER_CompareSet() , TIMER_InitCC() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::CMD

Command Register

Definition at line 50 of file efr32fg12p_timer.h .

Referenced by TIMER_Enable() , TIMER_Init() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::CNT

Counter Value Register

Definition at line 58 of file efr32fg12p_timer.h .

Referenced by TIMER_CounterGet() , TIMER_CounterSet() , TIMER_Init() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::CTRL

Control Register

Definition at line 49 of file efr32fg12p_timer.h .

Referenced by TIMER_Init() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::DTCTRL

DTI Control Register

Definition at line 69 of file efr32fg12p_timer.h .

Referenced by TIMER_EnableDTI() , TIMER_InitDTI() , and TIMER_Reset() .

__IM uint32_t TIMER_TypeDef::DTFAULT

DTI Fault Register

Definition at line 73 of file efr32fg12p_timer.h .

Referenced by TIMER_GetDTIFault() .

__IOM uint32_t TIMER_TypeDef::DTFAULTC

DTI Fault Clear Register

Definition at line 74 of file efr32fg12p_timer.h .

Referenced by TIMER_ClearDTIFault() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::DTFC

DTI Fault Configuration Register

Definition at line 71 of file efr32fg12p_timer.h .

Referenced by TIMER_InitDTI() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::DTLOCK

DTI Configuration Lock Register

Definition at line 75 of file efr32fg12p_timer.h .

Referenced by TIMER_Lock() , TIMER_Reset() , and TIMER_Unlock() .

__IOM uint32_t TIMER_TypeDef::DTOGEN

DTI Output Generation Enable Register

Definition at line 72 of file efr32fg12p_timer.h .

Referenced by TIMER_InitDTI() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::DTTIME

DTI Time Control Register

Definition at line 70 of file efr32fg12p_timer.h .

Referenced by TIMER_InitDTI() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::IEN

Interrupt Enable Register

Definition at line 55 of file efr32fg12p_timer.h .

Referenced by TIMER_IntDisable() , TIMER_IntEnable() , TIMER_IntGetEnabled() , and TIMER_Reset() .

__IM uint32_t TIMER_TypeDef::IF

Interrupt Flag Register

Definition at line 52 of file efr32fg12p_timer.h .

Referenced by TIMER_IntGet() , and TIMER_IntGetEnabled() .

__IOM uint32_t TIMER_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 54 of file efr32fg12p_timer.h .

Referenced by TIMER_IntClear() , and TIMER_Reset() .

__IOM uint32_t TIMER_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 53 of file efr32fg12p_timer.h .

Referenced by TIMER_IntSet() .

__IOM uint32_t TIMER_TypeDef::LOCK

TIMER Configuration Lock Register

Definition at line 60 of file efr32fg12p_timer.h .

uint32_t TIMER_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 59 of file efr32fg12p_timer.h .

uint32_t TIMER_TypeDef::RESERVED1[1U]

Reserved for future use

Definition at line 63 of file efr32fg12p_timer.h .

uint32_t TIMER_TypeDef::RESERVED2[8U]

Reserved registers

Definition at line 66 of file efr32fg12p_timer.h .

__IOM uint32_t TIMER_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 62 of file efr32fg12p_timer.h .

Referenced by BOARD_init() .

__IOM uint32_t TIMER_TypeDef::ROUTELOC2

I/O Routing Location Register

Definition at line 64 of file efr32fg12p_timer.h .

__IOM uint32_t TIMER_TypeDef::ROUTEPEN

I/O Routing Pin Enable Register

Definition at line 61 of file efr32fg12p_timer.h .

Referenced by BOARD_init() , and BOARD_rgbledSetRawColor() .

__IM uint32_t TIMER_TypeDef::STATUS

Status Register

Definition at line 51 of file efr32fg12p_timer.h .

__IOM uint32_t TIMER_TypeDef::TOP

Counter Top Value Register

Definition at line 56 of file efr32fg12p_timer.h .

Referenced by TIMER_Reset() , TIMER_TopGet() , and TIMER_TopSet() .

__IOM uint32_t TIMER_TypeDef::TOPB

Counter Top Value Buffer Register

Definition at line 57 of file efr32fg12p_timer.h .

Referenced by TIMER_Reset() , and TIMER_TopBufSet() .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/ efr32fg12p_timer.h