CMU_DPLLInit_TypeDef Struct ReferenceEMLIB > CMU
DPLL initialization structure. Frequency will be Fref*(N+1)/(M+1).
Definition at line 2321
of file em_cmu.h
.
#include <
em_cmu.h
>
Data Fields | |
bool | autoRecover |
CMU_DPLLEdgeSel_TypeDef | edgeSel |
uint32_t | frequency |
CMU_DPLLLockMode_TypeDef | lockMode |
uint16_t | m |
uint16_t | n |
CMU_DPLLClkSel_TypeDef | refClk |
uint8_t | ssAmplitude |
uint8_t | ssInterval |
Field Documentation
bool CMU_DPLLInit_TypeDef::autoRecover |
Enable automatic lock recovery.
Definition at line 2330
of file em_cmu.h
.
Referenced by CMU_DPLLLock().
CMU_DPLLEdgeSel_TypeDef CMU_DPLLInit_TypeDef::edgeSel |
Reference clock edge detect selector.
Definition at line 2328
of file em_cmu.h
.
Referenced by CMU_DPLLLock().
uint32_t CMU_DPLLInit_TypeDef::frequency |
PLL frequency value, max 40 MHz.
Definition at line 2322
of file em_cmu.h
.
Referenced by CMU_DPLLLock().
CMU_DPLLLockMode_TypeDef CMU_DPLLInit_TypeDef::lockMode |
uint16_t CMU_DPLLInit_TypeDef::m |
uint16_t CMU_DPLLInit_TypeDef::n |
CMU_DPLLClkSel_TypeDef CMU_DPLLInit_TypeDef::refClk |
uint8_t CMU_DPLLInit_TypeDef::ssAmplitude |
uint8_t CMU_DPLLInit_TypeDef::ssInterval |
Spread spectrum update interval.
Definition at line 2325
of file em_cmu.h
.
Referenced by CMU_DPLLLock().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_cmu.h