CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU
HFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
Definition at line
2182
of file
em_cmu.h
.
#include <
em_cmu.h
>
Data Fields |
|
| bool | autoSelEm01 |
| bool | autoStartEm01 |
| bool | autoStartSelOnRacWakeup |
| uint16_t | ctuneStartup |
| uint16_t | ctuneSteadyState |
| bool | lowPowerMode |
| CMU_OscMode_TypeDef | mode |
| uint8_t | regIshSteadyState |
| uint8_t | thresholdPeakDetect |
| uint8_t | timeoutPeakDetect |
| uint8_t | timeoutShuntOptimization |
| uint8_t | timeoutStartup |
| uint8_t | timeoutSteady |
| uint8_t | xoCoreBiasTrimStartup |
| uint8_t | xoCoreBiasTrimSteadyState |
Field Documentation
| bool CMU_HFXOInit_TypeDef::autoSelEm01 |
-
Deprecated: - Use CMU_HFXOAutostartEnable instead.
Definition at line
2194
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::autoStartEm01 |
-
Deprecated: - Use CMU_HFXOAutostartEnable instead.
Definition at line
2193
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup |
-
Deprecated: - Use CMU_HFXOAutostartEnable instead.
Definition at line
2195
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| uint16_t CMU_HFXOInit_TypeDef::ctuneStartup |
Startup phase CTUNE (load capacitance) value
Definition at line
2196
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState |
Steady-state phase CTUNE (load capacitance) value
Definition at line
2197
of file
em_cmu.h
.
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::lowPowerMode |
| CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode |
| uint8_t CMU_HFXOInit_TypeDef::regIshSteadyState |
Shunt steady-state current
Definition at line
2198
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::thresholdPeakDetect |
| uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect |
| uint8_t CMU_HFXOInit_TypeDef::timeoutShuntOptimization |
Timeout - shunt optimization
Definition at line
2202
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::timeoutStartup |
| uint8_t CMU_HFXOInit_TypeDef::timeoutSteady |
| uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup |
Startup XO core bias current trim
Definition at line
2199
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState |
Steady-state XO core bias current trim
Definition at line
2200
of file
em_cmu.h
.
Referenced by CMU_HFXOInit() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_cmu.h