NANDFLASH_Info_TypeDef Struct ReferenceKit Drivers > NANDFlash
NANDFLASH device information structure.
Definition at line
56
of file
nandflash.h
.
#include <
nandflash.h
>
Data Fields |
|
| uint32_t | baseAddress |
| uint32_t | blockSize |
| uint8_t | deviceCode |
| uint32_t | deviceSize |
| int | dmaCh |
| uint32_t | ecc |
| uint8_t | manufacturerCode |
| uint32_t | pageSize |
| uint8_t | spare [ NAND256W3A_SPARESIZE ] |
| uint32_t | spareSize |
Field Documentation
| uint32_t NANDFLASH_Info_TypeDef::baseAddress |
The device base address in cpu memory map.
Definition at line
57
of file
nandflash.h
.
Referenced by NANDFLASH_AddressValid() .
| uint32_t NANDFLASH_Info_TypeDef::blockSize |
Device block size in bytes.
Definition at line
63
of file
nandflash.h
.
| uint8_t NANDFLASH_Info_TypeDef::deviceCode |
The device ID .
Definition at line
59
of file
nandflash.h
.
| uint32_t NANDFLASH_Info_TypeDef::deviceSize |
Total device size in bytes.
Definition at line
60
of file
nandflash.h
.
Referenced by NANDFLASH_AddressValid() .
| int NANDFLASH_Info_TypeDef::dmaCh |
The DMA channel used, -1 if DMA is not used.
Definition at line
66
of file
nandflash.h
.
Referenced by NANDFLASH_Init() , NANDFLASH_ReadPage() , NANDFLASH_ReadSpare() , and NANDFLASH_WritePage() .
| uint32_t NANDFLASH_Info_TypeDef::ecc |
Result of ECC generation from last read/written page.
Definition at line
64
of file
nandflash.h
.
Referenced by NANDFLASH_ReadPage() , and NANDFLASH_WritePage() .
| uint8_t NANDFLASH_Info_TypeDef::manufacturerCode |
The device manufacturer code.
Definition at line
58
of file
nandflash.h
.
| uint32_t NANDFLASH_Info_TypeDef::pageSize |
Device page size in bytes.
Definition at line
61
of file
nandflash.h
.
Referenced by NANDFLASH_ReadPage() , and NANDFLASH_WritePage() .
| uint8_t NANDFLASH_Info_TypeDef::spare[ NAND256W3A_SPARESIZE ] |
Spare area content from last read page or spare operation.
Definition at line
65
of file
nandflash.h
.
Referenced by NANDFLASH_ReadPage() .
| uint32_t NANDFLASH_Info_TypeDef::spareSize |
Device page spare size in bytes.
Definition at line
62
of file
nandflash.h
.
Referenced by NANDFLASH_ReadPage() , and NANDFLASH_ReadSpare() .
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/hardware/kit/common/drivers/
nandflash.h