You are viewing documentation for version:
     
      5.8
     
     |
     
      5.9
     
     (latest) |
     
      Version History
     
    
    
    
     
      
       - 
        
        
        globalScope> Global
        
         BSP_TraceSwoSetup
        
        (void)
       
- 
        Deprecated function. New code should call
        
         BSP_TraceProfilerSetup()
        
        .
       
- 
        
        
        globalScope> Global
        
         EMU_MemPwrDown
        
        (uint32_t blocks)
       
- 
        This function is deprecated, use
        
         EMU_RamPowerDown()
        
        instead which maps a user provided memory range into RAM blocks to power down.
       
- 
        
        
        globalScope> Global
        
         EMU_UpdateOscConfig
        
        (void)
       
- 
        Oscillator status is saved in
        
         EMU_EnterEM2()
        
        and
        
         EMU_EnterEM3()
        
        .
       
- 
        
        
        globalScope> Global
        
         GPIO_IntConfig
        
        (GPIO_Port_TypeDef port, unsigned int pin, bool risingEdge, bool fallingEdge, bool enable)
       
- 
        Deprecated function. New code should use
        
         GPIO_ExtIntConfig()
        
        .
       
- 
        
        
        Module
        
         INT
        
       
- 
        These functions are deprecated and marked for removal in a later release. Use the
        
         CORE
        
        module instead. See
        
         Porting from em_int
        
        for information on how to convert existing code bases to use
        
         CORE
        
        .
       
- 
        
        
        globalScope> Global
        
         INT_Disable
        
        (void)
       
- 
        Deprecated and marked for removal in a later release. Use new CORE module instead.
       
- 
        
        
        globalScope> Global
        
         INT_Enable
        
        (void)
       
- 
        Deprecated and marked for removal in a later release. Use the new CORE module instead.
       
- 
        
        
        Module
        
         NVM
        
       
- 
        This driver is deprecated and marked for removal in a later release. New code should use
        
         NVM3
        
        .
       
- 
        
        
        globalScope> Global
        
         setupSWOForPrint
        
       
- 
        Use
        
         RETARGET_SwoInit
        
        instead
       
- 
        
        
        globalScope> Global
        
         SLEEP_Init
        
        (SLEEP_CbFuncPtr_t pSleepCb, SLEEP_CbFuncPtr_t pWakeUpCb)
       
- 
        New code should use the
        
         SLEEP_InitEx
        
        function for initializing the sleep module.
       
- 
        
        
        globalScope> Global
        
         UARTDRV_Init
        
        (UARTDRV_Handle_t handle,
        
         UARTDRV_InitUart_t
        
        *initData)
       
- 
        Deprecated; Use
        
         UARTDRV_InitUart()
        
        instead.
       
- 
        
        
        globalScope> Global
        
         USART_InitIrDA
        
        (const
        
         USART_InitIrDA_TypeDef
        
        *init)
       
- 
        Deprecated function. New code should use
        
         USARTn_InitIrDA()
        
        . This function uses DEFAULT_IRDA_USART, which unless otherwise specified, is USART0 on most devices, and USART1 on devices that don't have a USART0.
       
- 
        
        
        globalScope> Global
        
         WDOG_Enable
        
        (bool enable)
       
- 
        Deprecated function. New code should use
        
         WDOGn_Enable()
        
        . This function uses
        
         DEFAULT_WDOG
        
        .
       
- 
        
        
        globalScope> Global
        
         WDOG_Feed
        
        (void)
       
- 
        Deprecated function. New code should use
        
         WDOGn_Feed()
        
        . This function uses
        
         DEFAULT_WDOG
        
        .
       
- 
        
        
        globalScope> Global
        
         WDOG_Init
        
        (const
        
         WDOG_Init_TypeDef
        
        *init)
       
- 
        Deprecated function. New code should use
        
         WDOGn_Init()
        
        . This function uses
        
         DEFAULT_WDOG
        
        .
       
- 
        
        
        globalScope> Global
        
         WDOG_IsEnabled
        
        (void)
       
- 
        Deprecated function. New code should use
        
         WDOGn_IsEnabled()
        
        . This function uses
        
         DEFAULT_WDOG
        
        .
       
- 
        
        
        globalScope> Global
        
         WDOG_IsLocked
        
        (void)
       
- 
        Deprecated function. New code should use
        
         WDOGn_IsLocked()
        
        . This function uses
        
         DEFAULT_WDOG
        
        .
       
- 
        
        
        globalScope> Global
        
         WDOG_Lock
        
        (void)
       
- 
        Deprecated function. New code should use
        
         WDOGn_Lock()
        
        . This function uses
        
         DEFAULT_WDOG
        
        .