SEEMLIB
Detailed Description
Secure Element peripheral API.
Abstraction of the Secure Element's mailbox interface.
- Note
- Although commands to interact with the mailbox directly are available, it is always recommended to use the higher level APIs available in em_se and through mbedTLS.
- Using the SE's mailbox is not thread-safe in emlib, and accessing the SE's mailbox both in regular and IRQ context is not safe, either. If mbedTLS is compiled into the application, SE operations should be wrapped in se_management_acquire()/se_management_release() calls to synchronize access. If mbedTLS is not in use, it is the user's responsibility to not trigger simultaneous use of the SE mailbox.
Data Structures |
|
| struct | SE_Command_t |
| struct | SE_DataTransfer_t |
| struct | SE_DebugStatus_t |
| struct | SE_OTPInit_t |
| struct | SE_Status_t |
Macros |
|
| #define | SE_COMMAND_AES_CCM_DECRYPT 0x04060000UL |
| #define | SE_COMMAND_AES_CCM_ENCRYPT 0x04050000UL |
| #define | SE_COMMAND_AES_CMAC 0x04040000UL |
| #define | SE_COMMAND_AES_DECRYPT 0x04010000UL |
| #define | SE_COMMAND_AES_ENCRYPT 0x04000000UL |
| #define | SE_COMMAND_AES_GCM_DECRYPT 0x04030000UL |
| #define | SE_COMMAND_AES_GCM_ENCRYPT 0x04020000UL |
| #define | SE_COMMAND_APPLY_HOST_IMAGE 0x43060001UL |
| #define | SE_COMMAND_APPLY_SE_IMAGE 0x43030000UL |
| #define | SE_COMMAND_CHECK_HOST_IMAGE 0x43050001UL |
| #define | SE_COMMAND_CHECK_SE_IMAGE 0x43020000UL |
| #define | SE_COMMAND_CREATE_KEY 0x02000000UL |
| #define | SE_COMMAND_DBG_LOCK_APPLY 0x430C0000 |
| #define | SE_COMMAND_DBG_LOCK_DISABLE_SECURE 0x430E0000 |
| #define | SE_COMMAND_DBG_LOCK_ENABLE_SECURE 0x430D0000 |
| #define | SE_COMMAND_DBG_LOCK_STATUS 0x43110000 |
| #define | SE_COMMAND_DEFAULT (command) |
| #define | SE_COMMAND_DEVICE_ERASE 0x430F0000 |
| #define | SE_COMMAND_DEVICE_ERASE_DISABLE 0x43100000 |
| #define | SE_COMMAND_DH 0x0E000000UL |
| #define | SE_COMMAND_DISABLE_TAMPER 0xFD020001UL |
| #define | SE_COMMAND_ERASE_USER_DATA 0x430A0000UL |
| #define | SE_COMMAND_GET_CHALLENGE 0xFD000000UL |
| #define | SE_COMMAND_GET_STATUS 0xFE010000UL |
| #define | SE_COMMAND_HASH 0x03000000UL |
| #define | SE_COMMAND_HASHUPDATE 0x03010000UL |
| #define | SE_COMMAND_HMAC 0x03020000UL |
| #define | SE_COMMAND_INIT_OTP 0xFF000001UL |
| #define | SE_COMMAND_INIT_PUBKEY 0xFF070001UL |
| #define | SE_COMMAND_INIT_PUBKEY_SIGNATURE 0xFF090001UL |
| #define | SE_COMMAND_JPAKE_GEN_SESSIONKEY 0x0B020000UL |
| #define | SE_COMMAND_JPAKE_R1_GENERATE 0x0B000000UL |
| #define | SE_COMMAND_JPAKE_R1_VERIFY 0x0B000100UL |
| #define | SE_COMMAND_JPAKE_R2_GENERATE 0x0B010000UL |
| #define | SE_COMMAND_JPAKE_R2_VERIFY 0x0B010100UL |
| #define | SE_COMMAND_OPEN_DEBUG 0xFD010001UL |
| #define | SE_COMMAND_OPTION_CERT_BATCH 0x00000200UL |
| #define | SE_COMMAND_OPTION_CERT_DEVICE 0x00000100UL |
| #define | SE_COMMAND_OPTION_CERT_FACTORY 0x00000300UL |
| #define | SE_COMMAND_OPTION_CONTEXT_ADD 0x00000003UL |
| #define | SE_COMMAND_OPTION_CONTEXT_END 0x00000002UL |
| #define | SE_COMMAND_OPTION_CONTEXT_START 0x00000001UL |
| #define | SE_COMMAND_OPTION_CONTEXT_WHOLE 0x00000000UL |
| #define | SE_COMMAND_OPTION_ERASE_UD 0xDE1E7EADUL |
| #define | SE_COMMAND_OPTION_HASH_MD5 0x00000100UL |
| #define | SE_COMMAND_OPTION_HASH_SHA1 0x00000200UL |
| #define | SE_COMMAND_OPTION_HASH_SHA224 0x00000300UL |
| #define | SE_COMMAND_OPTION_HASH_SHA256 0x00000400UL |
| #define | SE_COMMAND_OPTION_MODE_CBC 0x00000200UL |
| #define | SE_COMMAND_OPTION_MODE_CFB 0x00000400UL |
| #define | SE_COMMAND_OPTION_MODE_CTR 0x00000300UL |
| #define | SE_COMMAND_OPTION_MODE_ECB 0x00000100UL |
| #define | SE_COMMAND_OPTION_MODE_OFB 0x00000500UL |
| #define | SE_COMMAND_OPTION_MODE_XTS 0x00000800UL |
| #define | SE_COMMAND_OPTION_PADDING_EMSA_PKCS 0x00000003UL |
| #define | SE_COMMAND_OPTION_PADDING_NONE 0x00000000UL |
| #define | SE_COMMAND_OPTION_PADDING_PSS 0x00000004UL |
| #define | SE_COMMAND_READ_CLOCK 0x07020000UL |
| #define | SE_COMMAND_READ_PUBKEY 0xFF080001UL |
| #define | SE_COMMAND_READ_PUBKEY_SIGNATURE 0xFF0A0001UL |
| #define | SE_COMMAND_READ_PUBKEYBOOT 0xFE020001UL |
| #define | SE_COMMAND_READ_SERIAL 0xFE000000UL |
| #define | SE_COMMAND_READPUB_KEY 0x02010000UL |
| #define | SE_COMMAND_SET_UPGRADEFLAG_HOST 0xFE030001UL |
| #define | SE_COMMAND_SET_UPGRADEFLAG_SE 0xFE030000UL |
| #define | SE_COMMAND_SIGNATURE_SIGN 0x06000000UL |
| #define | SE_COMMAND_SIGNATURE_VERIFY 0x06010000UL |
| #define | SE_COMMAND_STATUS_HOST_IMAGE 0x43070001UL |
| #define | SE_COMMAND_STATUS_OTP_VERSION 0x43080100UL |
| #define | SE_COMMAND_STATUS_SE_IMAGE 0x43040000UL |
| #define | SE_COMMAND_STATUS_SE_VERSION 0x43080000UL |
| #define | SE_COMMAND_TRNG_GET_RANDOM 0x07000000UL |
| #define | SE_COMMAND_WRITE_USER_DATA 0x43090000UL |
| #define | SE_DATATRANSFER_CONSTADDRESS 0x10000000UL |
| #define | SE_DATATRANSFER_DEFAULT (address, length) |
| #define | SE_DATATRANSFER_DISCARD 0x40000000UL |
| #define | SE_DATATRANSFER_LENGTH_MASK 0x0FFFFFFFUL |
| #define | SE_DATATRANSFER_REALIGN 0x20000000UL |
| #define | SE_DATATRANSFER_STOP 0x00000001UL |
| #define | SE_FIFO_MAX_PARAMETERS 13U |
| #define | SE_KEY_TYPE_AUTH 0x00000200UL |
| #define | SE_KEY_TYPE_BOOT 0x00000100UL |
| #define | SE_KEY_TYPE_ROOT 0x00000300UL |
| #define | SE_MAX_PARAMETERS 4U |
| #define | SE_OTP_MCU_SETTINGS_FLAG_SECURE_BOOT_ANTI_ROLLBACK (1 << 18) |
| #define | SE_OTP_MCU_SETTINGS_FLAG_SECURE_BOOT_ENABLE (1 << 16) |
| #define | SE_OTP_MCU_SETTINGS_FLAG_SECURE_BOOT_VERIFY_CERTIFICATE (1 << 17) |
| #define | SE_RESPONSE_ABORT 0x00090000UL |
| #define | SE_RESPONSE_AUTHORIZATION_ERROR 0x00020000UL |
| #define | SE_RESPONSE_BUS_ERROR 0x00040000UL |
| #define | SE_RESPONSE_CRYPTO_ERROR 0x00060000UL |
| #define | SE_RESPONSE_INTERNAL_ERROR 0x00050000UL |
| #define | SE_RESPONSE_INVALID_COMMAND 0x00010000UL |
| #define | SE_RESPONSE_INVALID_PARAMETER 0x00070000UL |
| #define | SE_RESPONSE_INVALID_SIGNATURE 0x00030000UL |
| #define | SE_RESPONSE_MASK 0x000F0000UL |
| #define | SE_RESPONSE_OK 0x00000000UL |
Typedefs |
|
| typedef uint32_t | SE_Response_t |
Functions |
|
| void | SE_addDataInput ( SE_Command_t *command, SE_DataTransfer_t *data) |
|
Add input data to a command.
|
|
| void | SE_addDataOutput ( SE_Command_t *command, SE_DataTransfer_t *data) |
|
Add output data to a command.
|
|
| void | SE_addParameter ( SE_Command_t *command, uint32_t parameter) |
|
Add a parameter to a command.
|
|
| SE_Response_t | SE_debugLockApply (void) |
|
Enables the debug lock for the part.
|
|
| SE_Response_t | SE_debugLockStatus ( SE_DebugStatus_t *status) |
|
Returns the current debug lock configuration.
|
|
| SE_Response_t | SE_debugSecureDisable (void) |
|
Disables the secure debug functionality.
|
|
| SE_Response_t | SE_debugSecureEnable (void) |
|
Enables the secure debug functionality.
|
|
| SE_Response_t | SE_deviceErase (void) |
|
Performs a device mass erase and debug unlock.
|
|
| SE_Response_t | SE_deviceEraseDisable (void) |
|
Disabled device erase functionality.
|
|
| __STATIC_INLINE void | SE_disableInterrupt (uint32_t flags) |
|
Disable one or more SE interrupts.
|
|
| __STATIC_INLINE void | SE_enableInterrupt (uint32_t flags) |
|
Enable one or more SE interrupts.
|
|
| SE_Response_t | SE_eraseUserData () |
|
Erases User Data section in MTP.
|
|
| void | SE_executeCommand ( SE_Command_t *command) |
|
Execute the passed command.
|
|
| SE_Response_t | SE_getStatus ( SE_Status_t *status) |
|
Returns the current boot status, versions and system configuration.
|
|
| SE_Response_t | SE_initOTP ( SE_OTPInit_t *otp_init) |
|
Initialize SE OTP configuration.
|
|
| SE_Response_t | SE_initPubkey (uint32_t key_type, void *pubkey, uint32_t numBytes, bool signature) |
|
Init pubkey or pubkey signature.
|
|
| __STATIC_INLINE bool | SE_isCommandCompleted (void) |
|
Check whether the running command has completed.
|
|
| __STATIC_INLINE SE_Response_t | SE_readCommandResponse (void) |
|
Read the status of the previously executed command.
|
|
| SE_Response_t | SE_readPubkey (uint32_t key_type, void *pubkey, uint32_t numBytes, bool signature) |
|
Read pubkey or pubkey signature.
|
|
| SE_Response_t | SE_serialNumber (void *serial) |
|
Read the serial number of the SE module.
|
|
| __STATIC_INLINE void | SE_waitCommandCompletion (void) |
|
Wait for completion of the current command.
|
|
| SE_Response_t | SE_writeUserData (uint32_t offset, void *data, uint32_t numBytes) |
|
Writes data to User Data section in MTP. Write data must be aligned to word size and contain a number of bytes that is divisable by four.
|
|
Macro Definition Documentation
| #define SE_COMMAND_DEFAULT | ( |
command
|
) |
Default initialization of command struct
Definition at line
334
of file
em_se.h
.
Referenced by SE_debugLockApply() , SE_debugLockStatus() , SE_debugSecureDisable() , SE_debugSecureEnable() , SE_deviceErase() , SE_deviceEraseDisable() , SE_eraseUserData() , SE_getStatus() , SE_initOTP() , SE_initPubkey() , SE_readPubkey() , SE_serialNumber() , and SE_writeUserData() .
| #define SE_COMMAND_OPTION_CONTEXT_ADDÂ Â Â 0x00000003UL |
Add more data input to the algorithm. Need to supply previous context, and get a context back
Definition at line
234
of file
em_se.h
.
| #define SE_COMMAND_OPTION_CONTEXT_ENDÂ Â Â 0x00000002UL |
End the algorithm, get the result
Definition at line
231
of file
em_se.h
.
| #define SE_COMMAND_OPTION_CONTEXT_STARTÂ Â Â 0x00000001UL |
Start the algorithm, but get a context to later add more data
Definition at line
229
of file
em_se.h
.
| #define SE_COMMAND_OPTION_CONTEXT_WHOLEÂ Â Â 0x00000000UL |
Run the whole algorithm, all data present
Definition at line
227
of file
em_se.h
.
| #define SE_COMMAND_OPTION_ERASE_UDÂ Â Â 0xDE1E7EADUL |
Magic paramater for deleting user data
Definition at line
243
of file
em_se.h
.
Referenced by SE_eraseUserData() .
| #define SE_COMMAND_OPTION_HASH_MD5Â Â Â 0x00000100UL |
Use MD5 as hash algorithm
Definition at line
188
of file
em_se.h
.
| #define SE_COMMAND_OPTION_HASH_SHA1Â Â Â 0x00000200UL |
Use SHA1 as hash algorithm
Definition at line
190
of file
em_se.h
.
| #define SE_COMMAND_OPTION_HASH_SHA224Â Â Â 0x00000300UL |
Use SHA224 as hash algorithm
Definition at line
192
of file
em_se.h
.
| #define SE_COMMAND_OPTION_HASH_SHA256Â Â Â 0x00000400UL |
Use SHA256 as hash algorithm
Definition at line
194
of file
em_se.h
.
| #define SE_COMMAND_OPTION_MODE_CBCÂ Â Â 0x00000200UL |
Execute algorithm in CBC mode
Definition at line
207
of file
em_se.h
.
| #define SE_COMMAND_OPTION_MODE_CFBÂ Â Â 0x00000400UL |
Execute algorithm in CFB mode
Definition at line
211
of file
em_se.h
.
| #define SE_COMMAND_OPTION_MODE_CTRÂ Â Â 0x00000300UL |
Execute algorithm in CTR mode
Definition at line
209
of file
em_se.h
.
| #define SE_COMMAND_OPTION_MODE_ECBÂ Â Â 0x00000100UL |
Execute algorithm in ECB mode
Definition at line
205
of file
em_se.h
.
| #define SE_COMMAND_OPTION_MODE_OFBÂ Â Â 0x00000500UL |
Execute algorithm in OFB mode
Definition at line
213
of file
em_se.h
.
| #define SE_COMMAND_OPTION_MODE_XTSÂ Â Â 0x00000800UL |
Execute algorithm in XTS mode
Definition at line
215
of file
em_se.h
.
| #define SE_COMMAND_OPTION_PADDING_NONEÂ Â Â 0x00000000UL |
Padding options for signature functionality.
Definition at line
237
of file
em_se.h
.
| #define SE_DATATRANSFER_DEFAULT | ( |
address,
|
|
length
|
|||
| ) |
Default initialization of data transfer struct
Definition at line
315
of file
em_se.h
.
Referenced by SE_debugLockStatus() , SE_getStatus() , SE_initOTP() , SE_initPubkey() , SE_readPubkey() , SE_serialNumber() , and SE_writeUserData() .
| #define SE_FIFO_MAX_PARAMETERSÂ Â Â 13U |
Maximum amount of parameters supported by the hardware FIFO
Definition at line
293
of file
em_se.h
.
| #define SE_KEY_TYPE_BOOTÂ Â Â 0x00000100UL |
Pubkey types
Definition at line
222
of file
em_se.h
.
Referenced by SE_initOTP() , SE_initPubkey() , and SE_readPubkey() .
| #define SE_MAX_PARAMETERSÂ Â Â 4U |
Maximum amount of parameters for largest command in defined command set
Definition at line
289
of file
em_se.h
.
Referenced by SE_addParameter() , and SE_executeCommand() .
| #define SE_RESPONSE_AUTHORIZATION_ERRORÂ Â Â 0x00020000UL |
User did not provide the required credentials to be allowed to execute the command.
Definition at line
258
of file
em_se.h
.
| #define SE_RESPONSE_BUS_ERRORÂ Â Â 0x00040000UL |
A command started in non-secure mode is trying to access secure memory.
Definition at line
265
of file
em_se.h
.
| #define SE_RESPONSE_CRYPTO_ERRORÂ Â Â 0x00060000UL |
An internal error was raised and the command did not execute.
Definition at line
269
of file
em_se.h
.
| #define SE_RESPONSE_INTERNAL_ERRORÂ Â Â 0x00050000UL |
Internal error
Definition at line
267
of file
em_se.h
.
| #define SE_RESPONSE_INVALID_COMMANDÂ Â Â 0x00010000UL |
Command was not recognized as a valid command, or is not allowed in the current context.
Definition at line
253
of file
em_se.h
.
| #define SE_RESPONSE_INVALID_PARAMETERÂ Â Â 0x00070000UL |
One of the passed parameters is deemed invalid (e.g. out of bounds).
Definition at line
271
of file
em_se.h
.
| #define SE_RESPONSE_INVALID_SIGNATUREÂ Â Â 0x00030000UL |
Signature validation command (e.g. SE_COMMAND_SIGNATURE_VERIFY) failed to verify the given signature as being correct.
Definition at line
263
of file
em_se.h
.
| #define SE_RESPONSE_OKÂ Â Â 0x00000000UL |
Command executed successfully or signature was successfully validated.
Definition at line
248
of file
em_se.h
.
Referenced by SE_initOTP() .
Typedef Documentation
| typedef uint32_t SE_Response_t |
Possible responses to a command
Definition at line
344
of file
em_se.h
.
Function Documentation
| void SE_addDataInput | ( | SE_Command_t * |
command,
|
| SE_DataTransfer_t * |
data
|
||
| ) |
Add input data to a command.
This function adds a buffer of input data to the given SE command structure The buffer gets appended by reference at the end of the list of already added buffers.
- Note
- Note that this function does not copy either the data buffer or the buffer structure, so make sure to keep the data object in scope until the command has been executed by the secure element.
- Parameters
-
[in] commandPointer to an SE command structure. [in] dataPointer to a data transfer structure.
Definition at line
132
of file
em_se.c
.
Referenced by SE_initOTP() , SE_initPubkey() , and SE_writeUserData() .
| void SE_addDataOutput | ( | SE_Command_t * |
command,
|
| SE_DataTransfer_t * |
data
|
||
| ) |
Add output data to a command.
This function adds a buffer of output data to the given command structure The buffer gets appended by reference at the end of the list of already added buffers.
- Note
- Note that this function does not copy either the data buffer or the buffer structure, so make sure to keep the data object in scope until the command has been executed by the secure element.
- Parameters
-
[in] commandPointer to an SE command structure. [in] dataPointer to a data transfer structure.
Definition at line
165
of file
em_se.c
.
Referenced by SE_debugLockStatus() , SE_getStatus() , SE_readPubkey() , and SE_serialNumber() .
| void SE_addParameter | ( | SE_Command_t * |
command,
|
| uint32_t |
parameter
|
||
| ) |
Add a parameter to a command.
This function adds a parameter word to the passed command.
- Note
- Make sure to not exceed SE_MAX_PARAMETERS .
- Parameters
-
[in] commandPointer to a filled-out SE command structure. [in] parameterParameter to add.
Definition at line
194
of file
em_se.c
.
References SE_MAX_PARAMETERS .
Referenced by SE_eraseUserData() , and SE_writeUserData() .
| SE_Response_t SE_debugLockApply | ( | void |
|
) |
Enables the debug lock for the part.
The debug port will be closed and the only way to open it is through device erase (if enabled) or through secure debug unlock (if enabled).
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully. SE_RESPONSE_INTERNAL_ERRORthere was a problem locking the debug port.
Definition at line
922
of file
em_se.c
.
References SE_COMMAND_DEFAULT , SE_executeCommand() , and SE_readCommandResponse() .
| SE_Response_t SE_debugLockStatus | ( | SE_DebugStatus_t * |
status
|
) |
Returns the current debug lock configuration.
- Parameters
-
[out] statusThe command returns a DebugStatus_t with the current status of the debug configuration.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully. SE_RESPONSE_INTERNAL_ERRORif there are configuration errors.
Definition at line
890
of file
em_se.c
.
References SE_DebugStatus_t::debugLockEnabled , SE_DebugStatus_t::deviceEraseEnabled , SE_addDataOutput() , SE_COMMAND_DEFAULT , SE_DATATRANSFER_DEFAULT , SE_executeCommand() , SE_readCommandResponse() , and SE_DebugStatus_t::secureDebugEnabled .
| SE_Response_t SE_debugSecureDisable | ( | void |
|
) |
Disables the secure debug functionality.
Disables the secure debug functionality that can be used to open a locked debug port.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully. SE_RESPONSE_INTERNAL_ERRORif there was a problem during execution.
Definition at line
965
of file
em_se.c
.
References SE_COMMAND_DEFAULT , SE_executeCommand() , and SE_readCommandResponse() .
| SE_Response_t SE_debugSecureEnable | ( | void |
|
) |
Enables the secure debug functionality.
Enables the secure debug functionality that can be used to open a locked debug port through the Get challenge and Open debug commands. This command can only be executed before the debug port is locked, and after a secure debug public key has been installed in the SE.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully. SE_RESPONSE_INVALID_COMMANDif debug port is locked. SE_RESPONSE_INVALID_PARAMETERif secure debug certificates are missing. SE_RESPONSE_INTERNAL_ERRORif there was a problem during execution.
Definition at line
946
of file
em_se.c
.
References SE_COMMAND_DEFAULT , SE_executeCommand() , and SE_readCommandResponse() .
| SE_Response_t SE_deviceErase | ( | void |
|
) |
Performs a device mass erase and debug unlock.
Performs a device mass erase and resets the debug configuration to its initial unlocked state. Only available before DEVICE_ERASE_DISABLE has been executed.
- Note
- This command clears and verifies the complete flash and ram of the system, excluding the user data pages and one-time programmable commissioning information in the secure element.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully. SE_RESPONSE_INVALID_COMMANDif device erase is disabled. SE_RESPONSE_INTERNAL_ERRORif there was a problem during execution.
Definition at line
993
of file
em_se.c
.
References SE_COMMAND_DEFAULT , SE_executeCommand() , and SE_readCommandResponse() .
| SE_Response_t SE_deviceEraseDisable | ( | void |
|
) |
Disabled device erase functionality.
This command disables the device erase command. It does not lock the debug interface to the part, but it is a permanent action for the part. If device erase is disabled and the device is debug locked, there is no way to permanently unlock the part. If secure debug unlock is enabled, secure debug unlock can still be used to temporarily open the debug port.
- Warning
- This command permanently disables the device erase functionality!
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully. SE_RESPONSE_INTERNAL_ERRORif there was a problem during execution.
Definition at line
1020
of file
em_se.c
.
References SE_COMMAND_DEFAULT , SE_executeCommand() , and SE_readCommandResponse() .
| __STATIC_INLINE void SE_disableInterrupt | ( | uint32_t |
flags
|
) |
Disable one or more SE interrupts.
- Parameters
-
[in] flagsSE interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the Secure Element module (SE_CONFIGURATION_(TX/RX)INTEN).
Definition at line
509
of file
em_se.h
.
| __STATIC_INLINE void SE_enableInterrupt | ( | uint32_t |
flags
|
) |
Enable one or more SE interrupts.
- Parameters
-
[in] flagsSE interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the Secure Element module (SEMAILBOX_CONFIGURATION_TXINTEN or SEMAILBOX_CONFIGURATION_RXINTEN).
Definition at line
527
of file
em_se.h
.
| SE_Response_t SE_eraseUserData | ( |
|
) |
Erases User Data section in MTP.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully or a signature was successfully verified, SE_RESPONSE_INVALID_COMMANDwhen the command ID was not recognized, SE_RESPONSE_AUTHORIZATION_ERRORwhen the command is not authorized, SE_RESPONSE_INVALID_SIGNATUREwhen signature verification failed, SE_RESPONSE_BUS_ERRORwhen a bus error was thrown during the command, e.g. because of conflicting Secure/Non-Secure memory accesses, SE_RESPONSE_CRYPTO_ERRORon an internal SE failure, or SE_RESPONSE_INVALID_PARAMETERwhen an invalid parameter was passed
Definition at line
616
of file
em_se.c
.
References SE_addParameter() , SE_COMMAND_DEFAULT , SE_COMMAND_OPTION_ERASE_UD , SE_executeCommand() , and SE_readCommandResponse() .
| void SE_executeCommand | ( | SE_Command_t * |
command
|
) |
Execute the passed command.
This function starts the execution of the passed command by the secure element. When started, wait for the RXINT interrupt flag, or call SE_waitCommandCompletion to busy-wait. After completion, you have to call SE_readCommandResponse to get the command's execution status.
- Parameters
-
[in] commandPointer to a filled-out SE command structure.
Definition at line
218
of file
em_se.c
.
References SE_MAX_PARAMETERS .
Referenced by SE_debugLockApply() , SE_debugLockStatus() , SE_debugSecureDisable() , SE_debugSecureEnable() , SE_deviceErase() , SE_deviceEraseDisable() , SE_eraseUserData() , SE_getStatus() , SE_initOTP() , SE_initPubkey() , SE_readPubkey() , SE_serialNumber() , and SE_writeUserData() .
| SE_Response_t SE_getStatus | ( | SE_Status_t * |
status
|
) |
Returns the current boot status, versions and system configuration.
- Parameters
-
[out] statusSE_Status_t containing current SE status.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKupon command completion. Errors are encoded in the different parts of the returned status object.
Definition at line
639
of file
em_se.c
.
References SE_Status_t::bootStatus , SE_DebugStatus_t::debugLockEnabled , SE_Status_t::debugStatus , SE_DebugStatus_t::deviceEraseEnabled , SE_Status_t::hostFwVersion , SE_addDataOutput() , SE_COMMAND_DEFAULT , SE_DATATRANSFER_DEFAULT , SE_executeCommand() , SE_readCommandResponse() , SE_Status_t::secureBootEnabled , SE_DebugStatus_t::secureDebugEnabled , and SE_Status_t::seFwVersion .
| SE_Response_t SE_initOTP | ( | SE_OTPInit_t * |
otp_init
|
) |
Initialize SE OTP configuration.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully
Definition at line
817
of file
em_se.c
.
References SE_OTPInit_t::enableAntiRollback , SE_OTPInit_t::enableSecureBoot , SE_addDataInput() , SE_COMMAND_DEFAULT , SE_DATATRANSFER_DEFAULT , SE_executeCommand() , SE_KEY_TYPE_BOOT , SE_readCommandResponse() , SE_readPubkey() , SE_RESPONSE_OK , and SE_OTPInit_t::verifySecureBootCertificate .
| SE_Response_t SE_initPubkey | ( | uint32_t |
key_type,
|
| void * |
pubkey,
|
||
| uint32_t |
numBytes,
|
||
| bool |
signature
|
||
| ) |
Init pubkey or pubkey signature.
Initialize public key stored in the SE, or its signature. The command can be used to write:
- SE_KEY_TYPE_BOOT
- SE_KEY_TYPE_AUTH
- Note
- These keys can not be overwritten, so this command can only be issued once per key per part.
- Parameters
-
[in] key_typeID of key type to initialize. [in] pubkeyPointer to a buffer that contains the public key or signature. Must be word aligned and have a length of 64 bytes. [in] numBytesLength of pubkey buffer (64 bytes). [in] signatureIf true, initialize signature for the requested key type instead of the public key.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully SE_RESPONSE_TEST_FAILEDwhen the pubkey is not set SE_RESPONSE_INVALID_PARAMETERwhen an invalid type is passed
Definition at line
780
of file
em_se.c
.
References SE_addDataInput() , SE_COMMAND_DEFAULT , SE_DATATRANSFER_DEFAULT , SE_executeCommand() , SE_KEY_TYPE_BOOT , and SE_readCommandResponse() .
| __STATIC_INLINE bool SE_isCommandCompleted | ( | void |
|
) |
Check whether the running command has completed.
This function polls the SE-to-host mailbox interrupt flag.
- Returns
- True if a command has completed and the result is available
Definition at line
448
of file
em_se.h
.
Referenced by SE_waitCommandCompletion() .
| __STATIC_INLINE SE_Response_t SE_readCommandResponse | ( | void |
|
) |
Read the status of the previously executed command.
This function reads the status of the previously executed command.
- Note
- The command response needs to be read for every executed command, and can only be read once per executed command (FIFO behavior).
- Returns
- One of the SE_RESPONSE return codes: SE_RESPONSE_OK when the command was executed successfully or a signature was successfully verified, SE_RESPONSE_INVALID_COMMAND when the command ID was not recognized, SE_RESPONSE_AUTHORIZATION_ERROR when the command is not authorized, SE_RESPONSE_INVALID_SIGNATURE when signature verification failed, SE_RESPONSE_BUS_ERROR when a bus error was thrown during the command, e.g. because of conflicting Secure/Non-Secure memory accesses, SE_RESPONSE_CRYPTO_ERROR on an internal SE failure, or SE_RESPONSE_INVALID_PARAMETER when an invalid parameter was passed
Definition at line
493
of file
em_se.h
.
References SE_waitCommandCompletion() .
Referenced by SE_debugLockApply() , SE_debugLockStatus() , SE_debugSecureDisable() , SE_debugSecureEnable() , SE_deviceErase() , SE_deviceEraseDisable() , SE_eraseUserData() , SE_getStatus() , SE_initOTP() , SE_initPubkey() , SE_readPubkey() , SE_serialNumber() , and SE_writeUserData() .
| SE_Response_t SE_readPubkey | ( | uint32_t |
key_type,
|
| void * |
pubkey,
|
||
| uint32_t |
numBytes,
|
||
| bool |
signature
|
||
| ) |
Read pubkey or pubkey signature.
Read out a public key stored in the SE, or its signature. The command can be used to read:
- SE_KEY_TYPE_BOOT
- SE_KEY_TYPE_AUTH
- Parameters
-
[in] key_typeID of key type to read. [out] pubkeyPointer to a buffer to contain the returned public key. Must be word aligned and have a length of 64 bytes. [in] numBytesLength of pubkey buffer (64 bytes). [in] signatureIf true, read signature for the requested key type instead of the public key.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully SE_RESPONSE_TEST_FAILEDwhen the pubkey is not set SE_RESPONSE_INVALID_PARAMETERwhen an invalid type is passed
Definition at line
725
of file
em_se.c
.
References SE_addDataOutput() , SE_COMMAND_DEFAULT , SE_DATATRANSFER_DEFAULT , SE_executeCommand() , SE_KEY_TYPE_BOOT , and SE_readCommandResponse() .
Referenced by SE_initOTP() .
| SE_Response_t SE_serialNumber | ( | void * |
serial
|
) |
Read the serial number of the SE module.
- Parameters
-
[out] serialPointer to array of size 16 bytes.
- Returns
- One of the SE_Response_t return codes.
- Return values
-
SE_RESPONSE_OKwhen serial number is returned successfully, SE_RESPONSE_INTERNAL_ERRORif not.
Definition at line
681
of file
em_se.c
.
References SE_addDataOutput() , SE_COMMAND_DEFAULT , SE_DATATRANSFER_DEFAULT , SE_executeCommand() , and SE_readCommandResponse() .
| __STATIC_INLINE void SE_waitCommandCompletion | ( | void |
|
) |
Wait for completion of the current command.
This function "busy"-waits until the execution of the ongoing instruction has completed.
Definition at line
462
of file
em_se.h
.
References SE_isCommandCompleted() .
Referenced by SE_readCommandResponse() .
| SE_Response_t SE_writeUserData | ( | uint32_t |
offset,
|
| void * |
data,
|
||
| uint32_t |
numBytes
|
||
| ) |
Writes data to User Data section in MTP. Write data must be aligned to word size and contain a number of bytes that is divisable by four.
- Note
- It is recommended to erase the flash page before performing a write.
- Parameters
-
[in] offsetOffset to the flash word to write to. Must be aligned to words. [in] dataData to write to flash. [in] numBytesNumber of bytes to write to flash. NB: Must be divisable by four.
- Returns
- One of the SE_RESPONSE return codes.
- Return values
-
SE_RESPONSE_OKwhen the command was executed successfully or a signature was successfully verified, SE_RESPONSE_INVALID_COMMANDwhen the command ID was not recognized, SE_RESPONSE_AUTHORIZATION_ERRORwhen the command is not authorized, SE_RESPONSE_INVALID_SIGNATUREwhen signature verification failed, SE_RESPONSE_BUS_ERRORwhen a bus error was thrown during the command, e.g. because of conflicting Secure/Non-Secure memory accesses, SE_RESPONSE_CRYPTO_ERRORon an internal SE failure, or SE_RESPONSE_INVALID_PARAMETERwhen an invalid parameter was passed
Definition at line
582
of file
em_se.c
.
References SE_addDataInput() , SE_addParameter() , SE_COMMAND_DEFAULT , SE_DATATRANSFER_DEFAULT , SE_executeCommand() , and SE_readCommandResponse() .