IADC_Init_t Struct ReferenceEMLIB > IADC
IADC init structure, common for single conversion and scan sequence.
       Definition at line
       
        629
       
       of file
       
        em_iadc.h
       
       .
      
      
       #include <
       
     
        em_iadc.h
       
       >
      
| Data Fields | |
| bool | debugHalt | 
| uint16_t | greaterThanEqualThres | 
| bool | iadcClkSuspend0 | 
| bool | iadcClkSuspend1 | 
| uint16_t | lessThanEqualThres | 
| uint8_t | srcClkPrescale | 
| uint8_t | timebase | 
| uint16_t | timerCycles | 
| IADC_Warmup_t | warmup | 
Field Documentation
| bool IADC_Init_t::debugHalt | 
| uint16_t IADC_Init_t::greaterThanEqualThres | 
Digital window comparator greater-than or equal threshold.
        Definition at line
        
         642
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| bool IADC_Init_t::iadcClkSuspend0 | 
Suspend IADC_CLK until PRS0 trigger.
        Definition at line
        
         630
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| bool IADC_Init_t::iadcClkSuspend1 | 
Suspend IADC_CLK until PRS1 trigger.
        Definition at line
        
         631
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| uint16_t IADC_Init_t::lessThanEqualThres | 
Digital window comparator less-than or equal threshold.
        Definition at line
        
         643
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| uint8_t IADC_Init_t::srcClkPrescale | 
User requested source clock divider (prescale+1) which will be used if the calculated prescaler value is less.
        Definition at line
        
         639
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| uint8_t IADC_Init_t::timebase | 
IADC clock cycles (timebase+1) corresponding to 1us. Used as time reference for IADC delays, e.g. warmup. If the user sets timebase to 0, then IADC_Init() will calculate the timebase using the currently defined CMU clock setting for the IADC.
        Definition at line
        
         634
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| uint16_t IADC_Init_t::timerCycles | 
Number of ADC_CLK cycles per TIMER event.
        Definition at line
        
         641
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_init() .
| IADC_Warmup_t IADC_Init_t::warmup | 
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_iadc.h