SMUEMLIB

Detailed Description

Security Management Unit (SMU) Peripheral API.

SMU forms the control and status/reporting component of bus-level security in EFM32/EFR32 devices.

Peripheral-level protection is provided via the peripheral protection unit (PPU). PPU provides hardware access barrier to any peripheral that is configured to be protected. When an attempt is made to access a peripheral without the required privilege/security level, PPU detects the fault and intercepts the access. No write or read of the peripheral register space occurs, and an all-zero value is returned if the access is a read.

// SMU is always clocked, so no call to CMU_ClockEnable() is necessary
// Initialize SMU to prevent access to CMU, EMU, SMU and GPIO
init.ppu.access.privilegedCMU = true;
init.ppu.access.privilegedEMU = true;
init.ppu.access.privilegedSMU = true;
init.ppu.access.privilegedGPIO = true;
SMU_Init(&init);

Data Structures

struct  SMU_Init_TypeDef
 
struct  SMU_PrivilegedAccess_TypeDef
 

Macros

#define SMU_INIT_DEFAULT
 

Enumerations

enum  SMU_Peripheral_TypeDef {
  smuPeripheralEMU = _SMU_PPUPATD0_EMU_SHIFT,
  smuPeripheralCMU = _SMU_PPUPATD0_CMU_SHIFT,
  smuPeripheralHFXO = _SMU_PPUPATD0_HFXO0_SHIFT,
  smuPeripheralHFRCO0 = _SMU_PPUPATD0_HFRCO0_SHIFT,
  smuPeripheralFSRCO = _SMU_PPUPATD0_FSRCO_SHIFT,
  smuPeripheralDPLL0 = _SMU_PPUPATD0_DPLL0_SHIFT,
  smuPeripheralLFXO = _SMU_PPUPATD0_LFXO_SHIFT,
  smuPeripheralLFRCO = _SMU_PPUPATD0_LFRCO_SHIFT,
  smuPeripheralULFRCO = _SMU_PPUPATD0_ULFRCO_SHIFT,
  smuPeripheralMSC = _SMU_PPUPATD0_MSC_SHIFT,
  smuPeripheralICACHE0 = _SMU_PPUPATD0_ICACHE0_SHIFT,
  smuPeripheralPRS = _SMU_PPUPATD0_PRS_SHIFT,
  smuPeripheralGPIO = _SMU_PPUPATD0_GPIO_SHIFT,
  smuPeripheralLDMA = _SMU_PPUPATD0_LDMA_SHIFT,
  smuPeripheralLDMAXBAR = _SMU_PPUPATD0_LDMAXBAR_SHIFT,
  smuPeripheralTIMER0 = _SMU_PPUPATD0_TIMER0_SHIFT,
  smuPeripheralTIMER1 = _SMU_PPUPATD0_TIMER1_SHIFT,
  smuPeripheralTIMER2 = _SMU_PPUPATD0_TIMER2_SHIFT,
  smuPeripheralTIMER3 = _SMU_PPUPATD0_TIMER3_SHIFT,
  smuPeripheralUSART0 = _SMU_PPUPATD0_USART0_SHIFT,
  smuPeripheralUSART1 = _SMU_PPUPATD0_USART1_SHIFT,
  smuPeripheralUSART2 = _SMU_PPUPATD0_USART2_SHIFT,
  smuPeripheralBURTC = _SMU_PPUPATD0_BURTC_SHIFT,
  smuPeripheralI2C1 = _SMU_PPUPATD0_I2C1_SHIFT,
  smuPeripheralCHIPTESTCTRL = _SMU_PPUPATD0_CHIPTESTCTRL_SHIFT,
  smuPeripheralLVGD = _SMU_PPUPATD0_LVGD_SHIFT,
  smuPeripheralSYSCFG = _SMU_PPUPATD0_SYSCFG_SHIFT,
  smuPeripheralBURAM = _SMU_PPUPATD0_BURAM_SHIFT,
  smuPeripheralIFADCDEBUG = _SMU_PPUPATD0_IFADCDEBUG_SHIFT,
  smuPeripheralGPCRC = _SMU_PPUPATD0_GPCRC_SHIFT,
  smuPeripheralRTCC = _SMU_PPUPATD0_RTCC_SHIFT,
  smuPeripheralLETIMER0 = 32 + _SMU_PPUPATD1_LETIMER0_SHIFT,
  smuPeripheralIADC0 = 32 + _SMU_PPUPATD1_IADC0_SHIFT,
  smuPeripheralACMP0 = 32 + _SMU_PPUPATD1_ACMP0_SHIFT,
  smuPeripheralACMP1 = 32 + _SMU_PPUPATD1_ACMP1_SHIFT,
  smuPeripheralI2C0 = 32 + _SMU_PPUPATD1_I2C0_SHIFT,
  smuPeripheralHFRCOEM23 = 32 + _SMU_PPUPATD1_HFRCOEM23_SHIFT,
  smuPeripheralWDOG0 = 32 + _SMU_PPUPATD1_WDOG0_SHIFT,
  smuPeripheralWDOG1 = 32 + _SMU_PPUPATD1_WDOG1_SHIFT,
  smuPeripheralAMUXCP0 = 32 + _SMU_PPUPATD1_AMUXCP0_SHIFT,
  smuPeripheralRADIOAES = 32 + _SMU_PPUPATD1_RADIOAES_SHIFT,
  smuPeripheralBUFC = 32 + _SMU_PPUPATD1_BUFC_SHIFT,
  smuPeripheralSMU = 32 + _SMU_PPUPATD1_SMU_SHIFT,
  smuPeripheralAHBRADIO = 32 + _SMU_PPUPATD1_AHBRADIO_SHIFT,
  smuPeripheralSEMAILBOX = 32 + _SMU_PPUPATD1_SEMAILBOX_SHIFT,
  smuPeripheralEnd
}
 

Functions

__STATIC_INLINE void SMU_EnablePPU (bool enable)
 Enable or disable PPU of SMU.
 
__STATIC_INLINE SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral (void)
 Get ID of the peripheral that caused an access fault.
 
__STATIC_INLINE void SMU_Init (const SMU_Init_TypeDef *init)
 Initialize PPU of SMU.
 
__STATIC_INLINE void SMU_IntClear (uint32_t flags)
 Clear one or more pending SMU interrupts.
 
__STATIC_INLINE void SMU_IntDisable (uint32_t flags)
 Disable one or more SMU interrupts.
 
__STATIC_INLINE void SMU_IntEnable (uint32_t flags)
 Enable one or more SMU interrupts.
 
__STATIC_INLINE uint32_t SMU_IntGet (void)
 Get pending SMU interrupts.
 
__STATIC_INLINE uint32_t SMU_IntGetEnabled (void)
 Get enabled and pending SMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
 
__STATIC_INLINE void SMU_IntSet (uint32_t flags)
 Set one or more pending SMU interrupts from SW.
 
__STATIC_INLINE void SMU_SetPrivilegedAccess (SMU_Peripheral_TypeDef peripheral, bool privileged)
 Change access settings for a peripheral.
 

Macro Definition Documentation

#define SMU_INIT_DEFAULT
Value:
{ \
{ { 0 } }, /* No peripherals access protected. */ \
true /* Enable SMU.*/ \
}

Default SMU initialization structure settings.

Definition at line 911 of file em_smu.h.

Enumeration Type Documentation

SMU peripheral identifiers.

Enumerator
smuPeripheralEMU 

SMU peripheral identifier for EMU

smuPeripheralCMU 

SMU peripheral identifier for CMU

smuPeripheralHFXO 

SMU peripheral identifier for HFXO0

smuPeripheralHFRCO0 

SMU peripheral identifier for HFRCO0

smuPeripheralFSRCO 

SMU peripheral identifier for FSRCO

smuPeripheralDPLL0 

SMU peripheral identifier for DPLL0

smuPeripheralLFXO 

SMU peripheral identifier for LFXO

smuPeripheralLFRCO 

SMU peripheral identifier for LFRCO

smuPeripheralULFRCO 

SMU peripheral identifier for ULFRCO

smuPeripheralMSC 

SMU peripheral identifier for MSC

smuPeripheralICACHE0 

SMU peripheral identifier for ICACHE0

smuPeripheralPRS 

SMU peripheral identifier for PRS

smuPeripheralGPIO 

SMU peripheral identifier for GPIO

smuPeripheralLDMA 

SMU peripheral identifier for LDMA

smuPeripheralLDMAXBAR 

SMU peripheral identifier for LDMAXBAR

smuPeripheralTIMER0 

SMU peripheral identifier for TIMER0

smuPeripheralTIMER1 

SMU peripheral identifier for TIMER1

smuPeripheralTIMER2 

SMU peripheral identifier for TIMER2

smuPeripheralTIMER3 

SMU peripheral identifier for TIMER3

smuPeripheralUSART0 

SMU peripheral identifier for USART0

smuPeripheralUSART1 

SMU peripheral identifier for USART1

smuPeripheralUSART2 

SMU peripheral identifier for USART2

smuPeripheralBURTC 

SMU peripheral identifier for BURTC

smuPeripheralI2C1 

SMU peripheral identifier for I2C1

smuPeripheralCHIPTESTCTRL 

SMU peripheral identifier for CHIPTESTCTRL

smuPeripheralLVGD 

SMU peripheral identifier for LVGD

smuPeripheralSYSCFG 

SMU peripheral identifier for SYSCFG

smuPeripheralBURAM 

SMU peripheral identifier for BURAM

smuPeripheralIFADCDEBUG 

SMU peripheral identifier for IFADCDEBUG

smuPeripheralGPCRC 

SMU peripheral identifier for GPCRC

smuPeripheralRTCC 

SMU peripheral identifier for RTCC

smuPeripheralLETIMER0 

SMU peripheral identifier for LETIMER

smuPeripheralIADC0 

SMU peripheral identifier for IADC0

smuPeripheralACMP0 

SMU peripheral identifier for ACMP0

smuPeripheralACMP1 

SMU peripheral identifier for ACMP1

smuPeripheralI2C0 

SMU peripheral identifier for I2C0

smuPeripheralHFRCOEM23 

SMU peripheral identifier for HFRCOEM23

smuPeripheralWDOG0 

SMU peripheral identifier for WDOG0

smuPeripheralWDOG1 

SMU peripheral identifier for WDOG1

smuPeripheralAMUXCP0 

SMU peripheral identifier for AMUXCP0

smuPeripheralRADIOAES 

SMU peripheral identifier for RADIOAES

smuPeripheralBUFC 

SMU peripheral identifier for BUFC

smuPeripheralSMU 

SMU peripheral identifier for SMU

smuPeripheralAHBRADIO 

SMU peripheral identifier for AHBRADIO

smuPeripheralSEMAILBOX 

SMU peripheral identifier for SEMAILBOX

Definition at line 78 of file em_smu.h.

Function Documentation

__STATIC_INLINE void SMU_EnablePPU ( bool  enable)

Enable or disable PPU of SMU.

Parameters
[in]enableSet to true to enable PPU; set to false otherwise.

Definition at line 927 of file em_smu.h.

References BUS_RegBitWrite().

Referenced by SMU_Init().

__STATIC_INLINE SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral ( void  )

Get ID of the peripheral that caused an access fault.

Note
The return value is only valid if SMU_IF_PPUPRIV interrupt flag is set.
Returns
ID of the peripheral that caused an access fault.

Definition at line 989 of file em_smu.h.

__STATIC_INLINE void SMU_Init ( const SMU_Init_TypeDef init)

Initialize PPU of SMU.

Parameters
[in]initPointer to initialization structure that defines which peripherals should only be accessed from privileged mode, and if PPU should be enabled.

Definition at line 944 of file em_smu.h.

References SMU_Init_TypeDef::enable, SMU_Init_TypeDef::reg, and SMU_EnablePPU().

__STATIC_INLINE void SMU_IntClear ( uint32_t  flags)

Clear one or more pending SMU interrupts.

Parameters
[in]flagsBitwise logic OR of SMU interrupt sources to clear.

Definition at line 1001 of file em_smu.h.

__STATIC_INLINE void SMU_IntDisable ( uint32_t  flags)

Disable one or more SMU interrupts.

Parameters
[in]flagsSMU interrupt sources to disable.

Definition at line 1017 of file em_smu.h.

__STATIC_INLINE void SMU_IntEnable ( uint32_t  flags)

Enable one or more SMU interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using SMU_IntClear() prior to enabling the interrupt.
Parameters
[in]flagsSMU interrupt sources to enable.

Definition at line 1038 of file em_smu.h.

__STATIC_INLINE uint32_t SMU_IntGet ( void  )

Get pending SMU interrupts.

Returns
SMU interrupt sources pending.

Definition at line 1054 of file em_smu.h.

__STATIC_INLINE uint32_t SMU_IntGetEnabled ( void  )

Get enabled and pending SMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.

Note
Interrupt flags are not cleared by this function.
Returns
Pending and enabled SMU interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in SMU_IEN register and
  • the OR combination of valid interrupt flags in SMU_IF register.

Definition at line 1074 of file em_smu.h.

__STATIC_INLINE void SMU_IntSet ( uint32_t  flags)

Set one or more pending SMU interrupts from SW.

Parameters
[in]flagsSMU interrupt sources to set to pending.

Definition at line 1093 of file em_smu.h.

__STATIC_INLINE void SMU_SetPrivilegedAccess ( SMU_Peripheral_TypeDef  peripheral,
bool  privileged 
)

Change access settings for a peripheral.

Set to limit access of a peripheral from privileged mode.

Parameters
[in]peripheralID of the peripheral to change access settings for.
[in]privilegedSet to true if the peripheral should only be accessed from privileged mode; set to false otherwise.

Definition at line 966 of file em_smu.h.

References BUS_RegBitWrite().