IADC_InitScan_t Struct ReferenceEMLIB > IADC
IADC scan init structure
       Definition at line
       
        699
       
       of file
       
        em_iadc.h
       
       .
      
      
       #include <
       
     
        em_iadc.h
       
       >
      
| Data Fields | |
| IADC_Alignment_t | alignment | 
| uint8_t | dataValidLevel | 
| bool | fifoDmaWakeup | 
| bool | showId | 
| bool | start | 
| IADC_TriggerAction_t | triggerAction | 
| IADC_TriggerSel_t | triggerSelect | 
Field Documentation
| IADC_Alignment_t IADC_InitScan_t::alignment | 
Alignment of data in FIFO.
        Definition at line
        
         700
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_initScan() .
| uint8_t IADC_InitScan_t::dataValidLevel | 
Data valid level before requesting DMA transfer.
        Definition at line
        
         702
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_initScan() .
| bool IADC_InitScan_t::fifoDmaWakeup | 
Wake-up DMA when FIFO reaches data valid level.
        Definition at line
        
         703
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_initScan() .
| bool IADC_InitScan_t::showId | 
Tag FIFO entry with scan table entry id.
        Definition at line
        
         701
        
        of file
        
         em_iadc.h
        
        .
       
Referenced by IADC_initScan() .
| bool IADC_InitScan_t::start | 
| IADC_TriggerAction_t IADC_InitScan_t::triggerAction | 
| IADC_TriggerSel_t IADC_InitScan_t::triggerSelect | 
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_iadc.h