HidKeyboardKit Drivers
Detailed Description
Implements a USB HID class keyboard.
HIDKBD Implementation
      The source code of the HIDKBD implementation resides in kits/common/drivers/hidkbd.c and
      
       hidkbd.h
      
      . This driver implements a basic USB keyboard. Refer to hidkbd examples for STK3700 and DK3750 for examples using this driver.
     
HIDKBD Device Configuration Options
This section contains a description of the configuration options for the driver. The options are #define's which are expected to be found in the application "usbconfig.h" header file. The values shown below are from the Giant Gecko STK3700 hidbkd example.
// USB interface number. Interfaces are numbered from zero to one less than // the number of concurrent interfaces supported by the configuration. // The interfac numbers must be 0 standalone HID device, for a // composite device which includes a HID interface it must not be in conflict // with other device interfaces. #define HIDKBD_INTERFACE_NO 0 // Endpoint address for HID input reports. #define HIDKBD_INTR_IN_EP_ADDR 0x81 // The bInterval reported with the interrupt IN endpoint descriptor. #define HIDKBD_POLL_RATE 24 // Timer id, see USBTIMER in the USB device stack documentation. // The HID driver use a timer to implement the idle-rate defined in the HID class spec. #define HIDKBD_IDLE_TIMER 0
| Data Structures | |
| struct | HIDKBD_Init_t | 
| struct | HIDKBD_KeyReport_t | 
| Macros | |
| #define | DEFAULT_IDLE_RATE 500 | 
| Typedefs | |
| typedef void(* | HIDKBD_SetReportFunc_t ) (uint8_t report) | 
| Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device. | |
| Functions | |
| void | HIDKBD_Init ( HIDKBD_Init_t *init) | 
| Initialize HID Keyboard driver. | |
| void | HIDKBD_KeyboardEvent ( HIDKBD_KeyReport_t *report) | 
| Report a keyboard press/release event. | |
| int | HIDKBD_SetupCmd (const USB_Setup_TypeDef *setup) | 
| Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command. | |
| void | HIDKBD_StateChangeEvent (USBD_State_TypeDef oldState, USBD_State_TypeDef newState) | 
| Handle USB state change events, this function must be called each time the USB device state is changed. | |
| const char HIDKBD_ReportDescriptor[69] | SL_ATTRIBUTE_ALIGN (4) | 
| Variables | |
| const char | HIDKBD_ReportDescriptor [69] | 
Macro Definition Documentation
| #define DEFAULT_IDLE_RATE 500 | 
Default idle-rate recommended in the USB HID class specification.
        Definition at line
        
         72
        
        of file
        
         hidkbd.c
        
        .
       
Referenced by HIDKBD_StateChangeEvent() .
Typedef Documentation
| typedef void(* HIDKBD_SetReportFunc_t) (uint8_t report) | 
Callback function pointer for HID output reports. This function will be called by the driver each time an output report is received by the device.
- Parameters
- 
         [in] reportOutput report byte. 
 Bit 0 : State of keyboard NumLock LED.
 Bit 1 : State of keyboard CapsLock LED.
 Bit 2 : State of keyboard ScrollLock LED.
        Definition at line
        
         59
        
        of file
        
         hidkbd.h
        
        .
       
Function Documentation
| void HIDKBD_Init | ( | HIDKBD_Init_t * | 
            init
            | ) | 
Initialize HID Keyboard driver.
- Parameters
- 
         [in] initPointer to a HIDKBD_Init_t struct with configuration options. 
        Definition at line
        
         198
        
        of file
        
         hidkbd.c
        
        .
       
References HIDKBD_Init_t::hidDescriptor , and HIDKBD_Init_t::setReportFunc .
| void HIDKBD_KeyboardEvent | ( | HIDKBD_KeyReport_t * | 
            report
            | ) | 
Report a keyboard press/release event.
- Parameters
- 
         [in] reportPointer to a HIDKBD_KeyReport_t struct with new key pressed information. 
        Definition at line
        
         213
        
        of file
        
         hidkbd.c
        
        .
       
| int HIDKBD_SetupCmd | ( | const USB_Setup_TypeDef * | 
            setup
            | ) | 
Handle USB setup commands. Implements HID class specific commands. This function must be called each time the device receive a setup command.
- Parameters
- 
         [in] setupPointer to the setup packet received. 
- Returns
- USB_STATUS_OK if command accepted, USB_STATUS_REQ_UNHANDLED when command is unknown. In the latter case the USB device stack will handle the request.
        Definition at line
        
         240
        
        of file
        
         hidkbd.c
        
        .
       
References SL_MIN .
| void HIDKBD_StateChangeEvent | ( | USBD_State_TypeDef | 
            oldState,
            | 
| USBD_State_TypeDef | 
            newState
            | ||
| ) | 
Handle USB state change events, this function must be called each time the USB device state is changed.
- Parameters
- 
         [in] oldStateThe device state the device has just left. [in] newStateThe new device state. 
        Definition at line
        
         337
        
        of file
        
         hidkbd.c
        
        .
       
References DEFAULT_IDLE_RATE .
| const char HIDKBD_ReportDescriptor [69] SL_ATTRIBUTE_ALIGN | ( | 4 | 
            | ) | 
HID report descriptor created with usb.org's "HID Descriptor Tool(DT)" version 2.4. The descriptor defines an input report which matches the HIDKBD_KeyReport_t typedef, and an output report with 3 bits for controlling NumLock, CapsLock and ScrollLock keyboard LED's