CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU
HFXO initialization structure. Init values should be obtained from a configuration tool, app. note or xtal datasheet.
       Definition at line
       
        549
       
       of file
       
        em_cmu.h
       
       .
      
      
       #include <
       
     
        em_cmu.h
       
       >
      
| Data Fields | |
| uint8_t | coreBiasAna | 
| uint8_t | coreBiasStartup | 
| CMU_HfxoCoreDegen_TypeDef | coreDegenAna | 
| CMU_HfxoCtuneFixCap_TypeDef | ctuneFixAna | 
| uint8_t | ctuneXiAna | 
| uint8_t | ctuneXiStartup | 
| uint8_t | ctuneXoAna | 
| uint8_t | ctuneXoStartup | 
| bool | disOnDemand | 
| bool | enXiDcBiasAna | 
| bool | forceEn | 
| bool | forceXi2GndAna | 
| bool | forceXo2GndAna | 
| uint8_t | imCoreBiasStartup | 
| CMU_HfxoOscMode_TypeDef | mode | 
| bool | regLock | 
| CMU_HfxoCbLsbTimeout_TypeDef | timeoutCbLsb | 
| CMU_HfxoSteadyStateTimeout_TypeDef | timeoutSteady | 
| CMU_HfxoSteadyStateTimeout_TypeDef | timeoutSteadyFirstLock | 
Field Documentation
| uint8_t CMU_HFXOInit_TypeDef::coreBiasAna | 
| uint8_t CMU_HFXOInit_TypeDef::coreBiasStartup | 
| CMU_HfxoCoreDegen_TypeDef CMU_HFXOInit_TypeDef::coreDegenAna | 
| CMU_HfxoCtuneFixCap_TypeDef CMU_HFXOInit_TypeDef::ctuneFixAna | 
Fixed tuning capacitance on XI/XO.
        Definition at line
        
         558
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::ctuneXiAna | 
Tuning capacitance on XI.
        Definition at line
        
         560
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::ctuneXiStartup | 
XI pin startup tuning capacitance.
        Definition at line
        
         554
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::ctuneXoAna | 
Tuning capacitance on XO.
        Definition at line
        
         559
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by BSP_initClocks() , and CMU_HFXOInit() .
| uint8_t CMU_HFXOInit_TypeDef::ctuneXoStartup | 
XO pin startup tuning capacitance.
        Definition at line
        
         553
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::disOnDemand | 
Disable on-demand requests.
        Definition at line
        
         566
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::enXiDcBiasAna | 
Enable XI internal DC bias.
        Definition at line
        
         562
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| bool CMU_HFXOInit_TypeDef::forceEn | 
| bool CMU_HFXOInit_TypeDef::forceXi2GndAna | 
| bool CMU_HFXOInit_TypeDef::forceXo2GndAna | 
| uint8_t CMU_HFXOInit_TypeDef::imCoreBiasStartup | 
Core bias intermediate startup current.
        Definition at line
        
         556
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| CMU_HfxoOscMode_TypeDef CMU_HFXOInit_TypeDef::mode | 
| bool CMU_HFXOInit_TypeDef::regLock | 
| CMU_HfxoCbLsbTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutCbLsb | 
| CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteady | 
Steady state timeout duration.
        Definition at line
        
         552
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
| CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteadyFirstLock | 
Steady state timeout duration for first lock.
        Definition at line
        
         551
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by CMU_HFXOInit() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_cmu.h